FTF_Austin_FTF-ACC-F1276_2015.pptx

File uploaded by Andrew Robertson Employee on May 13, 2015Last modified by Renee Fortenberry on Oct 5, 2015
Version 3Show Document
  • View in full screen mode

This session will explain how Freescale can enable customers to develop 76-81 GHz short and long range radar applications using the MPC577xK MCU, it will explain the concepts of the radar algorithms, including practical aspects such as SDADC or MIPI CSI sampling, Chirp Generation, Data Compression, R,V FFT, Detection and Tracking algorithms, and the benefits of the new Freescale IP that can allow them to improve their system resolution and accuracy. In this session customers will take away a detailed understanding of how to develop fast modulation radar systems using the MPC577xK MCU including the BOM cost advantages it also brings.

Outcomes