Example MPC5744P ADC GHS614

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5744P ADC GHS614

Example MPC5744P ADC GHS614

********************************************************************************

* Detailed Description:

* This example content a driver for ADC module.

* Basic ADC functionality is demonstrated via ADC_0 normal conversion for ADC_0 AN0 channel.

*

* For closer details on how ADC works I suggest you to check reference manual.

* This example sets system clock for 200MHz running from PLL0 module.

* Example contains basic ADC functionality demonstration. Software is starting normal ADC conversion

* on ADC_0 channel AN0.

* To demonstrate the measurement functionality on Freescale MPC57xx motherboard connect jumper to J53.

* By doing this the potentiometer is connected to AN0 ADC input. For further details see MPC57xx EVB schematics.

*

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx Motherboard + MPC5744PE257DC minimodule, MPC5744P,

* silicon mask set 1N65H

* Target :  internal_FLASH*

********************************************************************************

Labels (1)
Attachments
No ratings
Version history
Last update:
‎03-19-2015 05:13 AM
Updated by: