Gyroscope: FXAS2100x Breakout Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gyroscope: FXAS2100x Breakout Board

Gyroscope: FXAS2100x Breakout Board

Hi,

The FXAS2100x, is a small, low-power, yaw, pitch, and roll angular rate gyroscope with 16 bit ADC resolution. The full-scale range is adjustable from ±250°/s to ±2000°/s. It features both I2C and SPI interfaces.

Here is a Render of the FXAS2100x Breakout- Board downloaded from OSH Park:

PCB Render.png

Layout Design for this board:

Layout Render.png

In the Attachments section, you can find the Schematic Source File (SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM files.

If you're interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOME

Labels (1)
Attachments
No ratings
Version history
Last update:
‎01-21-2015 03:41 PM
Updated by: