Proximetry Multi-Network High Density Node Gateway Demo

Document created by Bill Krakar Employee on Dec 20, 2014Last modified by Diana Torres on Feb 28, 2018
Version 35Show Document
  • View in full screen mode

Proximetry Multi-Network High Density Node Gateway Demo

 

Proximetry Demo.png

View of the Proximetry web cloud interface and one of the i.MX6 Gateways in operation at our Austin demo network site.

 

Highlighted Features

  • 3 networks remotely managed simultaneously via the Proximetry cloud and agent software

  • IPv6, ZigBee PRO networks over 802.15.4 2.4 Ghz

Description

  • Our Austin, TX Network
    • Proximetry cloud and gateway agent software
    • i.MX6 Dual IOT Gateway
    • 1 x USB-KW24D512 running FlexibleIP with Border Router and VTUN interface over USB
    • 25-50 x TWR-KW24D512 running FlexibleIP with Router functionality
    • Mesh topology with all devices acting as Routers

 

  • Our Guadalajara, Mexico Network

    • Proximetry cloud and gateway agent software
    • i.MX6 Dual IOT Gateway
    • 1 x USB-KW24D512 ZigBee PRO Home Automation 1.2 Border Router
    • 50 x TWR-KW24D512 ZigBee PRO Home Automation 1.2 Router/Edge Nodes
    • Mesh topology with all devices acting as Routers

 

  • Texas State University, San Marcos TX Network
    • Proximetry cloud and gateway agent software

    • i.MX6 Dual IOT Gateway

    • 1 x USB-KW24D512 ZigBee PRO Home Automation 1.2 Border Router

    • 48 x USB-KW24D512 ZigBee PRO Home Automation 1.2 Router/Edge Nodes
    • Mesh topology with all devices acting as Routers

 

Demo Video

Under Construction

 

System Diagram

Cloud Connectivity Diagram for Kinetis Microcontrollers (MCUs)

 

Prox-TechnologyDiagram-01.png

 

 

Hardware Block Diagram

Block diagrams showing topology for the 3 remotely managed networks in the demo.

Networks can be managed locally via the Gateway or remotely via web interface to the cloud.

DOC-103189.png

 

Software Block Diagram

AirSync™ Agent SDK

Proximetry’s AirSync™ Agent software development kit enables IoT solutions developer to quickly integrate our advanced network management solutions into their devices and application. The development kit provides code examples of several small footprint remote client applications (20KB – 4KB) with fully-integrated application level messaging. The AirSync™ Agent SDK is provided in source code format in C, Java (SE, ME), JavaScript, and Python. The high level software architecture of the Agent SDK is shown in the figure below.

 

Contact Proximetry to download the AirSync™ Agent SDK.

 

Prox-ClientSDKDiagram-01.png

 

 

Connectivity Block Diagram

Block diagrams showing Connectivity details for each of the 3 networks.

All 3 networks currently implemented with Ethernet connection to WAN.

3G/4G WAN connectivity is also possible but hasn't been implemented yet in these networks.

DOC-103189-2.png

Full Listing of Products/Components

Note: For full listing or additional information for Products/Components used in this demo see "This Demo's IoT Highlights" and "Additional Products/Components" in the left hand column of this page. Note: If you aren't viewing this demo in the IoT Solutions Center, please use below link to access the full description in the IoT Solutions Center:

Proximetry Multi-Network High Density Node Gateway Demo

Attachments

    Outcomes