The i.MX 6 D/Q/DL/S/SL Linux L3.0.101_4.1.1 Patch release is now available on [www.freescale.com]www.freescale.com
· Target HW boards
o i.MX6DL SABRE SD board
o i.MX6Q SABRE SD board
o i.MX6DQ SABRE AI board
o i.MX6DL SABRE AI board
o i.MX6SL EVK board
This patch release is based on the i.MX 6 Linux 3.0.35_4.1.0 release. The purposes of this patch release are as follows:
· To fix the BSP multimedia GPU bugs
· To upgrade the Linux kernel to v3.0.101
· To upgrade the multimedia library
· To upgrade the GPU driver and library to 4.6.9p13
Please consult the release notes for more details.