Known issue: STB GUI for eCompass kits returns error when using without Adobe Flash Player + ActiveX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Known issue: STB GUI for eCompass kits returns error when using without Adobe Flash Player + ActiveX

Known issue: STB GUI for eCompass kits returns error when using without Adobe Flash Player + ActiveX

Issue


Using the STB GUI for eCompass kits RD4247MAG3110 and RD4247FXOS8700 only -- v6.1.0.1 on a machine that does not have the Adobe Flash Player ActiveX program installed may run into the following error after pressing the eCompass button:


STB GUI error.JPG.jpg


Solution


Install the Adobe Flash Player + ActiveX from Adobe.



Let us know if you are facing any other issues with the STB GUI v6.1.0.1.


Regards,

Tomas


Labels (1)
No ratings
Version history
Last update:
‎08-20-2014 07:20 AM
Updated by: