G5 Engineering: IP Camera Solution based on the i.MX 6 Applications Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

G5 Engineering: IP Camera Solution based on the i.MX 6 Applications Processor

G5 Engineering: IP Camera Solution based on the i.MX 6 Applications Processor

G5 Engineering demonstrates an IP camera solution based on i.MX6 apps processor at the FTF Americas 2014.

 


Features

  • Multiple IP cameras that are aggregated by one i.MX6 and then sent over an IP backhaul to a second i.MX 6 for integration into a single image
  • The images are brought out to the screen. No need to use Windows reducing virus instances
  • With a click of a button can change the display to 1x1 or 1x2 to 4x4 views

Featured NXP Products


Links

Labels (1)
No ratings
Version history
Last update:
‎07-11-2014 08:49 AM
Updated by:
NXP Employee