DDMS for Screen Capture i.MX51

Document created by Masaki Hayakawa on Jul 7, 2014
Version 1Show Document
  • View in full screen mode

Hi,

I have a custom board with lcd of 18bit rgb color, and 240x320 resolution.
OS is Android.
DDMS command of Android SDK captured screen, and ddm_screenscapture-2014-07-08.png outputed.
The gralloc library supported 240x320 for DDMS ?
LCD display is work (20140708.jpg).

 

logcat

I/imx5x.gralloc( 2207): id       = DISP3 BG
I/imx5x.gralloc( 2207): xres     = 240 px
I/imx5x.gralloc( 2207): yres     = 320 px

I/imx5x.gralloc( 2207): xres_virtual = 256 px

I/imx5x.gralloc( 2207): yres_virtual = 1152 px

I/imx5x.gralloc( 2207): bpp      = 16
I/imx5x.gralloc( 2207): r        = 11:5
I/imx5x.gralloc( 2207): g        =  5:6
I/imx5x.gralloc( 2207): b        =  0:5
I/imx5x.gralloc( 2207): width    = 38 mm (160.421051 dpi)
I/imx5x.gralloc( 2207): height   = 51 mm (159.372543 dpi)

I/imx5x.gralloc( 2207): refresh rate = 59.71 Hz

I/FslOverlay( 2207): /dev/graphics/fb0 fb_var: bits_per_pixel 16,xres 240,yres 320,xres_virtual 256,yres_virtual 1152

 

Best Regards,

Masaki Hayakawa.

Outcomes