Secure Tunnel Offload from WLAN AP to Switch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure Tunnel Offload from WLAN AP to Switch

Secure Tunnel Offload from WLAN AP to Switch

This demo will provide three modes to show the CAPWAP offloading capability of QorIQ platform. mode Iis the core-through mode which can be implemented by the CAPWAP stack to send the CAPWAP stack packets; Mode II is the offloading-mode which demonstrates the CAPWAP Encapsulation/De-capsulation capability of the SoC, and can be used in the AC case; Mode III is the net-bridge mode which is the basic usage for EAP which bridge the packets from PCIE to SEC and FM for offloading CAPWAP manipulation, the bridge is zero-memory copy in order to get high performance data. Together with the throughput data, this demo will help the customer to evaluate the EAP design with QorIQ platform.

 

Features
  • QorIQ T1 processors handle secure WLAN tunnels with offload engines instead of CPU cycles
  • CAPWAP tunneling firmware performs extra tasks (frag/ reassembly) and interfaces to the Linux user
  • Highly efficient bridging to WLAN radios ensures maximum WLAN performance
  • CAPWAP fragmentation and reassembly

Featured NXP  Products


Block Diagram
13161_13161.jpgCapture.JPG.jpg
Labels (1)
No ratings
Version history
Last update:
‎07-07-2014 03:41 PM
Updated by:
NXP Employee