Flying glasses demonstrator: Dual PMSM demo uses Qorivva MPC574xP and features spinning glasses mounted on the rotor of a first motor, while the second motor is equipped with a blade, "cutting" the glasses. Four glasses are mounted on the shaft of one motor while it is spinning. The second motor is running at the same time and it turn its propeller in a predefined movement so there is no damage to the glasses.
https://community.nxp.com/players.brightcove.net/4089003392001/default_default/index.html?videoId=43...
Features
- Permanent magnet Synchronous Motors
- Sensor used for speed and positioning measurement
Featured NXP Products
Training