Exercise 3: Toggle all 4 LEDs on the K60 Tower using the PIT0 as ROM version

Document created by peterurbanek on Mar 17, 2014
Version 1Show Document
  • View in full screen mode

To do:

 

Implement a program that lets the 4 LEDs on the Tower toggle all together using the PIT Interrupt.

This time, let the program run in the Flash.

 

* toggle period 0.5 s

* extract vector table and service routines in 'vector.c'

* Change the linker command file 'ldscript_flash'

* Take care of the 16 Byte security settings from $400-$410 in the Flash. Do not overwrite!!!

 

Hint: Use the 'arm_cm4.c and 'arm_cm4.h' from the freescale kinetis homepage, which include access functions for the NVIC.

For ease of use, these routines are included in the result file.

 

Result: TWR_K60_PIT0_Flash.zip

Attachments

Outcomes