To do:
Implement a program that lets the 4 LEDs on the Tower walk like this:
* a single LED from left to right,
* then the two left ones, the two right ones,
* the two outside and at least the two LEDs in the middle.
For easy observing write a wait routine, called 'delay (unsigned int ms)', of about 1 second without using any library functions. The processor will start with the standard frequency of 20...25 MHz. Estimate the time, that a loop needs to realize the time.
Hint: Do not forget to stop the Watchdog Module at the beginning.
Result:TWR_K60_Lauflicht.zip including a readme with the compiler options