• RT-Thread移植到KV56

    请问有没有RT-Thread移植到KV56系列上的资料呀?
    Deng Shuntian
    last modified by Deng Shuntian
  • The FRDM-KW36 can't connect with smart phone

    Hello All ~              I have used the button to config the FRDM-KW36 as a peripheral device for to connect to the smart phone. Although the smart ph...
    sihan chen
    last modified by sihan chen
  • i.MX 6/7 DDR Stress Test Tool

    Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private mess...
    Oliver Chen
    last modified by asimzaidi
  • How to configure QN908x for the continuous SCAN mode? And to scan more than ten devices.

    How to configure QN908x for the continuous SCAN mode? And to scan more than ten devices. We tried to test this feature [always scan mode] using Wireless UART (freertos version) example code - where we commented...
    Kishan Saralaya
    last modified by Kishan Saralaya
  • Race condition in MCUXpresso USART Driver

    The code contained in fsl_usart.c driver contains a race condition on transmit.  The error will occur in systems that have non-blocking transmit and receive happening simultaneously.   Starting at line 588 ...
    otsl
    last modified by otsl
  • Init task is stuck on xQueueSemaphoreTake()

    I am using FreeRTOS to run some tasks in my software on S32K144 board . Currently my init task is getting stuck on xQueueSemaphoreTake() function in Queue.c When I start my program the program runs for a while and the...
    Chandrika Joshi
    last modified by Chandrika Joshi
  • PTN5110 sourcing high voltage

    Hi there,   We have PTN5110 and would like to know how to source high voltage (more than 5V).    From the datasheet. it seems that if you want to support higher voltage, you need to use the EN_SNK1 pi...
  • Embedded source code for WCT1011A Automotive MP-A9 Wireless Charging

    Hello NXP support,   How can I download embedded source code for MP-A9 Wireless Charging? I'm using Freemaster but I can't see the directory location for them! (I'm working on a project and I need to evaluate t...
    MAHMOOD ALFAHQERI
    last modified by MAHMOOD ALFAHQERI
  • [ZGWUI tool] Usage of Read Attrib of General Tab?

    Dear Sirs,   About GUI tool of "ZigBee Gateway User Interface", how to set the parameters for "Read Attrib"?   Thanks!
    alan lin
    last modified by alan lin
  • Embedded source code for WCT1011A Automotive MP-A9 WPC

    Hello Everyone,   Would you please explain to me how can I download embedded source code for MP-A9 Wireless Charging? I'm using Freemaster but I can't see the directory location for it! (I'm working on a project...
    MAHMOOD ALFAHQERI
    last modified by MAHMOOD ALFAHQERI
  • MCUXpresso Config Tools V7.0 -- WDTT Configuration Bug

    Using LPC802M001JDH20   As configuring the WDTT, even though everything (including clocksource and frequency) in Config Tools software is specified;   Config Tools provides the following inside peripherals...
    Arda Otuz
    last modified by Arda Otuz
  • WPR1500-BUCK

    Hi   How to test the efficiency of wireless charging?
    liven deng
    last modified by liven deng
  • i.MX 8M Family DDR Tool Release

    Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private mess...
    Oliver Chen
    last modified by asimzaidi
  • NEW LPC1769

    I downloaded LPCXpresso on Mac (and windows 10). However, on both operating systems it says "emulator cannot be found" when I run debugging. I've tried reinstalling the program, unplugging, and powering on/off. I've s...
    Anna Young
    last modified by Anna Young
  • Not able to connect with MKE15Z using J-Link

    Hi All, I am new to NXP and Cortex based Micro-controllers, and working on a project. Everything was working fine, but I think I messed up a setting in the project and due to which I am not able to connect with my bo...
    xpress-embedo
    last modified by xpress-embedo
  • QN908x in FIDO2 USB Token

    Would like to know whether anybody used QN908x Controller as a FIDO2 USB/BLE  MCU. Kindly let me know if there is any limitation with respect to the FIDO Use case implementation perspective. 
    Kishan Saralaya
    last modified by Kishan Saralaya
  • Uart transfer or interrupt

    Hello all.   I have been working on a project with 4 UARTs. One of them will be used to transfer some data to external devices and receive some answers. However, the answers can have different sizes. I am try...
    Marcos Chiele
    last modified by Marcos Chiele
  • MIMXRT1064-EVK OpenSDA fails to run

    Hello everyone,   I have been playing with a MIMXRT1064-EVK for a few weeks now and suddenly, I'm not sure when and what I was doing at that time, its on-board OpenSDA debbuger lost its ability to run a program ...
    Marco Haddad
    last modified by Marco Haddad
  • MK22 USB HID transfer packet speed

    Hi,   I imported the generic HID example using MCUXpresso IDE, and changed the interval time to get the maximum theoretical transfer speed of 1000packets/s:   #define HS_HID_GENERIC_INTERRUPT_OUT_PACKET_SI...
    Bernat Albet
    last modified by Bernat Albet
  • PMSM Motor Parameter Measurement -> JScript Error?

    cliHello,   I am in the process of doing some fine tuning on some custom hardware and motors.  Sometime back I had used the Motor parameters measurment utility in the MCAT pmsm_ref_sol.pmp application from ...
    Frank Roberts
    created by Frank Roberts