• Using I2C api in uboot with 7ulp

    Hi,    I am using uboot from official repository Aurora : uboot-imx - i.MX U-Boot  Tag : rel_imx_4.14.98_2.3.0   I am using the mx7ulp_10x10_arm2 defconfig.    I would ...
    Arthur LAMBERT
    last modified by Arthur LAMBERT
  • S32k144-Problem about PWM output of FTM

    I want to output one PWM signal with 4000hz,50% duty cycle. I modify on the official  demo "ftm_pwm" ,the SDK is RTM3.0.0. I change the PE  configuration of PWM to "Edge-Aligned PWM" . ...
    qh c
    last modified by qh c
  • S32K VLPS mode entry and exit

    Hello all,         I have followed the Power management AN5425 pdf provided by Nxp for Power mode and exit  s32k116.      I have done for RUN to VLPS mode ...
    umesh shinde
    last modified by umesh shinde
  • S32K144 The number of CAN send/receive at once

    Hello,   I'm developing High-CAN/CAN-FD application with S32k144. The app sends and receives 22 can/can-fd data with different ID at once. Meanwhile, two CAN-FD data has to send but it hasn't while other high-ca...
    Soonhwan Jung
    last modified by Soonhwan Jung
  • iMXRT1021 flexspiNOR unable to use HAB Encrypted XIP

    Hi, I am using the iMXRT1021 with flexqspiNOR flash. We want to encrypt the .sb image and the use on-the-fly BEE decryption. I am using the elftosb.exe, sdphost and blhost to produce and flash the .sb image. ...
    Tony Thurgood
    last modified by Tony Thurgood
  • ISI Channel busy when use Maxim  9286

    Hi NXP,       When I use Maxim 9286 cameras on IMX8QM Android Platform, I found that the ISI Channel[0] busy problem. so the video0 of Maxim 9286 can't work.  the kernel the following error: ...
    yingjin yan
    last modified by yingjin yan
  • iMX8QM DDR Configuration

    Hi,   I would like to understand how to configure DDR for iMX8QM system. Our board has 8Go of DDR4 which is more than the iMX8QM MEK board.   How to configure the system to indicate additional RAM to init...
    Stan Bertrand
    last modified by Stan Bertrand
  • MPX5999D processing issue

    Hello NXP engineers,   This is Sunny from Plexus China, need your help to check below issue, please kindly give feedback asap, thanks first.   Your part MPX5999D is used for our customer new product, and c...
    Sunny Gao
    last modified by Sunny Gao
  • MATLAB Toolchain to program MPC5744P Custom Hardware

    Hello, I am designing a custom hardware(MPC5744P) compliance with MATLAB Target Hardware. I bought a DEVKIT-MPC5744P. Thanks to On-Board Debugger(OpenSDA), I am able to directly program DEVKIT-MPC5744P from...
    Samet Can Biçer
    last modified by Samet Can Biçer
  • NXP Simulink library for MPC5777C

    Hello,   I have been trying to use the CAN communication and ADC blocks with MBD_MPC574x_Config_Information block by selecting MPC5777C microprocessor but the CAN and ADC blocks shows the following err...
    Raman Nain
    last modified by Raman Nain
  • IAR "Fatal error: Failed to connect to CPU" MIMXRT1060-EVK

    After flashing a program with a possibly bad linker file to this board, my debugger can no longer connect to the processor. I read that some MCUs have an ISP mode where it allows the debugger to take control again. I ...
    Nicholas Sohacki
    last modified by Nicholas Sohacki
  • Bug in lpspi driver?

    Hello,   I was just testing the LPSPI driver and realized that the clock cycles in register LPSPI1>SCKPCS, PCSSCK and DBT get set wrong. I think there is a bug in the function LPSPI_MasterSetDelayTimes of the...
    Stefan Mitterhauser
    last modified by Stefan Mitterhauser
  • ADC output voltage

    Hello I work with a MKE18F512 and I have to use the ADC. We work with 5V Supply and a external 5V Ref Now I have the problem that the any ADC pin is at 2,5V and delivers up to 20µA out current. Could this be ...
    Tobias Härter
    last modified by Tobias Härter
  • s12g128 MSCAN filter dose not work properly

    Dear: Thanks for your attention! I have set s12g128 MSCAN in filter mode , there are two can id should be received,  id0 = 0x280, id1 = 0x1A0 , CAN filter configration as four 16bit mode , filter0 receive 0x2...
    gao qiang
    last modified by gao qiang
  • S32 Design Studio for Power Architecture have some bug.

    Hello.  Currently, I use S32 design studio to development MPC5746B.   But, I have some trouble.   To explain my current development environment(Processor Expert).   1. Add Can_pal (Ch0 ~ Ch2) ...
    lim sunghyun
    last modified by lim sunghyun
  • Derivative could not be unsecured

    Hello, i am trying to upload my first code in devkit-s12xe i am using code warrior v5.2 which is running in a 32bit windows 10 which is running on a VM inside a linux system. i am using "Lab2_ADC_PWM_S12XE.mcp" examp...
    Ankit Sultania
    last modified by Ankit Sultania
  • How to select external Oscillator using processor expert in S32DS project

    I am new on the processor expert and NXP 32bit MCUs. I want to select only the external oscillator in the clock setting.     How can I configure the external oscillator and then PLL system clock should...
    kashif sagheer
    last modified by kashif sagheer
  • Processor Expert sees less RAM on MK22FX512VLH12 than specified

    According to the product page (MK22FX512VLH12 Product Information|NXP) data sheet (https://www.nxp.com/docs/en/data-sheet/K22P64M120SF5.pdf) and reference manual (http://cache.freescale.com/files/32bit/doc/ref_manual/...
    Paul Kathol
    last modified by Paul Kathol
  • The mail list URL for yocto project is invalid

    should be updated to meta-freescale@lists.yoctoproject.org | Home 
    peak p
    last modified by peak p
  • Softreset not working if executing from OctalSPI flash

    Hello, I am using the embeddedartists imxrt1062 board which has the adesto ATXP032 as serial octal NOR flash. My application is burned into the NOR flash and is starting well at Powerup. Now I encounter the follo...
    Werner Kullmann
    last modified by Werner Kullmann