• SDK - how to config ADC input pin/channel ?

    I am looking for an example to proper initialize an input channel for the ADC (LPC54628). The usual way is to enable the appropriate GPIO pin, and assign the proper function (analog mode). All of the SDK examples us...
    frank meyer
    last modified by frank meyer
  • LSDK 20.04 build tensorflow with error

    How to build tensorflow without error with LSDK 20.04? flex-builder docker source setup.env flex-builder -c tensorflow   WARNING: /root/.cache/bazel/_bazel_root/e049e4c8f6a02b9cc6ec49b509d262b1/external/grpc/BUI...
    Mason Yen
    last modified by Mason Yen
  • MC33771

    Hi sir, In MC33771 how to differentiate charging and discharging of the battery?   Regards, Veeraju V Hallikeri
    Veeraju Hallikeri
    last modified by Veeraju Hallikeri
  • Can anyone explain what is Ethernet Independent Mode in LS1046A and at what cases it is used?

    Can anyone explain what is Ethernet Independent Mode in LS1046A and at what cases it is used? 
    Aravind kumar Navuluri
    last modified by Aravind kumar Navuluri
  • The error between the estimated position Angle with Luenberger observer and the actual position Angle

    hello!!! When the Lombergo observer is used, the Angle estimated by the observer differs from the real Angle by 180 ° sometimes,In this case,The closed loop will fail.I modeled and simulated the algori...
    董培 董
    last modified by 董培 董
  • NxpOpenBus.exe under unified_bootloader_framework

    From user manual - UBLUG.pdf in unified_bootloader_framework of S32K: 32位汽车通用MCU | NXP  There is a tool named NxpOpenBus.exe to programming via bootloader.  How can I download or find t...
    Gary Lu
    last modified by Gary Lu
  • KW37_38_39 Minimum BoM Presentation.pdf

    This guide describes the hardware for the KW38 minimum BoM development board. The KW38 Minimum BoM development board is configurable, low-power, and cost-effective evaluation and development board for application prot...
    Christophe Menard
    last modified by Christophe Menard
  • Downloading binary to SDCARD(SD4 Slot) using MfgTool on the MCIMX6SX-SDB board

    Hi,   I'm using MfgTools in Windows 10. The MfgTool_MultiPanel(Library: 2.7.0) was performed by executing the mfgtool2-yocto-mx-sabresd-sdcard-sd4.vbs of L4.9.88_2.0.0_mfg-tool. LOG : MfgTool_Initial.log ...
    DongHyun Kim
    created by DongHyun Kim
  • NFC active pairing for audio devices

    This post entry provides a detailed description of how to develop an NFC pairing solution for audio devices. For that, we will describe in detail an audio speaker prototype made by NXP. This post entry has been struct...
    Jordi Jofre Mk
    last modified by Jeremy Geslin
  • Can not loading the Tresos(v24) WorkSpace.

    My PC's OS is windows 10.  I installed tresos v24.0.0 tool.but it can't be loading when i open the tresos_gui.exe , with always stay in loading view.    And the window task manager sho...
    guoqiang zhu
    last modified by guoqiang zhu
  • How to force USB1 peripheral to only use full speed?

    I was wondering if there is a way to force the USB1 peripheral in device mode to only use full-speed operation.  I understand normally the host signals this, and the USB1 peripheral is capable of using full-speed...
    Conor Patrick
    last modified by Conor Patrick
  • LPC55S69 PLL1 does not function

    Hi     I am trying to use the inbuilt Clocks tool within MCUXpresso to configure the clocks for the FROHF96 functional group, for the LPC55S69EVK board.  I want to use PLL1 with the SD card, so I can r...
    Rory Hand
    last modified by Rory Hand
  • Autosar

    Hi, I am working on Autosar, can anyone help me to know which tools to be use to generated code for different layers of Autosar.
    Ajay Singh
    last modified by Ajay Singh
  • Bootstrap capacitor (Cbs) Precharging

    Hi all,   I am referring MC9S12ZVM-Family RM.(Rev 2.13) In the chapter 1.13.8.2.1 Bootstrap Precharge   The below chunk of data :  *********************************************************...
    PRATIBHA SURABHI
    last modified by PRATIBHA SURABHI
  • I.MX 7 ULP/Solo datalogger use

    I'm new to I.MX processors and only familiar with Beaglebone black (AM355x). But i'm looking for a 'upgrade' to the BBB, any idea how the 7(ULP/Solo) compare? It's a core A7 compared to core A8 but a much newer design...
    Michiel TJampens
    last modified by Michiel TJampens
  • Create Crypto Object: error 0x6985 (conditions not satisfied)

    I have been working with the SE050ARD for a few months now without problems.   Doing some code cleanup I enabled the option SSSFTR_SE05X_CREATE_DELETE_CRYPTOOBJ. After this, I can no longer function s...
    Jorge Ramirez Ortiz
    last modified by Jorge Ramirez Ortiz
  • P2020,TESC3 can not ping

    Hi    Thank to answer this question。    There are some problem about the chip P2020,I using 2 ETH PHY in this project,which using in TSEC1 and TSEC3。TSEC1 is no problem and it can ping ...
    Lu Yingyu
    last modified by Lu Yingyu
  • T1022 Antipads.

    I am using T1022 in my design, I want to know what size of antipad will i use on DDR4 DQS lanes and Clock lanes. and also on PCIe and SGMII lanes. Is 28 mil antipads is right?
    RAM PAL SINGH
    last modified by RAM PAL SINGH
  • AppWizard - floating point not supported?

    Hi I would like to use AppWizard to build a GUI for a sound analysis application I'm working on. I see in your tutorials that I should disable floating point to get AppWizard to work. But I need floating point arithm...
    Torbjörn Johansson
    last modified by Torbjörn Johansson
  • How to calculate sleep timings in i.MX6solo processor

    Hello Sir/Madam,   In our custom board we are using processor i.MX6solo(MCIMX6S6AVM10AC), i need to keep this device for sleep mode so i need to know how long it can be in sleep mode.  If you any calculati...
    Ramesha S P
    last modified by Ramesha S P