• NXP Simulink library for MPC5777C

    Hello,   I have been trying to use the CAN communication and ADC blocks with MBD_MPC574x_Config_Information block by selecting MPC5777C microprocessor but the CAN and ADC blocks shows the following err...
    Raman Nain
    last modified by Raman Nain
  • git.freescale.com down

    We noticed this morning our builds started failing. Looks like attempting to clone firmware-imx is failing.   When I try to clone the repo independent of a yocto build I see the following output:   git clo...
    Adam Bader
    last modified by Adam Bader
  • Is git://git.freescale.com down? fetch error

    After below commands $ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland $: bitbake fsl-image-qt5-validation-imx  Getting error@Git.freescale.com  Carlos_Musich ERROR...
    Rajath Kumar Divakar
    last modified by Rajath Kumar Divakar
  • ETPU crank tooth period (TCR1) to RPM conversion

    Hi, I am using the standard ETPU engine control library (AN4907SW or NXP etpu function generator site) decoding a 35-1 teeth with no CAM function and therefore engine cycle is 36 teeth (1 revolution). T...
    Turgay Kale
    last modified by Turgay Kale
  • ADC/GPIO/Clock Startup Stumper

    Came across an interesting issue and currently not satisfied with the "fix" performed. Some background, during testing of the MKEAZ128 chip a custom control board an issue was found that seemed to be an issue with the...
    cody hubman
    last modified by cody hubman
  • FTP and flash file system for RT1020?

    Hi,   What is the best way to get a file system set up in flash? For example, the RT1020-EVK has an 8MByte flash, and I would like to set up a flash FS that allows FTP access (via ethernet)?   I am l...
    rshipman
    last modified by rshipman
  • what is imx8 core base for jtag ~~Help

    for jtag openocd   I get BSDL file for i.MX 8M (REV 1)   it's 0x1cf80553 for sjc_tapid # System JTAG Controller if { [info exists SJC_TAPID] } {         set _SJC_TAPID ...
    jesse stone
    last modified by jesse stone
  • eIQ Software Clinic - Worth your time? (poll)

    Please let us know how you feel about this software clinic. 
    Megan Hansen
    last modified by Megan Hansen
  • What additional ML training/support do you need?

    What ML capabilities would you like to see MORE training or support on?
    Megan Hansen
    last modified by Megan Hansen
  • RFID/NFC tag

    Hello everyone,   I'm looking for a RFID/NFC tag chip able to interract with classic RFID readers (ISO14443) and NFC readers (ISO15693) and who can transmit differents datas depending on the technology used by t...
    simonschmitt
    last modified by simonschmitt
  • Altium,  i.MX 8M EVK

    Hello Yuri, Could I please have these files for use in Altium as well? Or is there a direct link to download? Thanks very much, Scott F
    Scott Foster
    last modified by Scott Foster
  • I can't install freemaster 3.0

    Hi, I'm having some difficulties installing freemaster 3.0.   A installanywhere window appears after I double click FMASTERSW30.exe. After its completion bar finishes, a window with the freemaster logo appe...
    gean sousa
    last modified by gean sousa
  • Connecting LS1043ARDB through UART serial connection on CodeWarrior

    I have a 1043ARDB and I want to establish a connection with it through CodeWarrior using the serial connection with the RJ45 to DB9 cable on the UART1 port and I am having some issues with it. I can connect and commun...
    Franklin Turner
    last modified by Franklin Turner
  • Install svc function

    How to install an svc function to call a specific svc handler in for S32K148?
    Smruthi Ramesh
    last modified by Smruthi Ramesh
  • Connect PCAL6524HE center slug to ground?

    On the footprint for the PCAL6524HE I/O expander, should the center copper slug on the HUQFN package be connected to ground or left floating?  It doesn't state explicitly what to do in the manual.
    bill von novak
    last modified by bill von novak
  • How to transmit continous data from FRDM-KW41ZMCU to ble device (NXP IOT toolbox is app)?

    Hello, I am trying to transmit a "Hello\n" message from FRDM-KW41Z MCU to NXP IOT Toolbox (wireless uart). But i am not able to receive any message. I am using demo example - "BLE-wireless uart" , wireless uart ...
    Pooja Vernekar
    last modified by Pooja Vernekar
  • EDP implementation on  i.MX6( ULL)

    Hi NXP and Community friends!   I have a question about EPD implementation on i.MX6(ULL) and hope to you can help me find answer for my question below.  In terms of EDP implementation on  i.MX6xx, ...
    Musadjan Alim
    last modified by Musadjan Alim
  • i.MXRT160EVKDS

    i need Altium version PCB and schematic files of Evaluation Board i.MXRT160EVKDS because we don't have Allegro PCB and integrated your CPU in a new project. Thx. Regards
    Paolo Chiesa
    last modified by Paolo Chiesa
  • How to burn emmc image by uuu

    Please tell me about uuu. I tried to burn image for i.mx6q board by uuu, but It is a situation that is stopped in the following situation. >uuu -b emmc_all bootloader rootfs.sdcard.bz2/*uuu (Universal Update Utili...
    takuroh yoshida
    last modified by takuroh yoshida
  • Using NXP(Freescale) VID and PID

    Hello. I am developing my commercial product that will have a USB-CDC communication protocol. I do not want to pay $5000 for my identifier. According to this, I have several questions: Can I use Freescale's VID 0x25...
    Evgeni Kosakovski
    last modified by Evgeni Kosakovski