• 关于RT1064官方MDK工程的一些问题

    我在使用RT1064 SDK中的hello world的MDK工程时,遇到了两个问题: 1.无法使用__weak关键字,如图 2.下载时出现下面的问题: 请问该如何解决
    陈 文龙
    last modified by 陈 文龙
  • variables got question mark when integrate with serial driver v3 for S12zVM

    Hi there, I have some code working with freemaster serial driver v2. I am integrating the driver v3 from https://community.nxp.com/docs/DOC-345150. I still need to use poll mode but all the variables gave me question ...
    Ke Li
    last modified by Ke Li
  • Android P9.0.0_2.2.0-ga booting issue with i.MX6 Solo

    Hi community,   Has anyone ever booted in 6Solo mode with i.MX6DL SABER-SD? I am trying to boot android p9 as i.MX6Solo mode using i.MX6DL SABRE-SD board. But  after booting u-boot, kernel don't boot-up a...
    Mamoru Kanou
    last modified by Mamoru Kanou
  • HAL library for S32K146/144 MCU?

    How can we use HAL library for S32K146/144 MCU?as I have learnt STM32F4 Discovery using HAL library, so it would be easy for me. currently, I am using S32Design Studio for ARM for coding in S32K146?
    Shivam Gupta
    last modified by Shivam Gupta
  • iMX8M Mini / IoT Core: power management support?

    Greetings, we're evaluating power management capabilities of NXP's Windows 10 IoT Core BSP for iMX8 Mini EVK (W1860_1_0_1_IMX-IOTCORE-B191011). Power management is claimed to be supported, but powercfg reports on...
    Gennady Kuznetsov
    last modified by Gennady Kuznetsov
  • Ventilator design (DRM127) - software

    I'm looking at https://www.nxp.com/applications/solutions/industrial/healthcare/ventilators-and-respirators:VENTILATORS-RESPIRATORS I got the DRM127 document from the website which provides design specification for V...
    Ramakanth Kona
    last modified by Ramakanth Kona
  • fsl-image-validation-imx-1.0-r0 do_rootfs: Could not invoke dnf

    Hello experts,   I'm building the fsl-image-validation-imx image using fsl-yocto-L4.9.123_2.3.0_mx8mm under Ubuntu-16.04 :   $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-li...
    Khang Le Truong
    last modified by Khang Le Truong
  • tinyalsa: pcm_open failed cannot open device '/dev/snd/pcmC2D0c'

    I am trying to implement an Android Application where it makes use of tinyalsa: pcm_open() API.  I get "cannot open device (0) for card(2): Permission denied" error when I tried to launch the application fro...
    Kyaw Naing
    last modified by Kyaw Naing
  • How to enter SNVS mode by SW on imx7d?

    Hi!   According to "i.MX 7Dual Applications Processor Reference Manual, Rev. 1, 01/2018"  part 5.1.4.4 "Power Modes" there are two ways to enter "SNVS" mode  from "RUN" mode: ONOFF long press, or SW. ...
    Pawel Lenkow
    last modified by Pawel Lenkow
  • SC18IS602B I2C bus to SPI bridge Chip Select Function

     Hi, I want to interface SC18IS602B with DAC AD5504. For this Chip Select has to toggle(low to high) after 16bits of data is transmitted. What is the behavior of Chip Select pin on SC18IS602B? Will it toggle fro...
    Shreya S
    last modified by Shreya S
  • Command Line utility command for MFGtool2  to display the result and exit the command prompt.

     I am using the MCIMX6Y2DVM microcontroller in my testing board, I am programming this controller manually using MFGtool2.exe. I want to automate the programming for my project. I am using LabVIEW an industrial a...
    M Harishankaran
    last modified by M Harishankaran
  • EBTresos tool installer issue

    my computer can't install EBTresos(EBtresosStudio_EBtresosStudio) tool, how to fix it.
    guang chen
    last modified by guang chen
  • Continuous noise issue during VOIP call

    Hello, I'm working on IMX8M Mini EVK with Android Pie (p9.0.0_2.3.0) OS. I have integrated CX9000 synaptics audio amplifier and CX20921 Dual MIC voice processor to the EVK.   There are two DMICs connected on ...
    Naman Thaker
    last modified by Naman Thaker
  • Autosar with Imx8/Imx6

    Hello Team,    I am planning to use the Imx8/Imx6 for integrating the Autosar. Could you kindly let me know on how to proceed with this. If i purchase the development board, will this come with the Autosar...
    Naveen B
    last modified by Naveen B
  • No response from OV5640

    Hello, I am making a program that uses MINISASTOCSI (OV5640) and cortex-M4 to communicate by I2C with iMX8MminiEVK. However, I cannot confirm the response from the I2C camera. The I2C driver uses MCUexpressoSDK (SDK_2...
    Tetsuya Sugiyama
    last modified by Tetsuya Sugiyama
  • rm67191 Driver

    IMX8M平台 linux系统    rm67191的配置: static const struct display_timing rad_default_timing = { .pixelclock = { 66000000, 132000000, 132000000 }, .hactive = { 1080, 1080, 1080 }, .hfront_porch = { 20, 20, 20 }...
    tan yd
    last modified by tan yd
  • Help with proximity sensor

    Looking for some advice. I want to use tags (preferably without any anchors) to build a proximity detector. Such that, each tag vibrates or sends a GPIO output when it gets within a certain range of any other tag. ...
    Mike Jopson
    last modified by Mike Jopson
  • Digest Operations using SE050

    Hi Guys,   I have an input string say 1000 chars long and I'd like to generate a hash value for it. I initially used the DigestOneShot function by sending in the input string by chaining them. Unfortunately ther...
  • iMX8MM-EVK LPDDR4 not work

    Hi guys,   I'm used sample iMX8MM-EVK pcb from NXP to make a board, 100% like iMX8MM-EVK.   When I using MSCALE_DDR_TOOL version 310 to test LPDDR4. Calibration and street test OK. Result is attached bello...
    Kieu Dich
    last modified by Kieu Dich
  • onnxruntime fetch fail

    Hi All Right now ,i am try to build the new yocto bsp 4.19.35 to generate the eiq for our algorithm development , but i encouter the issue showed below .   bitbake imx-image-full     WARNING: onnxrun...
    King Liu
    last modified by King Liu