• SLN-VIZN-IOT driver

    我使用你們的SLN-VIZN-IOT ,可是serial portㄧ直連接不起來,我安裝了 MCUXpressoIDE_11.1.1_3241.exe 也找過 SLN-VIZN-IOT Software Collateral v1.0.3 SLN-VIZN-IOT Hardware Package v1.0 這裡都沒有driver,想請問ㄧ下這塊版子的driver要去哪下載? 或是可以直接提供給我
    YI HUA WANG
    last modified by YI HUA WANG
  • Simple PWM pulse string on KEA128

    I'm having an issue getting this to work on a FRDM-KEAZ1284Q80 evaluation board. I'm attempting to make a simple unending pulse train of square waves at 1kHz. It does make pulses but in an odd pattern.  It also ...
    TOM SPARKS
    last modified by TOM SPARKS
  • Issue Writing to Vector Table on KE/KEA

    DEVICE:   KE06/KEA128  (two examples of each were tested)   To begin, I checked the value of VTOR and it reported the value of '0' for the offset.  I took this to mean the table is not ...
    TOM SPARKS
    created by TOM SPARKS
  • Flash driver with MQX

    Hi support:   In my project I need to store data on K70. I want to use an external serial flash memory. Is there any demos available for MQX? or any driver for SPI interface?
    Andy C
    last modified by Andy C
  • In I.MX28 BSP, USB AUTOMOUNT IS NOT WORKING in I.MX28 EVK

    Dear I.MX Community,     USB automount is not working.. when I plugged the USB device onto I.MX28  EVK, as am stuck with this issue from long time, could any body please do the needful in resolving thi...
    srinivasan shanmugam
    last modified by srinivasan shanmugam
  • Can't delete terminated debug sessions

    I copied/reloaded a couple of projects coming from MCUXpresso 10 into a new MCUXpresso 11.1.1 workspace, but every time I launch debugger looks like it can't be properly terminated. After that, the only way to start a...
    Luca Matteini
    last modified by Luca Matteini
  • LPC-Link2 with CMSIS-DAP & OpenOCD as Device Flasher

    We have completed development of a product based on the MKL27Z256VFM4 and setup a small programming station with a LPC-Link2 with CMSIS-DAP & OpenOCD. Setting up the LPC-Link2 with CMSIS-DAP went flawlessly. We ar...
    Robert Rau
    last modified by Robert Rau
  • MK20DX256VLH7 Crystal Question

    From what I have read in the reference manual I do not see a method to employ an external oscillator in place of the external crystal (not the 32.768 kHz clock crystal).   If it is possible, would an extern...
    Marv De Beque
    last modified by Marv De Beque
  • gAttErrCodeInsufficientEncryption_c error in client mode

    Hello members, I have 2 boards in my architecture one in client central and one in the server peripheral configuration. These are my pairing parameters of both side gapPairingParameters_t gPairingParamete...
    rahul singh
    last modified by rahul singh
  • SPI data length: Error description in LPC845.h

    In LPC845.h of SDK   The bit discription doesn't match the bit length. In the text it is correct, in the 'table' below not: 0b0001 does not code 1 bit in length. This made me busy for about 25 minutes until I...
    12345 67890
    last modified by 12345 67890
  • PWM pins on ls1021a

    Hi,   I want to add RGB LEDs on my chip and wonder if ls1021a processor does support PWM pins configuration via software pinmux.   If so anyone knows how to set those pins as PWM and access it vi...
    Elias Bitbaker
    last modified by Elias Bitbaker
  • Adding packages under core-image-base image

    Hi All,   I am working on yocto zeus (https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml).I am adding some packages under core-image-base image. I modified th...
    Nikhil sahu
    last modified by Nikhil sahu
  • TJA1145FD With MPC5746R

    Hello, I am currently using TJA1145.I find the examplehttps://community.nxp.com/message/936919?commentID=936919#comment-936919 .However, the function of MPC5746r sending SPI instruction to TJA1145 in this exampl...
    anony lee
    last modified by anony lee
  • Questions about T1042 processor and U-boot

    We have a custom board based on t1042 processor. Using codewarrior rcw override option, We successfully wrote RCW, FMan Ucode and U-boot in given flash locations in SDK V2.0 - 1703 ( Current Bank adresses ).   W...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • [Mikroe NFC USB Dongle] Unable to get the Eclipse C example project working

    Hello, I just bought the Mikroe NFC USB Dongle (with NXP PN7150).  It is provided with a C example software (Here: http://www.nxp.com/documents/software/SW4335.zip). I tested it on Windows 10...
    Marc de V.
    last modified by Marc de V.
  • Java Example for Mikroe NFC USB Dongle (NXP PN7150)

    Hello, I just bought the Mikroe NFC USB Dongle (with NXP PN7150). It is provided with a C example software (Here: http://www.nxp.com/documents/software/SW4335.zip). Do you know if there would be a Java one?...
    Marc de V.
    last modified by Marc de V.
  • flexCan pins for tx and rx

    Hi exports,   When I test nxp-ls1028ardb board, the I did not get the pins of flexCan for tx, rx and ground in docs of nxp-ls1028 including user maunal, reference manual etc.   Would you please give the pi...
    Tang zhantao
    last modified by Tang zhantao
  • IFC and memory stall on multi core

    Hi,   we use the LS1020a QoriQ and have something connected via IFC GPCM ASIC mode. Currently we run into race conditions then independent parts of the software try to read via IFC at the same time. Chapter 24 o...
    Eduard Stefes
    last modified by Eduard Stefes
  • NTAG 5 iOS Development Code

    I could compile the NTAG 5 iOS development source code without any error. I could run the app and NFC card detection without any problem. However, the GetAccelXI2CMaster function is always return 0 byte length as...
    Kevin Chia
    last modified by Kevin Chia
  • ETM Data Tracing

    Hi,   Can anyone help me to find out the NXP products that support ETM (memory) data tracing? Currently, I find i.MX53QSB has such a function. Meanwhile, I demand the products (or the development boards) can run...
    Hao ZHOU
    last modified by Hao ZHOU