• Does CW support an old 9S08QE8CWL?

    I have CW10.6, and need to modify a "WL" package (28 pin SOIC). The only options in CW are for a LC or FM. If I need to upgrade or pay a new license, I will. Any help will be greatly appreciated.
    Rande Newberry
    created by Rande Newberry
  • PN7462 ROM3 functions definition

    Hello, Where can I find a complete definition for the HAL functions mapped in ROM3 ? I have the NXP NFC reader library including the following HTML file PN7462AU-FW_v05.22.01_Full\ApiDocumentation\PN7462AU\PN7462AU...
    Julie Ronday
    last modified by Julie Ronday
  • S32K116 for UART1 switch component lin and lpuart

    We using S32K116 UART1 to implement two function lin and lpuart . How to switch two function component lin and lpuart ?
    Jeffery Huang
    last modified by Jeffery Huang
  • Can you access the UID with the latest iOS13 upgrade without an app?

    We want to move away from using our app, but need the UID for database references. 
    COREY MAITA
    last modified by COREY MAITA
  • MCUXpresso IDE with GNU Tools for Arm Embedded Processors "9-2019q4-major" Release

    Will MCUXpresso IDE be updated to include [GNU Arm Embedded Toolchain Version 9-2019-q4-major]?  If so...when?
    brent.hauck@tempocom.com
    last modified by brent.hauck@tempocom.com
  • Please provide the hardware design application note for LPC822M101JDH20J.

    Application note for LPC822M101JDH20J.
    Muralidhar M
    last modified by Muralidhar M
  • NXP Controller_Hardware_Design

    Please provide hardware design for MKE04Z8VTG4. Application note: For ADC peripheral.
    Muralidhar M
    last modified by Muralidhar M
  • Need Design file

    Hello,   I have go through your product list and find out that MMPF0100 IC is used with Zynq-7020. I am using two FPGA in my project and fro that i am finding power management IC for that. so i want full Schemat...
    nilam trivedi
    last modified by nilam trivedi
  • Application note for MKE04Z8VTG4 32-BIT ARM MICROCONTROLLER

    Hi sir,      Please provide the hardware design or application note for       MKE04Z8VTG4 32-BIT ARM MICROCONTROLLER for desinging details.
    Muralidhar M
    last modified by Muralidhar M
  • First steps with NXP

    Greetings! I am about to work with your mcus for a very first time. I want to use i.mx rt 1020. What is the prefered tool for programming and debugging? Do you have a special tool for manufacture programming? Th...
    Pavlin Stoyanoff
    last modified by Pavlin Stoyanoff
  • Device /dev/apex_comm couldn't be opened!

    Hello everyone,   I have built an demo application in /path/to/s32v234_sdk/demos/apps/pedestrian_detection_aggcf. When I run it on s32v234 board, the error occured like below:     What does it mean?...
    wq y
    last modified by wq y
  • Zigbee coordinator replacement

    I now need to implement a function, that is, when the coordinator is replaced, the data in the previous coordinator can be saved to the current coordinator, so that the coordinator can be replaced, the sub-device does...
    tianheng han
    last modified by tianheng han
  • Does receiving an ack response break sleep?

    Hi I use this function ZPS_eAplAfUnicastAckDataReq on sleep devices.   I found that this function has its own retransmission mechanism.   I want to know if i will go to sleep while waiting for ack...
    tianheng han
    last modified by tianheng han
  • PDUM_eAPduFreeAPduInstance

    HI,I need your help with some questions   When i use this function ZPS_eAplAfUnicastAckDataReq( ), I need to apply for some APUD.   I know this function  ZPS_eAplAfUnicastAckDataReq have Retransmissio...
    tianheng han
    last modified by tianheng han
  • Control a QN9080 PWM using BLE

    Open video

    Fabian Ramirez
    last modified by Fabian Ramirez
  • hard fault caused by BusFault

    Hi all, I encounter frequent hard fault as soon I use CAN & USB at the same time. I'm using FreeRTOS  on a MK64F MCU. I tried to analyze fault registers to find out the cause of the hard fault but I'm not s...
    Johannes Bruder
    last modified by Johannes Bruder
  • Freescale keaz flash security

    Hello. I made device using keazn64 uC on board. I need to lock any action via swd(reading flash image). I tried to edit flashConfig section in stratup file but it doesn't help. I use segger j-link for debugging. How s...
    VITALI HARUDKA
    last modified by VITALI HARUDKA
  • Patch to fix LS1043A SGMII2.5G is not working

    The u-boot in SDK2.0 has a bug on SGMII2.5 support. Need to add the patch.
    Wes Li
    last modified by Adrian Puga Candelario
  • S32K118  adc_hwtrigger compil problem

    This interface will pop up when compiling ADC module. The file causing the problem was not found in this path.Compilation failed,whar's the problem?need help.Thank you.
    zh ew
    last modified by zh ew
  • i.MXRT1020 EVK 24b RGB pins and usage?

    MIMXRT1020-EVK docs says that the i.MXRT1021 processor have 24 bits RGB interface but I can't find references of what pins are or software usage... Can help me to use it to handle a VGA monitor?
    Fabio Coutinho
    last modified by Fabio Coutinho