• bitbake fsl-image-qt5-validation-imx ExpansionError

    Hi, I have recently purchased imx8mini board. I have installed ubuntu16.04 in the vmware I have download the yocto project by using "repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux...
    black huang
    last modified by black huang
  • Debugger mass erase

    Hello,    Debugger call mass erase command , is this command the same with erase all blocks unsecured command, thus erase command = erase all blocks unsecured command?   if there is write pr...
    kui wu
    created by kui wu
  • UUU compile

    Hi, I used VS2019 compile uuu-1.3.191 on Win10. However, I got error as below:   Could some one sent me the file 'gitversion.h'? Thanks.
    Carolyn Zhang
    last modified by Carolyn Zhang
  • Signing error in i.MX8M Mini - FIT Image

        I've followed this tutorial (Manually build Boot binary for i.MX8M Mini) for building U-Boot and successfully got the FIT image without HDMI component. And when I tried signing the FIT image followi...
    Kanimozhi Thangappan
    last modified by Kanimozhi Thangappan
  • How to connect LS1043A to a Switch using RGMII

    Our design needs to connect a switch chip with the rgmii interface of LS1043A. The MARVELL 88E6390 11 port GE Switch is connected to EC2 using RGMII. We don't know how to connect the RGMII sig...
    德辉 曾
    last modified by 德辉 曾
  • who can give a sample and explain  process of LIN example run on s32k1xx EVB

    need: 1. build a *.ldf and *.npf sample file with code warrior above 10.0 version . 2. generated program files lin_cfg (lin_cfg.c,lin_cfg.h,lin_hw_cfg.h) will be amend with  uart port of s32k144 and integrate t...
    642142357@qq.com
    last modified by 642142357@qq.com
  • ECSPI demo stop working in MCUXpresso Software Development Kit

    I'm using M4 core's ESCPI in i.max8mq and I want to start with the follow example code: boards\evkmimx8mq\rtos_examples\freertos_ecspi\ecspi_loopback boards\evkmimx8mq\driver_examples\ecspi\ecspi_loopback Both of t...
    Wen Fu
    last modified by Wen Fu
  • S32K148EVB Mechanical Drawings or 3D Models

    I need some sort of document that shows me where the connector headers and mounting holes are on the NXP S32K148EVB board. Can anyone help with this? I'm trying to design an enclosure that holds this board along ...
    Liam Burns
    last modified by Liam Burns
  • Component Development Tools Troubleshooting

    Why can not import PEx component with driver *.drv to develop. It happens in CodeWarrior 11.1 and MCUXpresso. Also inherited component is not available in MCUXpresso, and in CodeWarrior  imported component i...
    Marceli Firlej
    last modified by Marceli Firlej
  • How to analyze MCSR(IVOR1) Error?

    I use MPC5746C Z4 Core,and use S32DS tool for program debugging. IVOR1 interrupt was triggered while the program was running. I monitored the value of MCSR,bit16 IF is 1,That means "An error occurred during the attem...
    shijie.zheng@preh.cn
    last modified by shijie.zheng@preh.cn
  • iMX8QXP: Use RPMSG to wake up M4 and A35

    The reference code is based on L4.14.78 GA1.0.0 BSP and M4 SDK 2.5.1.  It is tested on iMX8QXP MEK board, and it should also work for iMX8QM board.   In L4.14.78 GA1.0.0 BSP, MU_5 is used for RPMSG between...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • LPC2388 UART2 Issue

    Hi all,   I am looking to get UART2 working on the LPC2388 microcontroller.   Currently, UART0 and UART1 works on it as they are provided in the sample code bundle (using uVision -- the first link under Em...
    Dan Michael Zarate
    last modified by Dan Michael Zarate
  • Derivative 9S12D64 Support in CW 5.2

    I recently downloaded CodeWarrior® Development Studio for HCS12(X) v5.2 from the website and am finally getting a chance to see if it will solve my issue of recompiling an old project from 12 years ago. My bigges...
    Allen Shea
    last modified by Allen Shea
  • eTPU function selector doesn't contain SPI function for slave mode. Where can I download eTPU SPI slave mode example?

    1) eTPU function selector https://www.nxp.com/webapp/etpu/ contains example only for eTPU SPI master mode function. Example code for mpc5777c contains only binary etpu micro-program in the etpu_code array variable and...
    Alexey Besgodkov
    last modified by Alexey Besgodkov
  • Design files for i.MX 8 Multisensory Enablement Kit (MEK)

    Hi NXP Community Could you please email me the allegro files for i.MX 8 Multisensory Enablement Kit (MEK) because it is not available in the website, My email: calibronic@yahoo.com    with regards, Saei...
    saeid fallah
    last modified by saeid fallah
  • on imx8q, fastboot reboot bootloader and ahab reset

    Dear NXP:   I am wang shuaiqing from hirain company. We are using imx8qm/imx8qxp board.   I found AHAB status can update after the board power-off / on. But AHAB status do not update after board...
    帅卿 王
    last modified by 帅卿 王
  • i.MX6 QMediaPlayer does qtvideosink use IPU?

    I want to use qt5 with qml to show a dual-stream.   main.qml: import QtQuick.Window 2.1 import QtQuick 2.0 import QtMultimedia 5.12   Window {     id: window     visible: tr...
    Michael Stahl
    last modified by Michael Stahl
  • 如何将部分程序放在ITCM中运行

    使用MXRT1011 发现在显示复杂的GUI 界面需要大量计算 ,20*320的画面 3-10ms,想将数据放到TCM中 ,但是程序太大,只有(+RW +ZI)放到了DTCM中,想将一部分程序GUI核心程序放到ITCM中运行,其他程序放在flexspi中,但是一直没有弄好,不知道怎么弄,还请指导下,谢谢
    k xw
    last modified by k xw
  • Source code of I2C-util.exe for secondary I2C bootloader

    Is it possible to get the source code of the I2C-util.exe incuded in AN11780?   best regards martin
    Martin Hollenweger
    last modified by Martin Hollenweger
  • GPIO Input And Output Problem

    Hi ı am using MIMXRT1052 on custom board. I am  using  MCUXpresso as an ide with  SDK_2.7.0_MIMXRT1052xxxxB. I tried to use GPIO2  pin 22 for interrupt. But ı cant get any interrupt. I examin ...
    Omer Kaan Basakinci
    last modified by Omer Kaan Basakinci