• How to mask tags having UID more than 4 bytes in ISO14443A protocol in NXP NFC reader library.

    I am using the "NXP NFC Reader Library" for reading HF(ISO14443A) tags like "Classic"/"Ultralight" etc. I can read tags using the below functions call. ++++++++++++++++++++++++++++++++++++++++++ /*Symbol 6,7,8*/ st...
    Pallav Joshi
    last modified by Pallav Joshi
  • RT1052 SDK2.7 USB CDC VCOM DeInit & Reinit

    What's the proper way to tear down (and bring back up again) the USB CDC Vcom when using FreeRTOS Tasks?   My usbRxTask setup is the same as the SDK demo, but the demo doesn't show how to tear down/re-init. I a...
    variable_andrew
    last modified by variable_andrew
  • java.lang.IllegalArgumentException

    Hello community,   I can not display SerDes1:SerDes which is created with default Code Warrior QCVS SerDes Configuration Tool. Can anyone tell me how to fix this error ? Is there any patch recommended to apply ...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • SSD MobileNet Inference using ArmNN on i.MX8qmmek

    Hello Community,   I am using i.MX8qmmek with BSP 5.4.3_2.0.0. I have my custom C++ application for running inference using TfLite and OpenCV. The appliaction with TfLite was able to use the GPU acceleration. No...
    Ullas Bharadwaj
    last modified by Ullas Bharadwaj
  • Ping between two interfaces on one host

    I'm trying to setup a test environment for a network equipment. I need to be able to ping between different interfaces on single host. Unfortunately I am not able to ping from one interface to another with current set...
    dogan ugurlu
    last modified by dogan ugurlu
  • Android USB Camera - How is it tested?

    I'm running Android P (2.3.4) on iMX8MQ and trying to use an external USB camera. I haven't seen anything that implements the Camera2 external camera config (External USB Cameras  |  Android Open Source Proj...
    Michael Brooks
    last modified by Michael Brooks
  • In QN908x how to keep the configured NVDS data untouched while reloading firmware

    After saving the configured NVDS data tag values in the QN908x Flash when we reflash the firmware using QN908x programming tool - SWD Download option (where we un-check "Download NVDS File") previously saved NVDS data...
    Kishan Saralaya
    last modified by Kishan Saralaya
  • S9KEAZN64: How to disable the watchdog?

    Good morning. My name is Daniele Fingolo and I am a software developer of SMH Technologies. I'm trying to program the S9KEAZN64 device in question with a programmer that we developed. We are able to communicate with ...
    Daniele Fingolo
    last modified by Daniele Fingolo
  • GPIO Input And Output Problem

    Hi ı am using MIMXRT1052 on custom board. I am  using  MCUXpresso as an ide with  SDK_2.7.0_MIMXRT1052xxxxB. I tried to use GPIO2  pin 22 for interrupt. But ı cant get any interrupt. I examin ...
    Omer Kaan Basakinci
    last modified by Omer Kaan Basakinci
  • TPM (SLB9670) initialization failed on i.MX8 ECSPI2

    Hi,   I'm working on getting the Infineon SLB9670 to work on the ECSPI2 bus of an IMX8MQ processor on the 4.19.35 kernel built using Yocto. The device seems to get detected on the bus ( there's a "spi1.0" node i...
    Rohit Dubey
    last modified by Rohit Dubey
  • Vpuenc_h264 maximum encoder size

    I've had a real tough time trying to use the vpuenc_h264 with an image bigger than 1920x1080 in the imx8m mini, the reference manual says that the VPU can work with a maximum size of 4080x4080 and if we use the encode...
    Mauricio Montero
    last modified by Mauricio Montero
  • MC33PT2000 use issues(2020079)

    I am currently using this chip. For the half-bridge in the same bank, should the gate signals of his high-side boost mos and 24v mos be inverted? However, the two G-pole driving waveforms measured here are in the same...
    Young fly
    last modified by Young fly
  • Cannot capture video or image for SBGGR12_1X12 format with Pico DCAM20 Camera Module

    Hi, Currenty I am working on i.MX8M Nano with Camera module Pico DCAM20 (2 lanes). To add support for this driver, I added the driver file addi903x.c as attachment. Mark , the addi903x need 2 lanes 135Mhz mipi cl...
    Michael Tong
    last modified by Michael Tong
  • TP9950+iMX6D分辨率960x576不支持

    视频处理芯片是TP9950,CVBS进来的转换BT656,如果分辨率720x576是没有问题的,但是TP9950输出分辨率改为960x576时,驱动ioctl_g_fmt_cap返回960x576会出现如下错误,提示不支持。 ========================================================================================== tw9990:ioct...
    kaifeng ye
    last modified by kaifeng ye
  • u-boot on custom T1024 board

    Hi,   We have developed a custom board base on the T1024. The CPU boots from an SPI memory, the SPI is programmed with the following binaries : u-boot 2016.09 binary @ offset 0x000000 of the SPI flash fsl_fman...
    Renaud De Koninck
    last modified by Renaud De Koninck
  • Programming question on FRDM-56F83000

          I create one project about FRDM-56F83000 (File-> New -> Project -> New Stationery Project, MC56F83789 -> MC56F83000-EVK -> C_Application), then compiling and programming are normal....
    Derek Xiang
    last modified by Derek Xiang
  • How to jump to the other image in the internal flash?

    Hi,there I am developing with mcu:MKL17Z128VLH4, I tried KL43 too. How to jump to another image in the internal flash? description: 1, burn project A to the mcu, this image locates at 0x00000 address. 2, burn...
    yilong wang
    last modified by yilong wang
  • kobs-ng / imx-kobs for IMX6UL

    Hi, I have a custom board with an IMX6UL on it. It's set up to boot from NAND flash, specifically: MT29F1G08ABAEAWP.   Currently NAND is empty, and I'm booting using the serial download protocol over UART. ...
    Andrew Parlane
    last modified by Andrew Parlane
  • iPhone app/sources for NTAG I2C Plus Explorer Kit

    Is an example app available for the NTAG I2C Plus ICs? It would be nice to have a reference app, similar to what is available for Android.   It would be even nicer if NXP would offer a library to build up on, bu...
    Arno Moonen
    last modified by Arno Moonen
  • KW41Z Power Manager Demo App not working

    Hi,   I recently bought a KW41Z development kit and trying to understand the different functionalities I need by going though the demos. Most of them worked flawlessly but power_manager and power_mode_switch see...
    thibaut koch
    last modified by thibaut koch