• How to enable RT1064 ENET2?

    Hi,   I have a custom board with a RT1064 connected to a Ethernet switch via RMII. I'm using MCUXpresso IDE v11.02 with MCU SDK v2.62 and I've modified the code to communicate to the switch over SMI instead...
    Tim Meyer
    last modified by Tim Meyer
  • MPC5566 Error loading .PCP file

    I'm not able load PCP file.   As per pe micro forum (Link: http://www.pemicro.com/forums/forum.cfm?forum_topic_id=3630&forum_id=9#c21540) To check basic debug functionality, you can try the following: ...
    jtro 9
    last modified by jtro 9
  • How many clock cycle is required for a read/write operation in K66 controllers  

    May i know how many clock cycle is required for a read/write operation in K66 controllers . i need to know flex bus read write speed please help me to find. 
    sarath g s
    last modified by sarath g s
  • KDS update website link

    Hello, I develloped project into KDS few years ago. Since, I change My computer and reinstall KDS v3.2.   But Plugin for MQX not installated. Then I follow procedure said above, But error message appears: ...
    arnogir
    last modified by arnogir
  • Display "flash down" with imx8qm

    Hi, I'm going to describe a problem I'm encountering and I can't exactly understand which can be the cause.   I'm evaluating diffent board for a new project, in particoular I'm evaluating a board performing iMX8...
    Andrea Previtali
    last modified by Andrea Previtali
  • Advertisement for iBean

    Would you please let me know whether KW36 BLE library supports advertisement for iBean while it is connected to some device? In general, when the device is connected to the other device, it stops advertisement. Is it...
    Kojiro Kaizuka
    last modified by Kojiro Kaizuka
  • S32K144: Read 1s All Blocks command

    I run the "Read 1s All Blocks" command over a S32K144 block (0x800B) which I know it's all erased (I checked it with a customized function as depicted below). When I issued the command (see below) the return MGSTAT0 b...
    David Gabbay
    last modified by David Gabbay
  • mrfc630 lpcd wakeup (mifare card)

    i developing using mfrc630 chip and reading coin mifare card. hardware board is complete. but lpcd value is not constant.  exmple All 10 Samples are different lpcd value. i used nxp develop board (CLEV6630...
    hwang bora
    last modified by hwang bora
  • Register settings for MC34VR500V1

    Can I change voltage and sequence for this device via I2C? I tried it , but I can't write new register setting to Internal RAM area. For example, I wrote new Volt1 settings with 0xA8. But After writing 0xA8, I can'...
    KEIICHI NEGISHI
    last modified by KEIICHI NEGISHI
  • Reading out proprietary data from NXQ1TXH5

    WPC spec allows receivers to send data to transmitters to control charging operations. There are also proprietary packets defined in the WPC specs. If a receiver sends such proprietary packages to a NXQ1TXH5 tran...
    Matthias Nagl
    last modified by Matthias Nagl
  • i.MX8M Mini GPIOs and Power-up sequence

    Hi NXP team,   W are using i>MX8M Mini Quad core processor in our emergency calling Device product. This product will be used as VoIP to help elderly people and kids at home during emergency situations. We ne...
    Nija Mankodi
    last modified by Nija Mankodi
  • what interrupts types we can ignore and what not in MPC5777C MCU

    Hi Support Team,   We are using MPC5777C MCU in our Aero project. I have to list out the interrupts which have the enable/disable capability.  From e200Z759N3 Core Reference Manual i understood that  ...
  • I2C EEPROM

    Hi, I am using a 24AA02E64T-I/OT (Microchip) EEPROM and want to interface it with I2C . I am unable to find the driver support for the same in nxp android source.   Would like to know if there's any suppor...
    Ramesh Krishnan N
    last modified by Ramesh Krishnan N
  • How many max resolutions of camera i.MX7D/8Nano can receive?

    I am thinking of camera system using i.MX7D or i.MX8Nano. What is tha max resolutions of camera pixels that i.MX7D/i.MX8 Nano can receive ? Is it possible to use 8Mpixel(3264x2448) RGB Bayer 10-bit camera ...
    Ye Gu
    last modified by Ye Gu
  • i.MX6UL with Secure Boot and HAB errors

    I can't seem to find definitive information on what the cause may be to the HAB Event error of (0x22) or HAB_INV_ADDRESS.   --------- HAB Event 1 ----------------- event data:    0xdb 0x00 0x08 0...
    Joe Duong
    last modified by Joe Duong
  • Boot Hang issue in iMx8DX6

    Hi Sir, iMx8DX6 board stops at boot level and after we switch off and on the board it starts working I have attached the working and non working  logs for your reference   When the boot hangs it stop...
    sheraz ali shah
    last modified by sheraz ali shah
  • PCA9545 (correction: PCA9554) digital inputs damaged caused by long high rise times?

    Correction of the chip number from Alois Lang (Author of this article): PCA9554 Text changed from PCA9545 to PCA9554 (January, 3th. 2020)   We use a PCA9554 I2C Port Extender Chip. In our application, we use t...
    Alois Lang
    last modified by Alois Lang
  • Display pixel clock limitation to 74.25 MHz

    Hi,   I'm using a board with the IMX8 SoC and 4.14.98 IMX kernel.   I'm trying to add support for a MIPI-DSI display (800x480@60Hz) that needs a pixel clock of ~25MHz.   The problem is that there is ...
    Sebastian Panceac
    last modified by Sebastian Panceac
  • "Stalled on bus" - meaning

    Hi,   I'm trying to debug a LPC4330 on a custom board - as asked here https://community.nxp.com/message/1258844?commentID=1258844#comment-1258844 - and what happens is that as soon as the code of Reset Handler i...
    Francesco Varani
    last modified by Francesco Varani
  • IDE for iMX8MQ & iMX8QM Processor

    Dear NXP Support Community,   We are working on iMX8 family of processors, the target core of interest is M4 core on which real time application will run over MQX RTOS. I would like to know if anybody in the com...
    Sangram Singh
    last modified by Sangram Singh