• S32K148 chip, J-link can not connect after program disorder.

    Hello,   I have a issue with j-link debug. My platform is S32K148, the debug tools is j-link, the 4 pin connect, GND-VCC-SWD-CLK. But one time, I debug my code, maybe the program is not valid, the program run&#...
    Fish Yu
    last modified by Fish Yu
  • [JN-AN-1216] How long will the Coordinator keep the data before device request?

    Dear Sirs,   In [JN-AN-1216] "IoT Control bridge", how long will the Coordinator keep the data until the device polling for it? How to extend the period?   Thanks!
    alan lin
    last modified by alan lin
  • Implementing FAT16 on JM60 USB Stack 4.11

    Hello, I need an implementation of FAT16 in a JM60 microcontroller, but i don't know how to start it. Is there an example with FAT16 and MSD with internal flash for study? I don't need to storage large files, just ne...
    Eduardo Kamada
    last modified by Eduardo Kamada
  • Android USB Camera - How is it tested?

    I'm running Android P (2.3.4) on iMX8MQ and trying to use an external USB camera. I haven't seen anything that implements the Camera2 external camera config (External USB Cameras  |  Android Open Source Proj...
    Michael Brooks
    last modified by Michael Brooks
  • MCU can't exit VLPS mode

        We came across a problem that very much like the description of ERR011063 in the Mask Set Errata for Mask 0N57U, the platform we are using are S32K144 and TJA1169.   ERR011063: SMC: An as...
    罗 文
    created by 罗 文
  • S9KEAZN64: How to disable the watchdog?

    Good morning. My name is Daniele Fingolo and I am a software developer of SMH Technologies. I'm trying to program the S9KEAZN64 device in question with a programmer that we developed. We are able to communicate with ...
    Daniele Fingolo
    last modified by Daniele Fingolo
  • Where can we find the USB Certification Guide for i.MX8M Mini?

    Where can we find the USB Certification Guide for i.MX8M Mini like below? https://community.nxp.com/docs/DOC-105609 https://community.nxp.com/docs/DOC-333262
    m.c
    last modified by m.c
  • Does IMX8MM support WQHD?

    Hi Community.   I set a 2400x480 display to panel-simple.c with IMX8MM, I am getting the following error.   [ 0.000000] Kernel command line: console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200 root=...
    Takashi Kashiwagi
    last modified by Takashi Kashiwagi
  • How can we sync the newest commits of kernel and u-boot from nxp?

    eg. QorIQ series and i.MX series.   we use QorIQ series and i.MX series in our project, and use the kernel/u-boot acquired from the Yocto years ago. Since that time i think NXP had commited lots of upd...
    changbao ma
    last modified by changbao ma
  • How to config Lin module as slave node base MCAL driver in S32K series board?

    Now I try to add lin slave node application base MCAL driver, but when I find lin configuration in EB tresos, it does not have item to assign master or slave node. And in MCAL driver, it only provide Lin_SendFrame() t...
    aa aaa
    last modified by aa aaa
  • Can anyone explain how and where display is configured in windows 10 IoT for imx8mq ?

    In imx-iotcore\driver\video\imxdod directory, I found display driver which has code related to HDMI for imx8mq and MIPI DSI, LCDIF for imx8mm. But the driver seems incomplete as there is no code for DCSS for imx8...
    Abhishek H
    last modified by Abhishek H
  • K32W test tool

    I use "Test Tool 12.9.1.0" to test Multillink. The following screen will be presented without k32w selection items and the word of option may be overwritten on WIN10. How do I choose to make K32W work properly? Ca...
    Daniel Tseng
    last modified by Daniel Tseng
  • RT1052 SDK2.7 USB CDC VCOM DeInit & Reinit

    What's the proper way to tear down (and bring back up again) the USB CDC Vcom when using FreeRTOS Tasks?   My usbRxTask setup is the same as the SDK demo, but the demo doesn't show how to tear down/re-init. I a...
    variable_andrew
    created by variable_andrew
  • DDR4

    hi,         My chip is i.MX8M MINI, I replaced DDR, use 4GB ram, uboot will get stuck every time.       1.     I used mscale_ddr_tool_v310 to test,     &...
    扬 杨
    last modified by 扬 杨
  • USB3.0 device mode speed in IMX8X

    Hi,   We are working with IMX8X based device , where the device will act as a webcam and using the USB3.0 port. The device is now getting detected as a  super speed uvc gadget device. We have the requiremen...
    ros M
    last modified by ros M
  • Should there be a command line after booting Android?

    Hey guys, I have configured Android 9 for our custom board based on Sabresd board.It is booting properly, I am also able to see the android display. But in the log I keep getting healthd status lines. There should b...
    Himanshu Savargaonkar
    last modified by Himanshu Savargaonkar
  • the Download Path and Installation Steps of S32K144EVB-Q100 Board BSP

    hello:    I use NXP S32K144EVB-Q100 Board,I want to download the BSP of this S32K144EVB-Q100 Board from NXP, Can you tell me the Download Path and Installation Steps of S32K144EVB-Q100 Board BSP ? ...
    lin li
    last modified by lin li
  • Brand New FRDM-K64F failing...

    I've plugged in my brand new FRDM-K64F. I've installed MCUXpresso SDK, IDE, Config Tools and (windows) serial driver. I've compiled the "hello world" demo. But when I click on 'debug', I get: One thing to note: ...
    Robert Poor
    created by Robert Poor
  • Can we use a XIP flash and a data flash at the same FlexSPI controller?

    Hello,   the reference manual of RT1020 shows how to connect flash devices to FlexSPI (RT1020 has only 4 data lines for A and 4 for B not 8 as shown in the picture) We want to use XIP on Flash A1 (read only) ...
    Stefan Mitterhauser
    last modified by Stefan Mitterhauser
  • Using QSPI flash A1 for XIP and QSPI flash B1 for data storage

    I came across a few posts for using 2 QSPI devices like Can we use a XIP flash and a data flash at the same FlexSPI controller?  One of the replies mentioned XIP uses AHB while programming the flash uses IP...
    THIVYA ASHOK KUMAR
    last modified by THIVYA ASHOK KUMAR