• No compatible probes available on Ubuntu 18.04

    Hi,   I'm trying to setup MCUXpresso IDE to work with an LPC55S69-EVK board on a 64bit Ubuntu 18.04 machine.   I've followed the instructions in MCUXpresso_IDE_Installation_Guide.pdf to install the MC...
    John Smith
    last modified by John Smith
  • MESA with T1042 ?

    Hi community, Is it possible to compile a kernel with MESA for T1042 using Yocto ? If answer is yes, what is the procedure to do this ? Thanks.
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • End consumer firmware upgrades

    I was hoping to find some guidance on the best solution for end user firmware upgrades with the iMXRT1062.   I’m aware of NXP’s boot image “MFG Tool” solution (https://community.nxp.com/d...
    Mike Spenard
    last modified by Mike Spenard
  • How to use device tree to get a rotary-encoder device

    What I want to do: Create a rotary encoder device in Linux with Yocto Project and device tree (/dev/rotary-encoder). The device should be visible after boot, so that it can be used in user space.   My Hardware: ...
    Michael Nehls
    last modified by Michael Nehls
  • elftosb issue

    Hi, I'm trying to use elftosb (V4.0.0) to generate an updated version of the flashloader sb file, and having some troubles. I created a bd file with the following contents;   options { flags = 0x00; startAddr...
    Dave Marples
    last modified by Dave Marples
  • S32K144EVB/Generated code download issue

    Hi NXP MBDT team,   I tried several times to generate the code of a basic example "gpio_s32k144.mdl" and download it to the board without success (the code is well generated but the download process did not acco...
    MOHAMED BENDERRADJI
    last modified by MOHAMED BENDERRADJI
  • Connecting LS1043ARDB through UART serial connection on CodeWarrior

    I have a 1043ARDB and I want to establish a connection with it through CodeWarrior using the serial connection with the RJ45 to DB9 cable on the UART1 port and I am having some issues with it. I can connect and commun...
    Franklin Turner
    last modified by Franklin Turner
  • I can't install freemaster 3.0

    Hi, I'm having some difficulties installing freemaster 3.0.   A installanywhere window appears after I double click FMASTERSW30.exe. After its completion bar finishes, a window with the freemaster logo appe...
    gean sousa
    last modified by gean sousa
  • QN9090 debug issue

    Hello team, I am trying to debug and run an example code with QN9090 but without a success, please find below my error screen and error log while (trying to) debug. it looks like an issue with the GBD toolchain whil...
    Shai Berman
    last modified by Shai Berman
  • NVT2001 spice model

    Can I download the NVT20xx spice model?
    Yingda Qin
    last modified by Yingda Qin
  • i.MXRT1010: How to configure FlexRAM?

    My current (default) FlexRAM settings are Flash: 16MB, SRAM_DTC: 32KB, SRAM_ITC: 32KB, SRAM_OC: 32KB NCACHE_REGION: 32 KB. My program needs bigger SRAM_DTC (64KB). I can change SRAM_DTC size in MCUExpresso &...
    Naveen Kumar
    last modified by Naveen Kumar
  • jn5169 Zigbee Route reply

    We have configured jn5169 zigbee as co-ordinator. We have connected the same to multiple sensors including gas leak sensor. We notice that in some cases co-ordinator stops sending route reply to route request received...
    Hariprasad Anumala
    last modified by Hariprasad Anumala
  • git.freescale.com down

    We noticed this morning our builds started failing. Looks like attempting to clone firmware-imx is failing.   When I try to clone the repo independent of a yocto build I see the following output:   git clo...
    Adam Bader
    last modified by Adam Bader
  • Use of Development Boards in 3rd Party Products

    I am new to ARM. I just purchased a Cortex-M SW development package and noticed that there is a lot of activity around ST's STM32 Nucleo development boards. However, their license agreement states that these boards ca...
    Paul McKneely
    last modified by Paul McKneely
  • p5040 serial port

    I'm looking for the DB-9 port pin outs and signal names for the p5040 rdb board
    Steve Billmire
    last modified by Steve Billmire
  • How to select JTAG as debug port on LPC54S018M

    I do not understand the wording in chapter 47 on how to select JTAG port for MCU debug at power up. How do I select JTAG port from hardware standpoint ? I do not understand how the boundary scan work to select SWD or ...
    bob belmont
    last modified by bob belmont
  • iMXRT1021 flexspiNOR unable to use HAB Encrypted XIP

    Hi, I am using the iMXRT1021 with flexqspiNOR flash. We want to encrypt the .sb image and the use on-the-fly BEE decryption. I am using the elftosb.exe, sdphost and blhost to produce and flash the .sb image. ...
    Tony Thurgood
    last modified by Tony Thurgood
  • How to install google Attestation keybox on IMX6Quad processor with Android

    Dear all,   I want to install google Attestation keybox on i.MX6Quad processor with Android to pass the“ run gts -m GtsGmscoreHostTestCases -t com.google.android.gts.security.AttestationRootHostTest#testEc...
    wenbo he
    last modified by wenbo he
  • PCIE   link up faile

    我们的产品中用到PCIE转以太网芯片。下面是电路   目前遇到的情况是不管在ep模式下还是在rc模式下都link up file PCIE_VP/VPH.  电压正常,这个和HDMI用同样的供电  ,HDMI现在能正常运行! Reset引脚也已经配置。 现在测量CLK1时,能测量到有1.3V左右的电压,但是测不到100M的波形。 RC模式下还是会出现下面的log。  ...
    军 李
    last modified by 军 李
  • Debug Challenge Response using TRACE32

    Does anyone know how to read the Challenge and write the Response using Lauterbach TRACE32 with a T4240?