• RM67295  + IMX8MM

    Now  I use RM67295  to display,but there is just RM67191 in the source. So can I  change the code of RM67191 to RM67295? If NXP have the code of  RM67295  pls update it to the git .T...
    qiao weibiao
    last modified by qiao weibiao
  • i.mx 8M Mini Evaluation Kit (imx8mmevk) - Debugging port is not recognizable

    Hi,    I recently purchased a i.mx 8M Mini Evaluation Kit board and was testing the board.  Using HDMI cable, I checked that the prebuilt Android image (coming with the board) boots fine.   ...
    Chang Min Park
    last modified by Chang Min Park
  • Looking for the old Freescale Learning Accademy resources

    Hello, time ago i watch some educational videos from the Freescale website about how to create a c# GUI for DEMOJM, and if I remember right also some etpu relate videos. Now I can't find that videos in the NXP site; A...
    damien darhk
    last modified by damien darhk
  • Beginner questions on MPC and ETPU

     I'm totaly new on etpu, never used MCP before, only HC08,HCS08 and HCS12, or Coldfire v1. I'm a bit confusing about the tool to use: in some AN I read that for MCU code is needed CW for MPC55xx/56xx 2.10, and if...
    damien darhk
    last modified by damien darhk
  • EVK-MIMX8MM: Cortex M4 debug w/ J-Link v8/v9

    Hello. Is it possible to debug Cortex M4 aux processor on IMX8MM (evk board) with Segger J-Link v8 or v9 (_not_ J-link plus as mentioned in "Getting started with MCUCpresso SDK for EVK-MIMX8MM") ? I am going to use O...
    Dmitry Bogdan
    last modified by Dmitry Bogdan
  • Why are interrupts not working in debug?

    MCUXpresso 11.1.1, MKV42F64, barebone, PE Micro Multilink. I have interrupts set up on PIT and PORT. When I run the application without the debug interface, the program runs correctly, detecting external interrupts an...
    Malcolm Macdonald
    last modified by Malcolm Macdonald
  • How to test S12ZVL LVI interrupt

    Hello everyone,   Currently, I am implementing the low voltage Interrupt for the S12ZVL chip. However, when I was trying to test it, I could not trigger the interrupt for LV. According to the datasheet, I have a...
    Junxi Cai
    last modified by Junxi Cai
  • LS1043A IFC clock generation during power-on-reset

    Hi,   Question on the generation of clock outputs by the LS1043A processor during the power-on-reset sequence.  While PORESET_B is being held asserted to the LS1043A will the processor generate a clock outp...
    Michael Macheski
    last modified by Michael Macheski
  • Zigbee Security issue with FRDM-KW41Z

    We are trying to get the FRDM-KW41Z eval board with  frdmkw41z_wireless_examples_zigbee_3_0_end_device_freertos example(SDK version: 2.2.1) connect with our zigbee network. After our ZC device replied a successfu...
    Jason Jiang
    last modified by Jason Jiang
  • FlexSPI read flash by AHB and IP commands

    Hello,   We are using the i.MX RT1060 with a NOR flash. The flash is read by AHB commands by the processor to fetch instructions (XIP) and we have a driver which also reads data from the flash at boot time but b...
    Armand Ciejak
    last modified by Armand Ciejak
  • Enabling Cryptographic Hardware Acceleration on LS1088ARDB

    What kernel modules do I need to install to get the LS1088ARDB to see the ARM crypto drivers. I am running layerscape 18.06 and using openwrt 19.07
    Reza Mohammadi
    last modified by Reza Mohammadi
  • How to setup sai1 tdm mode for imx8mq-evk? 

    The end goal is to configure sai1, txd0 for 8 frame, 32-bit, TDM mode (if it's not already) under Yocto Linux.    In "fsl-imx8mq-evk.dts", I see "fsl,sai-multi-lane" and "fsl,dataline,dsd = ...", ...
    John Adamson
    last modified by John Adamson
  • dts additions for interfaced SoC to iMX8MM EVK

    Hi,   I am working with IMX8M Mini EVK and yocto project build details:   Build Configuration: BB_VERSION = "1.38.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-16.04" TARGET_SYS = "aarch64-pok...
    Sreedhar A
    created by Sreedhar A
  • Steps to add the firmware binary into /lib/firmware directory in rootfs in i.MX8MM yocto project

    Hi,   I am working with IMX8M Mini EVK and yocto project build details:   Build Configuration: BB_VERSION = "1.38.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-16.04" TARGET_SYS = "aarch64-pok...
    Sreedhar A
    last modified by Sreedhar A
  • Flexcan stall status

    Hi, I am using the FlexCAN on the FRDM-K64 demo board starting from the example. It happened several times that the internal controller stall on TxBusy status and I am no longer able to send any packets. How sh...
    Fabio Benevento
    last modified by Fabio Benevento
  • KW36 FSCI bootloader

    I want to use FSCI bootloader to update KW36 and I flow this: Reprogramming a KW36 device using the FSCI bootloader . It look like success: But I press the sw, it does not start advertising. Doe...
    mo xinyu
    last modified by mo xinyu
  • Is Micron NOR MT25QU02GCBB8E12-0SIT compable with LS1088A?

    Is Micron NOR flash MT25QU02GCBB8E12-0SIT compatible with the LS1088AXN7Q1A processor?
    Samuel Stewart
    last modified by Samuel Stewart
  • LSPI Transfer fail with Assert for non 32 bit multiples

    Trying to upgrade a previous MC33664 driver up to the latest ARMV2.2 S32DS tools and the latest RTM 3.03 SDK.   So far I have found that the older BCC library relies on 5,10 or 15 byte packets etc - all multiple...
    Mike Newton
    last modified by Mike Newton
  • Breakpoints fail after NMI

    I have a board with an FS45 SBC that generates an NMI on a problem to an S32K144, in a similar arrangement to the NewTec BMS reference design. As I apply power to 5V peripherals, it causes a momentary power dip, which...
    Mike Newton
    last modified by Mike Newton
  • Can I write multiple NDEF with the TagXplorer app on PC?

    For example, a vCard and a URL on the same NFC tag.
    Austen Thomas
    last modified by Austen Thomas