• MBD based stateflow timestep problem

    hello I have a question when i use the stateflow in the MPC5744P_MBD. I want to use stateflow to do some pin voltage-level changes for some communication, But when i do a simple test, every index++ in simulink-st...
    hao xue
    last modified by hao xue
  • How to read Tag data using PN7150?

    Hello NXP,   I am working with PN7150 NFC Controller to read/write ICODE Tags. I am able to read UID but I am finding it difficult to read the Tag data.   Would it be possible to provide I2C com...
  • CTIMER DMA requests/triggers, pacing the transfers

    I got a DMA0 channel to successfully trigger from a CTIMER0 trigger source. The setup is as follows (using a custom board, not EVAL):   1. CTIMER0 with match1, with a capture input as source (10 MHz clock). Also...
    Hemanth M
    last modified by Hemanth M
  • i.MX8MQ is hanging in busfreq-imx8mq.c driver

    Hi NXP Team,   We are trying to port the i.MX8MQ custom board to Linux kernel 5.4.3. We are using the 5.4.3 kernel provided by the NXP team.   Please note that on the same board, previous version 4.7 is wo...
    Harshit Shah
    last modified by Harshit Shah
  • I.MX8M MIPI-CSI2 voltage level

    Hi ALL,   We are using I.MX8M in one of our solutions in which we are utilizing MIPI-CSI2 for acquiring CMOS Sensor Signals .    In the CMOS sensor datasheet, it is mentioned that VDD_MIPI is ...
    wei shi
    last modified by wei shi
  • Multiple & Repeated Icons on Toolbar of MCU Xpresso

    Hi, I have Updated my MCUXpresso to latest version - MCUXpresso IDE v11.1.0 [Build 3209] [2019-12-12].   The issue with IDE is irritating multiple and repeated on icons on toolbar.    Please do...
    ATHMESH NANDAKUMAR
    last modified by ATHMESH NANDAKUMAR
  • Output a kHz range clock through a GPIO?

    Hi I'm trying to output a 4 kHz 50% duty cycle square waveform through a GPIO. What is the simplest way of doing that?  It doesn't need to be exactly 4 kHz. I accept some tolerance around the target.&...
    Andre Luis Vilas Boas
    last modified by Andre Luis Vilas Boas
  • S12ZVML MINIBRD error 0x80000103

    Getting an error while trying to run S12ZVM_FOC_SENSORLESS on MINIBRD . Please find the attached error screen .   Regards, Basil 
    Basil Mathew Tharian
    last modified by Basil Mathew Tharian
  • Include not found in MCUXpresso

    Good morning I have the MCUXpresso showing these marking as unresolved inclusion. It seems the system include files are not reachable.     The project directory includes are added and for local include ...
    Pietro di Castri
    last modified by Pietro di Castri
  • Where could find demo code based on single-shunt for S12ZVM-EFP?

    There are three current sampling methods whichusesshunts in inverter legs as current sensors,tri-shunt,dual-shuntandsingle-shunt. S12ZVM-EFP supportsdual-shunt and single-shunt. There are two demo projects, one is for...
    Peter Shi
    last modified by Peter Shi
  • How To Use Clocks Config Tool?

    Hı ı am working on imxrt 1052 in MCUXpresso11.1.1. I tried to change clock settings in source files and config tool but ı could not. How can USDHC1 set as in example?
  • DDR: Failed to read SPD from address 81 [t1042]

    Hello nxp;   My custom design has a serious DDR problem, I have 16 GB total amount of Physical ram on design. Corresponding U-boot log (taken with Code Warrior -> Connect -> Debug session).   I ...
    Yusuf Altıparmak
    last modified by Yusuf Altıparmak
  • ls1043  support 4G DDR

    Our own board uses the ls1043 chip, the lsdk version is 2004, and the sdk supports 2G by default DDR, I want to know how to support 4G DDR, how to modify ATF and uboot, and whether there is a patch.
    wu bo
    last modified by wu bo
  • Is git://git.freescale.com down ?

    Hi,   I'm working on QorIQ T1024 (SDK-V2.0). Since this morning around 11h00 CEST time the url git://git.freescale.com/ppc/sdk/u-boot.git seems dead.    Is it normal and if so can anybody give me...
    Renaud De Koninck
    last modified by Renaud De Koninck
  • Hex file for IAP in lpc1788

    Hello Everyone   I'm looking for how to read hex file from USB (USB Interfaced successfully) and decode the data in RAM for write into internal flash of lpc1788 for In-Application Programming. In which form...
    rameshlalji9595@gmail.com
    last modified by rameshlalji9595@gmail.com
  • Suitability of i.MX processors for the best quality UAC 2.0 receiving

    Hello dear friends! I have a very unobvious sophisticated question about USB audio. Now I have delevoped my own portable hi-end audio and I want to provide for it a USB DAC functions. I know that it is possible with i...
    Vladislav Redin
    created by Vladislav Redin
  • USB-PD Sink support

    Hi, I am looking for the USB-PD sink support in my custom board. The power delivery requirement at a glance: USB-PD support on Type C connector Default Sink/Consumer power role, No power role swap required No...
    Ritesh Patel
    last modified by Ritesh Patel
  • process dma data from adc

    hi all i am working on a project dealing with transferring adc data via DMA. i need to know the the end of data address at destination buffer where i stopped conversion so i can put a flag for end of data. i also nee...
    navid fanaee
    last modified by navid fanaee
  • PTN3460

    Hi, I am using ptn3460 with KOE tx18d206vm0bpa display. As a result, I get only half of the picture I need. I attached the EDID that I use and display datasheet. I tried different modes: Vesa 24 bpp, Jeida 24 bpp, Ves...
    Oleg Losyakov
    last modified by Oleg Losyakov
  • imx8mq config dts(SPI)

    board:IMX8MQ-EVK Bsp:4.14.78 I want to change the default routing for the next three pins by configuring the device tree. Because we now want to lead out 40 pins on the new board for users' independent developmen...
    gao bo
    last modified by gao bo