• FFMPEG plugin support for NXP i.MX 8MQuad Evaluation Kit

    Is FFMPEG plugin supports for NXP i.MX 8MQuad Evaluation Kit.How it works,is there any code sample available?
    Abhishek Chouhan
    last modified by Abhishek Chouhan
  • Gstreamer support for NXP i.MX 8MQuad Evaluation Kit

    Is Gstreamer plugin supports for NXP i.MX 8MQuad Evaluation Kit,how it works,any codesample or steps are available?
    Abhishek Chouhan
    last modified by Abhishek Chouhan
  • Lifetime of LPC54608

    Actually we are using LPC54608 Controller to interface 10 types of devices through serial ports. But the customer has asked me that, what is the lifetime of your major components in the product. In my routing pro...
    Avinash G
    last modified by Avinash G
  • The startup time in S32R274 is too long

    The startup time is too long for me, and I found the process of initializing SRAM ECC costs about 80ms. If I delete this process, It cannot start normally. So, How can I reduce the time in startup.s?  
    群 张
    last modified by 群 张
  • test log of "Seamless redundancy test case"

    Hi Yiping,   It seems that the switch tsn test logs did not include the " Seamless redundancy test case".   Would you please help to check it? And if the logs available, please help to send me the ...
    Tang zhantao
    last modified by Tang zhantao
  • FRDM-KW36 - Extended Advertising

    Hi, NXP expert.   I am testing beacon(extended Advertising) using KW36 Board. The Gap_SetExtAdvertisingParameters function returns an error while testing an extended Advertising using the beacon ...
    ayden hong
    last modified by ayden hong
  • iomux register read and write

    I am using memtool to read the value from iomux register; for example, I want to read the SPI2_CS0 with the address of 0x401C0, but failed with bus error. But I can read the 0x5A000000 (version id register for spi) ...
    andy G
    last modified by andy G
  • Adding packages under core-image-base image

    Hi All,   I am working on yocto zeus (https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml).I am adding some packages under core-image-base image. I modified th...
    Nikhil sahu
    last modified by Nikhil sahu
  • Q2: CAN transmission in a proper way?

    I have custom made LPC54618 board & I want to communicate with x number of other CAN devices. I have used MCAN_TransferSendBlocking() function till now which worked until number of devices are less. I certainly mo...
    gmk1@amararaja.co.in
    last modified by gmk1@amararaja.co.in
  • How can I boot to LPC55 to BOOT ROM from firmware code?  Previous method doesn't work

    I'm trying to get the LPC55 to enter the bootloader from application code.  I previously tried this solution which edits the `BOOTERRORCOUNTER` of the AOREG1 register.  This solution did work on my LPCXpress...
    Conor Patrick
    last modified by Conor Patrick
  • i.MX8 QuadXPlus chipset roadmap

    Hi. i.MX8 QuadXPlus chipset has been developed, so please contact us to know the schedule available. Please share if you have the latest (2020year) Roadmap related to i.MX8 QuadXPlus chipset.   Have a nice day.
    hwang jinha
    last modified by hwang jinha
  • about imx8mm on android9

    first、Our board is resigned by imx8mm evk,while some module chips had been removed. second、I flash images to sd card and boot from sd,the android kernel is stop here and not return [    5.202213] dm ...
    zhou wei
    last modified by zhou wei
  • Udoo Neo Full is loading imx6q-udoo-hdmi.dtb

    Hi Everyone! I'm newbie in linux system! After checking /sys/var/term.log, I saw linux OS of my udoo board, it load imx6q-udoo-hdmi.dtb and it dose not load any *.dtb file in /boot/dts folder. I tried to at this li...
    Anh Pham Tuan
    last modified by Anh Pham Tuan
  • Automatic configuration of ddr stress tool within uboot

    Hi,   We use the ddr stress tool via uboot as part of our QA process. It's manually driven and we would like to automate it. Is it possible to automatically configure it to run a preconfigured stress test via ub...
    joerutledge
    last modified by joerutledge
  • How to identify display on imx8qxp

    As imx8qxp can driver more displays(DSI0, DSI1 and LCDIF),  How to identify display in application while all these display drived ? thanks. our test environment is L4.14.98_2.3.0_images_MX8QXPMEK(rootfs is&...
    Ping Wu
    last modified by Ping Wu
  • LCP540 to LPC546 - Pin compatibility

    Hello, according to the NXP website LPC540 and LPC546 are pin compatible. I also checked the pin mapping.   I got the MCU professionally reworked from LPC540 to LPC546. My PCB is not working properly anymore now...
    Jana Beck
    last modified by Jana Beck
  • Is there any Mechanical drawings related SLN-VIZN IOT kit availabe?

    I was looking for the mechanical drawings of the camera module MT9M114 that nxp supply along with the SLN-ViZN iot kit[based on imxRT-106F cross over mcu]. I searched over the net, but couldn't find the part no: or an...
    Delwyn Joseph
    last modified by Delwyn Joseph
  • P2020,TESC3 can not ping

    Hi    Thank to answer this question。    There are some problem about the chip P2020,I using 2 ETH PHY in this project,which using in TSEC1 and TSEC3。TSEC1 is no problem and it can ping ...
    Lu Yingyu
    last modified by Lu Yingyu
  • imx8mm evk HABv4 problem

    Dear nxp     use   i.MX_Android_Security_User_Guide.pdf documents verification 8mm HABv4 Funtion,the motherboard cannot start or burn. What caused this problem. Have you encountered such a pr...
    Aber fu
    last modified by Aber fu
  • Does NXP keep legacy Linux SDK's?

    I need to recreate a U-Boot that was built with the gcc-4.3.74-eglibc-2.8.74/powerpc-linux-gnu/bin/powerpc-linux-gnu-gcc tool chain but have been unable to find it anywhere.   I found major and minor, but n...
    Kurt Copley
    last modified by Kurt Copley