• HOW TO TEST AUTOSAR SW-C on NXP Microcontrollers

    To learn more about AUTOSAR SW-C, design, simulation and test on NXP HW please check this webinar
  • RTM SDK QSPI watermark functions/QSPI example.

    S32 Design Studio for ARM 2018.R1 with Update 11.   Example project qspi_external_flash_s32k148 from "S32K1xx RTM SDK v3.0.0" (can't find a 3.0.2 example but "S32 Design Studio S32K1xx SDK RTM 3.0.2 Patch for SD...
    Magnus Johansson
    last modified by Magnus Johansson
  • How to export Generated Code to S32 Design Studio IDE (applicable for MBDT for MPC5744P v2.0)

    In case you need to export the generated code to S32 Design Studio for PA IDE, now there is an easy way. No more painful job of reconstruction the project manually and setting all sort of compiler flags. Here is what ...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • Comments related to the PN7150 NFC library

    Hi,   I just managed to adapt the source code example for PN7150 for the EVK-RT1064 board and for the Arduino PN7150 board (source code: evkmimxrt1060_PN7150).   I used the latest versions of MCUxpresso ID...
    Neculai Agavriloaei
    last modified by Neculai Agavriloaei
  • QSPI Flash Help - MIMXRT1050

    Hello,   I am using the MIMXRT1050 with QSPI flash on Keilv5 IDE. My QSPI flash manual: https://www.winbond.com/resource-files/w25q256jv%20spi%20revg%2008032017.pdf   I am using the flexspi_nor_polling_...
    Kamal Nasif
    last modified by Kamal Nasif
  • Re: Supported operating systems of IMX6_L4.1.15_2.0.0_MFG_TOOL

    Hello.Can I ask additional question? Can I use MFGTool with the system that is Windows10 + USB3.0? Recognized by the device manager on WIndows10, but displayed as "No Device Connected" in the MFGTool application. Eval...
    takuroh yoshida
    last modified by takuroh yoshida
  • 欢迎来到恩智浦电源管理芯片中文技术社区

    尊敬的客户:      感谢你选择恩智浦半导体的芯片,如果有任何技术问题,请您在本社区提问,我们将会尽快回复。 谢谢。
    Jinyu Zhang
    last modified by Jinyu Zhang
  • Motor Control Class: Lecture 5 - Hall Sensors

    In this fifth lecture of the motor control course we discuss about how can we read the hall sensors to obtain the rotor position in order to know how to apply the correct voltage sequence to the motor phases...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • Keypad Port (KPP) on the i.MX RT1010 EVK

    Thanks to NXP for providing example code for the KPP peripheral on the RT1010. The one thing they missed was a wiring diagram for the example (although doc/readme.txt gives the connections) - so I thought I'd provide ...
    John Adriaan
    last modified by John Adriaan
  • Slight error in SDK i.MX RT 1015 clock config code

    Hi All   This is the example code in SDK for i.MX RT 1015 clock configuration and the DCDC voltage regulator setting for 500MHz operation:     /* Setting the VDD_SOC to 1.5V. It is necessary to c...
    Mark Butcher
    last modified by Mark Butcher
  • i.MX RT1064 and PN7150 NCI Library

    Hello,   I have adapted the NXPNCI-PN7150 software example to work with the iMX RT1064 microcontroller. For this purpose I used the MIMXRT1064-EVK development board and the Arduino PN7150 board (OM5578 / PN7150S...
  • mfgtool2 damage two pico-imx7d SOM modules. Where it spoiled?

    Hi,   I have this issue: My other imx7d pico android things start kit died, again    I was following the steps of this link: iMX7D Pico won't boot    I used the <LIST name = "e...
    NEUBER DE SOUSA
    last modified by NEUBER DE SOUSA
  • Drivers for 88W8964

    Hey everyone!   I'm one of may OpenWRT contributors and I'm also a owner of a Linksys WRT3200ACM witch has a NXP 88W8964 wifi chip. Before being NXP bought all the wireless solutions from Marvell, they were dev...
    Tiago Gaspar
    last modified by Tiago Gaspar
  • How-to Add missing derivatives to CodeWarrior Classic HCS12(X) 5.2 (Unofficial Method)

    The Good and the Bad about CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.2 Removed more than half of the supported chips for "market reasons" (see table below) Updated P&E drive...
    Rodney McGee
    last modified by Rodney McGee
  • URGENT: Problems using ADC of MXRT1051

    We are a bit under pressure to solve this problem, would be nice someone could help fast.   Wenn we measure with ADC the signals makes a jump than it reaches a certain level.    First picture sho...
    Thomas Kintzel
    last modified by Thomas Kintzel
  • 1.2 S32V enablement

    SOFTWARE The S32 Design Studio for ARM® The S32 Design Studio for Vision The Vision Toolbox for MATLAB® The Automotive Ethernet Audio Video Bridging (AVB)     HARDWARE The SBC-S32V234 evaluat...
    Toño Hernández
    last modified by Toño Hernández
  • 1.1 S32V overview

    The S32V234 is our 2nd generation vision processor family designed to support computation intensive applications for image processing and offers an ISP, powerful 3D GPU, dual APEX-2 vision accelerators, security and s...
    Toño Hernández
    last modified by Toño Hernández
  • 1.0 S32V INTRODUCTION

    WHAT YOU WILL LEARN: Understand the basic aspects of S32V234 vision processors, the second generation vision MPU family for supporting computation intensive applications for image processing     1...
    Toño Hernández
    last modified by Toño Hernández
  • Devkit S12ZVC : CANH stucked High

    Hello, I've got a problem with the CAN bus, I've configured the MSCAN0 with code warrior expert (bit rate: 250 kbit). The system works fine in loop back mode: I can send data and the event CAN1_OnFullRxBuffer() ...
    Luca Ferrario
    last modified by Luca Ferrario
  • S32K144 board detection problem

    Hello, recently, I have bought S32k144 EVB and I have watched tutorials how to control it and etc, but the thing is that I cannot establish communication between this board and my laptop. When I turn on Freemaster pr...
    Tautvydas Karvelis
    last modified by Tautvydas Karvelis