• Achieve Exceptional Graphics for IoT Devices of Tomorrow with NXP's i.MX 8M Nano Applications Processor.pdf

    Ethan Fernandes
    last modified by Ethan Fernandes
  • Self-Service Library

    Overview  Libraries strive to provide great service and to ensure easy access to media products. With thousands of visitors choosing from copious books, CDs, videos, and computer games, storing and controlling in...
    Juan Rodarte
    last modified by Juan Rodarte
  • Handheld Scanner

    Overview  Barcode scanners are essential in everyday activities including grocery scanning, identifying hospital patients, and tracking boxes or products in a production line or warehouse. In all cases, they must...
    Juan Rodarte
    last modified by Juan Rodarte
  • Electronic Shelf Labels

    Overview  These shelf-mounted displays can be updated wirelessly, anywhere onsite, so there’s no more need for staff to manually change price labels or print, sort, and replace labels when prices change. P...
    Juan Rodarte
    last modified by Juan Rodarte
  • High-End Tablets And Payment Terminals

    Overview  NXP provides full solutions to power high-end payment terminals. NXP is at the forefront of contact and contactless payment solutions and is a leader in providing security solutions for the banking and...
    Juan Rodarte
    last modified by Juan Rodarte
  • POS Printer

    Overview  NXP offers PowerQUICC. and ColdFire. processors and a large selection of 8-bit MCUs that support common point-of-sale (POS) printer applications for retail and services industry customer receipts. ...
    Juan Rodarte
    last modified by Juan Rodarte
  • FreeMASTER 3.0.1 Update - Release Announcement

    Updated version 3.0.1 of the NXP FreeMASTER tool has just been published online.    For more details, please read the recently posted FreeMASTER 3.0 Announcement. Also see downloads, documentation and other...
    Michal Hanak
    last modified by Michal Hanak
  • Overview of supported NFC/MCU Combinations

    This page contains information about the supported NXP MCU/MPU and NXP NFC product combinations which have ready to use packages. These can be used as a reference. The table below contains link to where you can find t...
    Ali Khan
    last modified by Richard Schmidmaier
  • QN9080 PCB RF validation with Non Signaling Test Using MT8872

           My customer asks if QN9080 can be tested with MT887x. We co-work with Anritsu Taiwan to integrate QN9080 and MT887x to perform 1M bps, 2M bps and Frame error rate test. This docume...
    Jason Chiang
    last modified by Jason Chiang
  • iMX8QXP: Use JPEG decoder in M4 SDK

    iMX8QXP/iMX8QM have hardware JPEG decoder: The JPEG-D-X core. This is the example code to use this hw decoder in M4 SDK to decode JPEG files.     M4_JPEG_DECODER_SDK_2.5.1.7z The attached "rear_view_c...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • Using the QN908x FreeRTOS BLE Abstraction Layer Stack to create Tasks and Queues.

    Introduction  In this document, we are focusing on the usage of two functions of FreeRTOS: Creation of tasks and the use of queues as a way to trigger a generic functionality in our application. NXP’s SDK a...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • Example MPC5644A eQADC channel 146 conversion+calibration CW210

    ******************************************************************************** * Detailed Description: * Initializes eQADC module, performs calibration and converts channel 146 * (voltage level of VDD) to check c...
    David Tosenovjan
    last modified by David Tosenovjan
  • Example XPC567XFKIT PinToggleStationery CW210

    ******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, bl...
    David Tosenovjan
    last modified by David Tosenovjan
  • Example XPC567XRKIT PinToggleStationery CW210

    ******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, bl...
    David Tosenovjan
    last modified by David Tosenovjan
  • Example MPC5777C External SRAM_test GHS714

    ******************************************************************************** * Detailed Description: * Application performs basic initialization then it initializes EBI for external * SRAM connected to MPC5777C-51...
    David Tosenovjan
    last modified by David Tosenovjan
  • RDAIRBAGPSI5 Airbag Reference Platform

    Overview  The Freescale Airbag Reference Platform (ARP) is an application demonstrator system which provides an airbag Electronic Control Unit (ECU) implementation example using complete Freescale standard produ...
    Juan Rodarte
    last modified by Juan Rodarte
  • RDSABRE_FOR_EREADERS: SABRE for eReaders

    OverviewThe NXP Smart Application Blueprint for Rapid Engineering (SABRE) series of market-focused reference designs delivers the SABRE platform for eReaders based on the i.MX508 processor. The i.MX508 is the fir...
    Juan Rodarte
    last modified by Juan Rodarte
  • Manually build Boot binary for i.MX8M Mini

    Sometimes it is helpful/faster to build a i.MX8MM boot binary outside of the Yocto environment.   There are instructions on how to accomplish this on different places, this document tries to provide an example f...
    Renato Nogueira Frias
    last modified by Renato Nogueira Frias
  • Kinetis Motor Suite

    KINETIS DESIGN STUDIO IS NO LONGER SUPPORTED BY NXP. Follow this link for more information:Kinetis Motor Suite    Demo Kinetis motor suite is a highly intuitive motor control development solution that en...
    edk
    last modified by Fabian Ramirez
  • Using a TensorFlow Lite Model to Perform Handwritten Digit Recognition on RT1060

    Convolutional Neural Networks are the most popular NN approach to image recognition. Image recognition can be used for a wide variety of tasks like facial recognition for monitoring and security, car vision for safety...
    David Piskula
    last modified by David Piskula