• unable to connect to git.freescale.com

    Recently many customers faced the issue about connecting the git.freesacle .com failed when they built old bsp version like 4.1.15 or 3.14.52,  when the customer repo init according to the yocto user guide, they ...
    Joan Xie
    last modified by Joan Xie
  • i.MX 6/7 DDR Stress Test Tool

    Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private mess...
    Oliver Chen
    last modified by asimzaidi
  • i.MX 8M Family DDR Tool Release

    Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private mess...
    Oliver Chen
    last modified by asimzaidi
  • FXLS8471Q - Accelerometer motion detection function example code

    Hi Everyone,   If you are interested in a simple bare metal example code illustrating the use of the accelerometer motion detection function, please find below one of my examples I created for the FXLS8471Q acc...
    Tomas Vaverka
    last modified by Tomas Vaverka
  • mPOS (MOBILE Point-of-Sale)

    Fabian Ramirez
    last modified by Fabian Ramirez
  • Automated verification of ARM TrustZone configuration

    Automated verification of ARM TrustZone configuration   Data security is an essential part of embedded systems design. Security features are being implemented to microcontrollers. One of the present technologies...
    Marek Vitula
    last modified by Marek Vitula
  • FRWY LS1046A TP NFC demo

    Introduction The FRWY LS1046A comes with the mikroBUS connector that enables the capability to connect different peripheral depending on the application's requirements. The mikroBUS intends to be used for prototyping ...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • FRWY LS1046A TP Video Vault demo

    IntroductionThe LS1046A MPU capabilities to manage data are one of the cornerstones in its design, this makes it a perfect choice when the end-application is related to data network management. The Frame Management fe...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • iMX 8M Mini Register Programming Aid DRAM PLL setting

    The Register Programming Aid (RPA) provides a default DRAM PLL setting (DRAM frequency) based on the default setting supported in u-boot.  It is highly recommended to use the default DRAM frequency settings in th...
    asimzaidi
    last modified by asimzaidi
  • Port MCUBoot2.0.0 to TWR-K60D100

    Abstract MK60 is a popular MCU in Kinetis K family. NXP has prepared some kinds of bootloader for TWR-K60D100. But as we all know, MCUBoot2.0.0 is the most update bootloader for Kinetis family. It is a configurable f...
    Jing Pan
    last modified by Jing Pan
  • FRWY LS1046A TP CPU Performance Benchmarking Demo

    Introduction Overview Block Diagram Video Products Introduction LS1046A has four 32-bit/64-bit Arm Cortex-v8 A72 CPUs arranged as a single cluster of four cores. LS1046A shares a single 2 MB L2 wit...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • FRWY LS1046A TP Machine Learning/Video Analytics

    IntroductionOverviewThe following demo is part of a bundle of examples that shortly will be available in the LSDK. As can be seen in the video, there is a menu for the user to select the desired demo and start testing...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • Model-Based Design Toolbox for MPC57xx Automotive Microprocessors Version 3.1.0

          Product Release Announcement Automotive Microcontrollers and Processors NXP Model-Based Design Toolbox for MPC57xx – version 3.1.0     Austin, Texas, USA December 16th, 2019...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • How to change Linux Kernel configuration file in Yocto Project metalayer

    How to change Linux Kernel configuration file in Yocto Project metalayer Preparing the requirements Download the metalayer Git clone the Linux Kernel source code Customize the configuration Copy the ...
    Daiane Angolini
    last modified by Daiane Angolini
  • i.MX 8/8X Series DDR Tool Release - Draft

    Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages ...
    asimzaidi
    last modified by asimzaidi
  • Get GPS Coordinates and send them through Sigfox

    About the demo components Video Limitations: Useful Links Required Items: Hardware Diagram: Step-by-Step Guide Results: About the demo components For this demo, we are using the Sigfox...
    Fabian Ramirez
    last modified by Fabian Ramirez
  • Example MPC5777C FlexCAN simple TXRX ECC enabled GHS616

    ******************************************************************************** * Detailed Description: * * Configures the FlexCAN to transmit and receive a CAN message. * ECC reporting in the FlexCAN module is enabl...
    Petr Stancik
    last modified by Petr Stancik
  • Example MPC5604B LINFlex LIN Master-Slave communication demo CW210

    This demo performs a communication on LIN bus between two MPC5604B EVBs.   LinFlex0 LIN Master ******************************************************************************** * Detailed Description: * - send...
    Petr Stancik
    last modified by Petr Stancik
  • Safe video switch using ADV7180 and i.MX6Q Automotive Board

    i.MX6Q Automotive board has one ADV7180 analog video decoder with 2 video inputs. By default, only input 1 is used (connector J42).     To connect 2 analog video sources and switch the display between the...
    rogeriopimentel
    last modified by Adrian Puga Candelario
  • NXP Tech Session - Enabling Motor Control Across a Range of NXP MCUs with MCUXpresso and FreeMASTER

    View the rest of the NXP eXperience here
    Ethan Fernandes
    last modified by Ethan Fernandes