• Excel MPC5777C clock configurator

    This config tool simplifies PLL setting calculation and clock configuration for MPC5777C device.                 Follow these steps  ...
    Petr Stancik
    last modified by Petr Stancik
  • MX8M_Series_Design_Resource_Guide_V1-20200228_chn.

    目录 1 www.nxp.com公网资源 .............................................. 2 1.1 www.nxp.com Documentation ................................ 3 1.2 www.nxp.com Tools&Software ............................... 6 2 nxp 社区资源 .....
    John Li
    last modified by John Li
  • Build Ubuntu For i.MX8 Series Platform

    The Guide is how to use Ubuntu filesystem with i.MX8 series platform.At present, I had try it on i.MX8QXP with 4.14.98 kernel with ubuntu16.04.   The Document will be continuously updated with enable VPU, ubuntu...
    Gnar Fang
    last modified by Gnar Fang
  • Patch to Support BT656 and BT1120 Output For i.MX6 BSP

    Here are two patches to support BT656 and BT1120 output for i.MX6 ipuv3. With this patch, the i.MX6 can support the CVBS output on TV encoder. It is useful for a TV box.   "L3.0.35_1.1.0_GA_bt656_output_patch.zi...
    Qiang Li - Mpu Se
    last modified by Adrian Puga Candelario
  • Manually build Boot binary for i.MX8M Mini

    Sometimes it is helpful/faster to build a i.MX8MM boot binary outside of the Yocto environment.   There are instructions on how to accomplish this on different places, this document tries to provide an example f...
    Renato Nogueira Frias
    last modified by Renato Nogueira Frias
  • i.MX 8 MCUs with SafeAssure®-Certified Features—Camera, Video, Audio, Trusted Environment

    This class will explain several software solutions offered for the i.MX 8. SafeAssure software allows for a system partitioning that takes full advantage of the ability of some of the safety features of the i.MX 8. Fa...
    Renee Fortenberry
    last modified by Renee Fortenberry
  • i.MX8QXP gamma tuning

    This doc show how to use i.MX8QXP Display Controller GammaCor unit to tune gamma. HW: i.MX8QXP MEK board, HDMI monitor SW: i.MX Linux 4.14.98_2.2.0 BSP release, patch in this doc   1.Introduce gamma The gamma, ga...
    PengFushi
    last modified by PengFushi
  • PCF2129 RTC example code

    ************************************************************************************************** * The PCF2129AT is a CMOS Real Time Clock (RTC) and calendar with an integrated * Temperature Compensated Crystal Os...
    Tomas Vaverka
    last modified by Tomas Vaverka
  • Example MPC5674F MPU Initialization CW210

    ******************************************************************************** * Detailed Description: * MPU is initialized to cover all resources (flash, RAM, peripheral bridges). * All masters are allowed to read...
    Lukas Zadrapa
    last modified by Lukas Zadrapa
  • i.MX7D DRAM Register Programming Aid

    These are detailed programming aids for the registers associated with DRAM initialization (LPDDR3, DDR3, and LPDDR2). The last work sheet tab in the tool formats the register settings for use with the ARM DS5 debugger...
    m_j
    last modified by m_j
  • eIQ Transfer Learning Lab with i.MX RT

    This lab will cover how to take an existing TensorFlow image classification model, and re-train it to categorize images of flowers. This is known as transfer learning. This updated model will then be converted into a ...
    Anthony Huereca
    last modified by Anthony Huereca
  • eMMC5.0 vs eMMC5.1

    Biyong Sun
    last modified by Biyong Sun
  • imx_builder --- standalone build without Yocto

     Dec 11, 2019: imx_builder_12112019.tgz --- add support  L4.19.35_1.1.0 August 28, 2019:  imx_builder_08282019.tgz   --- add i.MX8MM July 03, 2019:  imx_builder_07032019.tgz --- add i.M...
    Biyong Sun
    last modified by Biyong Sun
  • eIQ ML Software Clinic - Lab and Software Files

    Please find the necessary software and documentation for the eIQ for i.MX RT Software Clinic.   Attached to this post you will find: Updated source code - eIQUpdate.exe.zip that adds camera ...
    Anthony Huereca
    last modified by Megan Hansen
  • MX8X_4.19.35_kernel_V4-20200217_chn linux kernel定制文档

    Contents 1 创建 i.MX8QXP Linux 4.14.98_ga 板级开发包编译环境 2 1.1 下载板级开发包 ...................................................... 2 1.2 创建yocto编译环境: ................................................ 3 2 Device Tree .................
    John Li
    last modified by John Li
  • MX8X_4.19.35_ga_BootLoader_V6-20200217_chn bootloader定制文档

    目录 1 i.MX8X 板级开发包镜像结构 ...................................... 3 2 创建 i.MX8QXP Linux 4.19.35 板级开发包编译环境 ... 3 2.1 下载板级开发包 ....................................................... 3 2.2 创建yocto编译环境: ..........................
    John Li
    last modified by John Li
  • OpenVX Vision Image Extension API Introduction - Basic API

    Introduction EVIS (Enhanced Vision Instruction Set) is an API level program language, which is applicable on GC7000XSVX (i.MX8QM) and VIP8000NanoSi (i.MX8MP). The instructions take advantage of the enhanced visio...
    Devin Jiao
    last modified by Devin Jiao
  • How to use OpenVX extension for NPU/GPU to accelerate machine vision applications

    This guide is about how to use EVIS to create user nodes and kernels in OpenVX to implement image processing on NPU(i.MX8MP)/GPU(i.MX8QM). Take gaussian filter as an example. It is tested on i.MX8QM and i.MX8MP. ...
    Devin Jiao
    last modified by Devin Jiao
  • change DRP to DFP for i.MX 8QuadXPlus MEK with C0 chips

    For early i.MX 8QuadXPlus MEK boards with C0 chips, power on the board when the board is connected to the PC with USB Type-C cable may cause the PC to shut down directly. This is a hardware known issue. another t...
    Faqiang Zhu
    last modified by Faqiang Zhu
  • Linux fw_printenv fw_setenv to access U-Boot's environment variables

    Biyong Sun
    last modified by Biyong Sun