• Longevity Extended to 15 Years on More than 100 MCU Devices 

    NXP understands that in addition to offering breakthrough innovations its ongoing investment and commitment to longevity is critical to being your trusted supplier. This paired with the continued demand and broad mark...
    Monica Velez
    last modified by Monica Velez
  • MCUXpresso IDE v11.1.0 SDK Handling Hotfix

    An issue has been identified in MCUXpresso IDE v11.1.0 with SDK 2.7 that in certain circumstances can cause the IDE to issue one or more erroneous duplicate file error popups when importing SDK examples or creati...
    LPCX presso support
    last modified by LPCX presso support
  • Modifying the latest Adafruit 2.8" LCD for SDK graphics examples

    Our MCUXpresso SDK is expanding to include more and more graphics examples, including LittleVGL and emWIN support for SPI-based LCDs. The examples we provide can be ported to different controllers, but are based/...
    Brendon Slade
    last modified by Brendon Slade
  • Powerful i.MX8 QM/QP SBC to Ease Development Challenges and Accelerate Innovations

    Oftentimes, developing an end application is like a scary game of maze. One can easily get lost in its winding paths lined with unseen twists and obstacles. A wrong choice can lead you to start all over again, making ...
    iWave Systems
    last modified by iWave Systems
  • QNX RTOS on iWave’s i.MX8QM/QP SMARC Module

    QNX is a Unix-like Real Time Operating System primarily developed for safety and mission critical embedded systems and includes the following unique features; Microkernel architecture Dynamically upgradable services a...
    iWave Systems
    last modified by iWave Systems
  • Flash Magic updates for LPC84x FAIM

    EmSA recently released some updates to FAIM support on LPC84x devices in their popular Flash Magic tool. If you are using this unique feature of the LPC84x device series be sure to update to version 12.65 or later to ...
    Brendon Slade
    created by Brendon Slade
  • MCUXpresso IDE v11.1.0 - Board SDK Creator

    NXP provides MCUXpresso SDKs that are configured for use with our standard evaluation boards. These can be used when carrying out your initial evaluation of our MCUs and early development work. However, in most cases ...
    LPCX presso support
    last modified by LPCX presso support
  • MCUXpresso IDE v11.0.1 LPC55xx Debug Hotfix

    Background  As part of the MCUXpresso IDE v11.0.1 release, we had to make some major changes to our LinkServer debugging mechanism to support the latest silicon revision of the LPC55xx family of devices (revisio...
    LPCX presso support
    last modified by LPCX presso support
  • Embedded Artists Winter sale - LPC54018 IoT Module for 5 Euros

    Embedded Artists are having a Winter Sale, offering the LPC54018 IoT module for only 5 Euros: LPC54018 IoT powered by Amazon Web Services (AWS) - Embedded Artists    The baseboard to accompany the module i...
    Brendon Slade
    last modified by Brendon Slade
  • DDR tool for i.MX

    This document introduces the double data rate (DDR) RAM configuration and validation tool, which is an embedded component of Config tools for i.MX.   The DDR tool has two components: DDR configuration tool and DD...
    Adrian Stoica
    last modified by Adrian Stoica
  • Config Tools for i.MX v7 Now Available

    We are pleased to announce that Config Tools for i.MX Application Processors v7 are now available.   The Config Tools for i.MX is a set of configuration tools that provide an efficient method for evaluation and...
    Petr Struzka
    last modified by Petr Struzka
  • MCUXpresso Ecosystem Enhancements

    NXP's MCUXpresso Software and Tools has expanded to include a new Secure Provisioning Tool, support for integrated third software solutions and has major improvements in the user experience for software selection. Thi...
    Devonna Dorton
    created by Devonna Dorton
  • New Secure Provisioning Tool and IDE, SDK, Config Tools Releases Now Available

    New versions of MCUXpresso SDK, IDE, and Configuration Tools are now available, along with a new Secure Provisioning Tool. Please see below to learn more about these updates updates and enhanced features in the new re...
    Megan Hansen
    last modified by Megan Hansen
  • MCUXpresso IDE v11.1.0 Now Available

    We are pleased to announce that MCUXpresso IDE v11.1.0 (build 3209) is now available. This is a major new version of the IDE, and contains many new features and enhancements over the previous MCUXpresso IDE v11.0...
  • 5V, Robustness, Touch and Motor Control? Get All That And More With The KE1xZ MCU Family

    The 5V KE MCU series has been designed to maintain high reliability and robustness in harsh electrical noise environments primarily targeting white goods and industrial applications, but now extending its success to c...
    Omar Cruz
    last modified by Omar Cruz
  • The Gigahertz MCU Era

    Announced in October, the i.MX RT1170 is NXP’s latest break-through technology within the i.MX RT series of Crossover MCUs.  What makes the i.MX RT1170 so cutting edge?   The i.MX RT1170 is the world&...
    Kathleen Jachimiak
    last modified by Kathleen Jachimiak
  • IMX8M mini mipi ov5640 is OK!

    开发板是imx8M mini,我们自己做的板子,使用官方镜像yocto 4.14.98,OV5640 mipi摄像头,验证及其测试: root@imx8mmevk:~# uname -a Linux imx8mmevk 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbea #1 SMP PREEMPT Thu Dec 12 08:23:58 UTC 2019 aarch64 aarch64 aarch64 ...
    jianfei chang
    last modified by jianfei chang
  • 移植开源的国密密码工具箱GmSSL到i.MX平台

    GmSSL是一个开源的密码工具箱,支持SM2/SM3/SM4/SM9/ZUC等国密(国家商用密码)算法、SM2国密数字证书及基于SM2证书的SSL/TLS安全通信协议,提供符合国密规范的编程接口与命令行工具,可以用于构建PKI/CA、安全通信、数据加密等符合国密标准的安全应用。GmSSL项目是OpenSSL项目的分支,并与OpenSSL保持接口兼容。因此GmSSL可以替代应用中的OpenSSL组件,并使应用自动具备基于国密的安全能...
    Xiaodong Zhang
    last modified by Xiaodong Zhang
  • LPC800 MCU Series: Entry-level 8-bit alternative MCUs, Priced Right 

    Based on the ultra-low-power Arm Cortex -M0+ Core the LPC800 MCU series offers a range of memory, small footprint and low-pin options for basic microcontroller applications. By being fully compatible with the Cortex-M...
    Omar Cruz
    last modified by Omar Cruz
  • Quick and Easy Development for Machine Learning and Artificial Intelligence at the Edge

    The next generation of machine interfaces is here. As embedded technology evolves, NXP continues to innovate with technologies like cloud-based/local voice control and face recognition for secure access/authentication...
    Nick Gonzalez
    last modified by Nick Gonzalez