• Crossover Code Challenge – Jump start your next design with these winning projects

    The Hackster Crossover Code Challenge might be over, but really, it’s just the beginning for you. Now it’s your chance to take advantage of all the ideas to jump start your next design.   The Crossov...
    Kathleen Jachimiak
    last modified by Kathleen Jachimiak
  •       "Mini-Monkey" Part 2: Using MCUXpresso to Accelerate the PCB Design Process

    In part two in this series on designing with the LPC55S69 VFBGA98 package,  I am going to show you how to use the NXP MCUXpresso SDK tools to help with physical design process.    Combining so...
    Eli Hughes
    created by Eli Hughes
  • "Mini-Monkey" Part 1: How to design with the LPC55S69 in the VFBGA98 package

    Now that we have discussed the LPC5500 series at a high level and investigated some of the cool features,  it is time to roll up our sleeves work on some real hardware.    In this next series of ar...
    Eli Hughes
    last modified by Eli Hughes
  • Unleashing a world of smart possibilities with iWave, Crank Software & the NXP i.MX8 series.

    iWave Systems and Crank Software partnered up to support rich graphics on the powerful NXP i.MX 8 series system on modules and SBC boards. Powered by NXP i.MX8 application processors, the SOM and SBC are optimize...
    iWave Systems
    last modified by iWave Systems
  • MCUXpresso Config Tools v7 Now Available

    We are pleased to announce that MCUXpresso Config Tools v7 are now available.   MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution. Fea...
    Petr Struzka
    last modified by Petr Struzka
  • MCUXpresso Secure Provisioning v1 Now Available

    We are pleased to announce that MCUXpresso Secure Provisioning Tool v1 is now available.   MCUXpresso Secure Provisioning Tools is a graphical user interface (GUI) tool covering the secure boot process, aimed pr...
    Petr Struzka
    last modified by Petr Struzka
  • MCUXpresso IDE v11.1.1 Now Available

    We are pleased to announce that MCUXpresso IDE v11.1.1 (build 3241) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v11.1.0, and we recommend that all existing ...
    LPCX presso support
    last modified by LPCX presso support
  • Debugging Kinetis KE0x MCUs with MCUXpresso IDE v11.1.1 (LinkServer)

    Please find attached a document detailing how to debug the Kinetis KE0x range of MCUs via LinkServer (CMSIS-DAP) debug connections using MCUXpresso IDE version 11.1.1 (or later).   This document and updates with...
  • Effortless GUI Development with NXP Microcontrollers

    More products today include graphical user interfaces than ever before, and consumers have a growing expectation that they be visually appealing and intuitive to use. Luckily, NXP and its partners make the process of ...
    Shelby Unger
    last modified by Shelby Unger
  • LPC5500 MCU Series: There's a lot under the hood  (Part 2 of 3) - Dual USB and Lots of RAM

    I recently wrote about the ample processing capabilities built into the LPC55S69 MCU. In this article I am going to highlight some very useful IO interfaces and memory.   Dual USB   One killer feature in s...
    Eli Hughes
    last modified by Eli Hughes
  • LPC5500 MCU Series: There's a lot under the hood  (Part 3 of 3) - SCT, "Programmable Logic" and Boot ROM

    I recently wrote about the ample processing capabilities built into the LPC55S69 MCU  in addition to the Dual USB capabilities and large banks of RAM.  Now it is time to explore some peripherals and features...
    Eli Hughes
    last modified by Eli Hughes
  • LPC5500 MCU Series: There’s a lot under the hood (Part 1 of 3)

    Most of my life, programming and embedded microcontrollers has been a passion of mine.  Over the course of my career I have gained experienced on many different architectures including some that are very speciali...
    Eli Hughes
    last modified by Eli Hughes
  • LPCScrypt v2.1.1 is now available

    LPCScrypt v2.1.1 | NXP  is now available. This release incorporates the latest versions of LPC-Link2 firmware for both CMSIS-DAP and also SEGGER J-Link.   LPCScrypt is a command-line based, fast flash (inte...
    LPCX presso support
    last modified by LPCX presso support
  • Ubuntu 18.04 LTS support for iWave's i.MX 8QM SMARC SOM and SBC Products

    The Debian based open-source Linux distribution Ubuntu finds its wide use across Desktop, Servers, Containers, and now in IoT and cloud applications. Being very secure and its OpenStack support, it is further getting ...
    iWave Systems
    last modified by iWave Systems
  • Longevity Extended to 15 Years on More than 100 MCU Devices 

    NXP understands that in addition to offering breakthrough innovations its ongoing investment and commitment to longevity is critical to being your trusted supplier. This paired with the continued demand and broad mark...
    Monica Velez
    last modified by Monica Velez
  • MCUXpresso IDE v11.1.0 SDK Handling Hotfix

    An issue has been identified in MCUXpresso IDE v11.1.0 with SDK 2.7 that in certain circumstances can cause the IDE to issue one or more erroneous duplicate file error popups when importing SDK examples or creati...
    LPCX presso support
    last modified by LPCX presso support
  • Modifying the latest Adafruit 2.8" LCD for SDK graphics examples

    Our MCUXpresso SDK is expanding to include more and more graphics examples, including LittleVGL and emWIN support for SPI-based LCDs. The examples we provide can be ported to different controllers, but are based/...
    Brendon Slade
    last modified by Brendon Slade
  • Powerful i.MX8 QM/QP SBC to Ease Development Challenges and Accelerate Innovations

    Oftentimes, developing an end application is like a scary game of maze. One can easily get lost in its winding paths lined with unseen twists and obstacles. A wrong choice can lead you to start all over again, making ...
    iWave Systems
    last modified by iWave Systems
  • QNX RTOS on iWave’s i.MX8QM/QP SMARC Module

    QNX is a Unix-like Real Time Operating System primarily developed for safety and mission critical embedded systems and includes the following unique features; Microkernel architecture Dynamically upgradable services a...
    iWave Systems
    last modified by iWave Systems
  • Flash Magic updates for LPC84x FAIM

    EmSA recently released some updates to FAIM support on LPC84x devices in their popular Flash Magic tool. If you are using this unique feature of the LPC84x device series be sure to update to version 12.65 or later to ...
    Brendon Slade
    created by Brendon Slade