• Effortless GUI Development with NXP Microcontrollers

    More products today include graphical user interfaces than ever before, and consumers have a growing expectation that they be visually appealing and intuitive to use. Luckily, NXP and its partners make the process of ...
    Shelby Unger
    last modified by Shelby Unger
  • LPC5500 MCU Series: There's a lot under the hood  (Part 2 of 3) - Dual USB and Lots of RAM

    I recently wrote about the ample processing capabilities built into the LPC55S69 MCU. In this article I am going to highlight some very useful IO interfaces and memory.   Dual USB   One killer feature in s...
    Eli Hughes
    last modified by Eli Hughes
  • LPC5500 MCU Series: There's a lot under the hood  (Part 3 of 3) - SCT, "Programmable Logic" and Boot ROM

    I recently wrote about the ample processing capabilities built into the LPC55S69 MCU  in addition to the Dual USB capabilities and large banks of RAM.  Now it is time to explore some peripherals and features...
    Eli Hughes
    last modified by Eli Hughes
  • LPC5500 MCU Series: There’s a lot under the hood (Part 1 of 3)

    Most of my life, programming and embedded microcontrollers has been a passion of mine.  Over the course of my career I have gained experienced on many different architectures including some that are very speciali...
    Eli Hughes
    last modified by Eli Hughes
  • LPCScrypt v2.1.1 is now available

    LPCScrypt v2.1.1 | NXP  is now available. This release incorporates the latest versions of LPC-Link2 firmware for both CMSIS-DAP and also SEGGER J-Link.   LPCScrypt is a command-line based, fast flash (inte...
    LPCX presso support
    last modified by LPCX presso support
  • Ubuntu 18.04 LTS support for iWave's i.MX 8QM SMARC SOM and SBC Products

    The Debian based open-source Linux distribution Ubuntu finds its wide use across Desktop, Servers, Containers, and now in IoT and cloud applications. Being very secure and its OpenStack support, it is further getting ...
    iWave Systems
    last modified by iWave Systems
  • Longevity Extended to 15 Years on More than 100 MCU Devices 

    NXP understands that in addition to offering breakthrough innovations its ongoing investment and commitment to longevity is critical to being your trusted supplier. This paired with the continued demand and broad mark...
    Monica Velez
    last modified by Monica Velez
  • MCUXpresso IDE v11.1.0 SDK Handling Hotfix

    An issue has been identified in MCUXpresso IDE v11.1.0 with SDK 2.7 that in certain circumstances can cause the IDE to issue one or more erroneous duplicate file error popups when importing SDK examples or creati...
    LPCX presso support
    last modified by LPCX presso support
  • Modifying the latest Adafruit 2.8" LCD for SDK graphics examples

    Our MCUXpresso SDK is expanding to include more and more graphics examples, including LittleVGL and emWIN support for SPI-based LCDs. The examples we provide can be ported to different controllers, but are based/...
    Brendon Slade
    last modified by Brendon Slade
  • MCUXpresso Config Tools v7 Now Available

    We are pleased to announce that MCUXpresso Config Tools v7 are now available.   MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution. Fea...
    Petr Struzka
    last modified by Petr Struzka
  • Powerful i.MX8 QM/QP SBC to Ease Development Challenges and Accelerate Innovations

    Oftentimes, developing an end application is like a scary game of maze. One can easily get lost in its winding paths lined with unseen twists and obstacles. A wrong choice can lead you to start all over again, making ...
    iWave Systems
    last modified by iWave Systems
  • QNX RTOS on iWave’s i.MX8QM/QP SMARC Module

    QNX is a Unix-like Real Time Operating System primarily developed for safety and mission critical embedded systems and includes the following unique features; Microkernel architecture Dynamically upgradable services a...
    iWave Systems
    last modified by iWave Systems
  • Flash Magic updates for LPC84x FAIM

    EmSA recently released some updates to FAIM support on LPC84x devices in their popular Flash Magic tool. If you are using this unique feature of the LPC84x device series be sure to update to version 12.65 or later to ...
    Brendon Slade
    created by Brendon Slade
  • MCUXpresso IDE v11.1.0 - Board SDK Creator

    NXP provides MCUXpresso SDKs that are configured for use with our standard evaluation boards. These can be used when carrying out your initial evaluation of our MCUs and early development work. However, in most cases ...
    LPCX presso support
    last modified by LPCX presso support
  • MCUXpresso IDE v11.0.1 LPC55xx Debug Hotfix

    Background  As part of the MCUXpresso IDE v11.0.1 release, we had to make some major changes to our LinkServer debugging mechanism to support the latest silicon revision of the LPC55xx family of devices (revisio...
    LPCX presso support
    last modified by LPCX presso support
  • Embedded Artists Winter sale - LPC54018 IoT Module for 5 Euros

    Embedded Artists are having a Winter Sale, offering the LPC54018 IoT module for only 5 Euros: LPC54018 IoT powered by Amazon Web Services (AWS) - Embedded Artists    The baseboard to accompany the module i...
    Brendon Slade
    last modified by Brendon Slade
  • DDR tool for i.MX

    This document introduces the double data rate (DDR) RAM configuration and validation tool, which is an embedded component of Config tools for i.MX.   The DDR tool has two components: DDR configuration tool and DD...
    Adrian Stoica
    last modified by Adrian Stoica
  • Config Tools for i.MX v7 Now Available

    We are pleased to announce that Config Tools for i.MX Application Processors v7 are now available.   The Config Tools for i.MX is a set of configuration tools that provide an efficient method for evaluation and...
    Petr Struzka
    last modified by Petr Struzka
  • MCUXpresso Secure Provisioning v1 Now Available

    We are pleased to announce that MCUXpresso Secure Provisioning Tool v1 is now available.   MCUXpresso Secure Provisioning Tools is a graphical user interface (GUI) tool covering the secure boot process, aimed pr...
    Petr Struzka
    created by Petr Struzka
  • MCUXpresso Ecosystem Enhancements

    NXP's MCUXpresso Software and Tools has expanded to include a new Secure Provisioning Tool, support for integrated third software solutions and has major improvements in the user experience for software selection. Thi...
    Devonna Dorton
    created by Devonna Dorton