• QN9080 - What is the maximum bandwidth in WUART profile

    Hello Team, I have a customer who plans to use #QN9080-001-M17 in their next platform design. he needs to transmit raw data (prefer using WUART profile) at a minimum of 1.25Mbps (I know this device support ...
    Shai Berman
    last modified by Shai Berman
  • K32W LPC tool

    I thought of another solution, but I wonder if it is feasible? Because multilink is not feasible on k32w now. Is it possible to use  LPC-link2 to connect to SWD . I don't know if this behavior can be used dire...
    Daniel Tseng
    last modified by Daniel Tseng
  • BLE RSSI

    I am making a call to Gap_ReadRssi shortly after the connection is established and I am getting RSSI readings of 0.  I expected to see a value of 127 (gGapRssiNotAvailable_d) or something correct (likely -50...
    Michael Brudevold
    last modified by Michael Brudevold
  • K32W CTS/RTS

     Because Uart coce of the original SDK only has TX/RX, neither will add CTS/RTS.   Does UART need to add CTS/RTS?
    Daniel Tseng
    last modified by Daniel Tseng
  • BT Firmware Init Failed

    Hi Team,   I was trying to load mbt8xxx.ko bt module on Ubuntu 18.04 (kernel 5.0.0-23-generic) ended with the above error.   Here are the logs :- [ 6837.045298] mmc0: new SDIO card at address 0001 [ 7124....
    Sadashiv Magadum
    last modified by Sadashiv Magadum
  • K32W: Timeout

    In the LPC-link2 USB connection: 1. When I entered the DK6 Flash Programmer, I found that the timeout jumped out,      how many seconds will it jump out of the DK6 Flash programmer? 2. When I d...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W (WIFI Co-existence)

    The documents on the NXP website do not provide WIFI Co-existence related documents(Pin settings, software timing diagram). Is NXP currently ready for this function(WIFI Co-existence)? If so, can it be released?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Flash Programmer

    K32W board needs to use FTDI_USB or USB_UART to execute Flash Prrogrammer. But usually Uart of SOC is directly connected to PIO8/PIO9(TX/RX) of K32W, and there is no FTDI_USB/USB_UART How does SOC do Flash Programmer?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W baud rate

    1. Update with "DK6 Production Flash Programmer".     I know that when using LPC-Link2 USB connection can not reach 1M baud rate, what is the default speed?     What is  the  highes...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W ISP mode

    If the SOC(Wifi module) is connected to K32W, can Uart Rom Bootloader(ISP mode) run to 1M speed with no CTS/RTS ?
    Daniel Tseng
    last modified by Daniel Tseng
  • RFID TAG

    Hello,   I am working on an automotive project and I need to find RFID tags that can be scanned from radius up to 300ft, along with the scanner for it.   Thank you
    Mahmoud Abdelhadi
    last modified by Mahmoud Abdelhadi
  • K32W FTDI interface can't work

    I use "LPC-Link2" for debugging can work, but it doesn’t work when I use "FTDI". FTDI : JP4&JP7 short 2 and 3. PC's USB connection Carrier Main Board show following: Use MCUXpresso IDE to download, it w...
    Daniel Tseng
    last modified by Daniel Tseng
  • Thread Router Eligible Device GPIO Control

    Hello community,   I've started a Thread project, which I intend to modify so that I control the LEDs of a node 2 over the air, pressing the switches in node 1. I'm currently using the "frdmkw41z_wireless_examp...
    Santiago Roman
    last modified by Santiago Roman
  • K32W ISP for LPC-LINK2

    Refer to "ch 2.5.2 ISP button" of UM11393 DK6 Production Flash programmer can be executed on FTDI USB interface. Can the DK6 Production Flash programmer be executed on LPC-Link2?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W: JN-UG-3127

    UM11394   NXP's official website cannot find this file(JN-UG-3127). I want to understand the meaning of each parameter  
    Daniel Tseng
    last modified by Daniel Tseng
  • USB-KW41Z  BLE sniffer does not decode Ethernet II "data". Missing wireshark plug in?

    USB-KW41Z  BLE sniffer does not decode Ethernet II "data" on wireshark. It is like the "kinetis adapter information" plug in does not work.   Set up: Windows 10 + wireshark 2.6.1 + Kinetis protocol an...
    Roberto Quilez
    last modified by Roberto Quilez
  • .sNwkStatusIndicationEvent.u8Status = 0x11

    Hi Mario,   JN5169 / AN1216 / SW4170   I cannot find the enum or the #define of the field u8Status in the structure ZPS_tsAfNwkStatusIndEvent. The stack is sending me this event often with status = 0x11. ...
    Benoit Roue
    last modified by Benoit Roue
  • K32W BLE MAC

    How to write BLE MAC? Where is BLE MAC written in Flash?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Python

    I study UM11394: "IoT_ZTBGetting Started" has the following problems: 1. Why K32W need to install Python?(Do not understand his purpose, the previous chip did not require this to install python) 2. Does FTDI and L...
    Daniel Tseng
    last modified by Daniel Tseng
  • Where can I download the source program of the FRDM-KW38 resident example?

    Hi everyone.    I'm using a FRDM-KW38.   It is introduced in the  Quick Start Guide of FRDM-KW38 that when frdm-kw38 is powered on for the first time,  the LED will blink, and the s...
    Liu chengwu
    last modified by Liu chengwu