• KW41 Proximity Reporter

    I have studied ch5.5 Proximity Reporter of BLE Demo Applications User's Guide.pdf. This example is divided into two parts: 1. "Immediate Alert"     Press High or Middle will immediately show different lights...
    Daniel Tseng
    last modified by Daniel Tseng
  • QN908x OTAP_Clinet_ATT won't work

    Dear Sir            I can’t see NXP_OTAA in IOT Tool box after I follow API Guide based on newest QN9080 SDK.            Could yo...
    Li-Chin Wang
    last modified by Li-Chin Wang
  • KW41Z ZigBee Write Attributes Response

    Grettings,   I'm working with a KW41Z and MCUXpresso. I have a ZigBee router as server and a ZigBee end device as client. The end device as source sends an Write Attributes command to Zr  and I need to know...
    Alejandro Velez
    last modified by Alejandro Velez
  • mode of mkw36a512vfp4

    1)The names of pin 10 and 12 are both DCDC_ LN, and the two names are the same.    Why? How to use it? 2)The advantages and disadvantages between buck mode and bypass mode in the mkw36a512vfp4,  ...
    Bin Wang
    last modified by Bin Wang
  • I want to know, can 640K FLASH of JN5189 be used as a memory?

    Can the data be stored to 640K FLASH of JN5189 when the program is running? Thanks for your time.
    hs q
    last modified by hs q
  • KW36 GATT Client  read characteristic descriptors

    Environment: Two FRDM-KW36 installed 「Wireless Uart」 We want to add GattClient_ReadCharacteristicDescriptor () to read characteristic on the GATT client side of wireless Uart  and  GattClient_WriteCharacter...
    Daniel Tseng
    last modified by Daniel Tseng
  • Zigbee end device transmission message in network

    Hi everybody!   I am new to Zigbee network, I used some JN5169 modules from NXP to create Zigbee network and I used JN516x ZigBee SDK for development. But I have an unclear problem, hope you can help me. Does t...
    Dai Nguyen
    last modified by Dai Nguyen
  • Can not Read/Write long attributes on GATT Client in KW41Z BLE Stack

    Hi,   I need to program a BLE Central using GATT Client API to read and write a characteristic with 255 bytes. After connection, getting MTU is 247. In the BLE Application Developer's Guide saying The GATT Cli...
    HUNG PHAM
    last modified by HUNG PHAM
  • KW41Z controlled from another MCU Host Device

    Hello Juan Carlos Pacheco,   maybe you or someone else could help me with my little project. I want to control the KW41Z Chip, which is on the FRDM-KW41Z board, from a host system via the UART0 on the PinHeaders...
    Steffen Jahnke
    last modified by Steffen Jahnke
  • [JN-AN-1172] include library fail?

    Dear Sirs,   I follow the JN-AN-1186 to inlucde libRecal_JN5169.a, as below:   INCCFLAGS += -I$(COMPONENTS_BASE_DIR)/HardwareApi/Include/ INCCFLAGS += -I$(COMPONENTS_BASE_DIR)/Recal/Include/ LDLIBS += libR...
    alan lin
    last modified by alan lin
  • KW41Z -  concurrent operation of stack's

    Hi,   I found information, that KW41Z support concurrent operation of wireless comunication. Is there documentation on how to do this?   In MCUexpresso middleware selection does not work when I create pr...
    Adrian Chmiel
    last modified by Adrian Chmiel
  • Why is the return value of ZPS_eAplZdoRejoinNetwork(TRUE) 0xa3?

    Hello, the chip I used is JN5169.I recently encountered a problem when I called the ZPS_eAplZdoRejoinNetwork(TRUE) function in my project and it returned 0xa3, meaning ZPS_APL_APS_E_ILLEGAL_REQUEST.When this error occ...
    震 孙
    last modified by 震 孙
  • Ble Kw41z multiple peripheral device at the same time

    Hello everyone, i'm trying to modify a device with Ble stack inside a kw41z that use wireless uart nxp demo. My fw is ok and it "speaks" with a smartphone app without problems. Now i need to program more of one devi...
    marco mangraviti
    last modified by marco mangraviti
  • Reboot will be caused immediately as soon as it received Socket Bind command for the TCP protocol + Stream socket type. 

    Hello Sir,       Does anybody has the fiollowing experience in Thread code with KW41 ? We used router Eligible Device code loading into FRDM-KW41 and tried to create, bind and liste...
    Jason Chiang
    last modified by Jason Chiang
  • Example code for IAS Zone cluster for JN5189

    Hi,   I am exploring JN5189 for ZigBee. I have set-up MCUXpresso IDE v11.1.1_3241 in my windows machine and also downloaded SDK_2.6.0_JN5189DK6.   I am doing the feasibility on JN5189 for the ...
    Ankit Patel
    last modified by Ankit Patel
  • 602 and 612 RF mixers

    Hello,   I am investigating the old 602 and 612 RF mixers (Gilbert cell) and try to know what are the differences. I was reading both datasheets and both seems the same except in the Icc max current where 602 dr...
    Javier Romo
    last modified by Javier Romo
  • What does this status means ZPS_APL_ZDP_E_NOT_ACTIVE?

    Hello Every One, Some stack related details. stack : JN-SW-1470 build version : 1840 application : JN-AN-1217   Here i am trying to send report attribute manually for power,temperature and humidity with addre...
    jay prajapati
    last modified by jay prajapati
  • HW kill-switch for BLE on QN908x

    Hello,   On QN908x is there a hardware register kill-switch bit for the entire BLE periphery? Sometimes it just refuses to shutdown to PD0. Happens like once in 1800-32400 shutdowns. We need to use CPU r...
  •       JN5168-001-M00Z Eagle Library

    Hello,   I have purchased a JN5168-001-M00Z module, and a would like to make a breakout board (breadboard friendly) in order to try this module. I would like to know if you have the associated Eagle library (sy...
    Thomas Coin
    last modified by Thomas Coin
  • In Ble how to Send data from client to server and control the led

    Hello Team,  I'm a beginner in rigado r14z  Currently working on BLE  In that can anyone explain how to send the data from the client to the server and with that data I need to control the led of the...
    Manoj Kumar
    last modified by Manoj Kumar