RFIDDISCOVER CLI tool? Hello, I just wanted to know if a CLI tool is available to use for the RFIDDISCOVER software? I would like to write a script that sends a set of fixed commands to the device instead of having to manually input... KW36 required: RSA 1024 algorithm library support Hi, The current nxp sdk of kw36 does not support RSA 1024 encryption/decryption algorithm. Will nxp be able to add RSA-1024 code in our framework in the nxp sdk we have? Regards Sai... QN9080 -- How to use ISP Command I checked Ch 7.5 UART ISP of UM11023 I shorted JP15 into ISP mode, 1. There is no response from UART input 0x33? 2. If 0x33 is OK, how to input clock,baud rate,and CRC? (0x71 0x50 0x08 ? ? ? ) ... Gap_LoadEncryptionInformation will make chip crash when in secure connection mode Hi, about the API Gap_LoadEncryptionInformation, it is work fine while using the legacy pairing mode, but will make chip crash when in secure connection. Regards, Ziv JN5169 Control PA Hi all, I have a plan to design new USB dongle JN5169 with PA SE2431L. Because cost down, I don't want to use IC 74HC1G32 (file attach). That mean JN5169 must control PA directly. Is that possible??? jn5169 an1218 transmit power Hi NXP: As jn5169 datasheet mention, the tx power can be set 10, 8.5 or 3 dbm I'd want to ask how to set in the an1218 example? Thanks a lot Chris KW36 : Pairing getting failed sometimes in huawei P8 Hi, I try to pair Huawei P8 with KW36. I have imported hid device example with security mode 1 and level 2. I use just works pairing. Sometimes i see pairing is getting failed , can you please let me know w... KW36: Pairing request not initiated by iphone to KW36 in some half paired scenario Hi, I use KW36 with hid device example and my kw36 acts as a peripheral (slave) device. Mode 1 level 2 is security. I try the following usecase 1 : (a) Pair ios with kw36. (b) Delete the ... About output state in the OFF state Hi, all. As BGU8007, BGU8009 and BGU8103 has ENABLE pin. ENABLE=Low means OFF state according to the datasheet. Does output become to Hi-Z when OFF state? best regards, tomo How to enable QN9080 Coexistence? In the "connectivity Framework Reference" document, it is mentioned that MWS_CoexistenceEnable () can turn on the coexistence of QN9080. 1。I need to enable gMWS_UseCoexistence_d ,but MWS_coexistenceInit() i... QN9020 : What are the connection parameters stored in NVDS? Hi, Can you please let me know what connection parameters are stored in the NVDS by the stack? From nvds.h file, I found an "enum NVDS_TAG" with values like "NVDS_TAG_BD_ADDR... Zigbee Task with KW41Z Hello, I have this function, in the End Device SDK Example of MCUXpresso, to send a dummy write attribute command to a custom attributes arleady created in another node in the network with that Short Address: ... High CPU Utilization during BLE Scan caused by hsdk threads Hi, We are running a BLE scanning test process by using hsdk library to communicate with the NXP bluetooth chip to preform BLE scan. After this test process starts scanning by calling GAPStartScanningRequest function ... How to change ble device name (kw41z) with more of 8 characters? Hello, i need to change the ble device name in a firmware for kw41z. Into app_config.c file, there is an gapAdStructure_t array named advScanStruct[3]. The last element of this array contains: .adType =... Where the file ZigbeeControlBridge_JN5169.bin can be downloaded? I'm following the applicaiton note : JN-AN-1223. On Page 2, we need to download the firmware : ZigbeeControlBridge_JN5168.bin Where should I download this file? KW36: "LL_FEATURE_RESP" not sent from KW36 when some phone request "LL_FEATURE_REQ" Hi, I am using KW36. I use hid device example and try to pair vivo x25 I tried connecting 14 times, pairing 11 times with Vivo X25, second time connect req(FrameNo: 26951) , we see LL_FEATURE_RE... KW35 Bluetooth authentication modulation wave testing problem When we certified the MKW35A512, the wireless council required testing of single carrier and modulated waves at 2.402GHZ and 2.480GHZ transmission frequencies.The single carrier test can be passed, but the modulation ... CLRC663 Plus & HTRC110 CE Certified ? Do either of the following have CE Certification ? CLRC66303 HTRC110 Thanks in advance. MKW41Z512-HT mass erase Hi expert, I was try to program and read the flash in MKW41Z512, when I program, I do mass erase first, and it could erase and program successful, but after that, I restart ( power off then power on)... Does KW41Z's HCI support TX power adjustment? Use example of hci_black_box on KW41Z SDK 2.2.1. Find #define gHciSetTxPowerCommand_c 0x012D "vendor_debug_commands.h" is no define any function. Does this TX power command feature allow custome...