• kw41z power consumption

    Use SDK example "power manager(A)" and "smac low power node(B)" to test power consumption Use Hardware FRDM-KW41Z- ver A3   Measurement point is SH504   Question: 1. Why is there such a big difference in po...
    Daniel Tseng
    last modified by Daniel Tseng
  • Problem building JN-AN-1218 for LPCXpresso

    Greetings, I am trying to build the JN-AN-1218 application note with LPCXpresso and JN-SW-4270 SDK. System I use is Windows 7, the version I use is as stated below, JN-AN-1218-v1008 JN-SW-4270-Zigbee 3.0-v1841 LPCXp...
    Chee Kit Au
    last modified by Chee Kit Au
  • How to use more than one application of IOT toolbox in one code?

    Hello,   I am new in development with NXP KW36 module. My requirement is to create one project which have below functionalities:    1. wireless uart    2. Over the air programming...
    Chintan Patel
    last modified by Chintan Patel
  • FORMAT DESFIRE EV2

    Hello, i can't format my desfair ev1 card, after authentication in app 00 (root) i send format command and recive next answer: f2 01 after which I can not use the card. How right format the card? I trying se...
    Leonov Dima
    last modified by Leonov Dima
  • How to get the Software development material about JN5189

    Such as  "JN518X Integrated Peripherals API User Guide"  And why can't  I download the "JN5189(T)/JN5188(T) User manual"
    德平 吕
    last modified by 德平 吕
  • NTAG I2C explorer kit not working

    Hi, i have bought NTAG I2C explorer kit. i have went through all manuals and guide.   while i m trying to operate with smartphone.i m not seeing functionality.   i hope so, by default(taken out from box)...
    afrid thenebanda
    last modified by afrid thenebanda
  • QN908x OTAP_Clinet_ATT won't work

    Dear Sir            I can’t see NXP_OTAA in IOT Tool box after I follow API Guide based on newest QN9080 SDK.            Could yo...
    Li-Chin Wang
    last modified by Li-Chin Wang
  • Using Battery Monitor in QN9080

    Hello All, I am Using QN9080 and want to use the Battery Monitor to be able to get battery levels at any time I am trying to edit ADC Temperature senor Example  but I think it is not as simple as just changing ...
    Karim Osama
    last modified by Karim Osama
  • return E_ZCL_FAIL when register endpoint

    My application have 4 endpoint. If I dont import OTA Upgrade, I still can control these 4 endpoint. But, when I import OTA Upgrade, I can not control any Endpoint, but EP 1. In UART log, I see error when register EP ...
    Giau Nguyen
    last modified by Giau Nguyen
  • QN9090 debug issue

    Hello team, I am trying to debug and run an example code with QN9090 but without a success, please find below my error screen and error log while (trying to) debug. it looks like an issue with the GBD toolchain whil...
    Shai Berman
    last modified by Shai Berman
  • jn5169 Zigbee Route reply

    We have configured jn5169 zigbee as co-ordinator. We have connected the same to multiple sensors including gas leak sensor. We notice that in some cases co-ordinator stops sending route reply to route request received...
    Hariprasad Anumala
    last modified by Hariprasad Anumala
  • Send request enroll - IAZone Cluster !!!

    Hi support team !!! Now I'm working with IASZone Cluster Base on JN-AN-1201-Zigbee-Intruer-Alarm-System (ZONE). I build a project for my sensor - JN-AN-1217-Router There are something have modified: - Add cluster IAS...
    Tran Minh Tan
    last modified by Tran Minh Tan
  • Range issue in Zigbee

    We are evaluating range problem in of our zigbee products  For setting the Transmit Power we are using the below API and for enabling external PA we are configuring the below GPIOs       vI...
    Hariprasad Anumala
    last modified by Hariprasad Anumala
  • Some questions about routing devices

    Hello, I have three questions to ask for some help.   First: for the routing devices that have already entered the network, is it possible to change the node network state of the device under any circumstances or...
    震 孙
    last modified by 震 孙
  • BLE Border Router with FRDM-KW41Z as a Radio

    Hi Team, Currently i'm working on Openthread Border router(Rasberrypi) with FRDMKW41Z as a radio. I have gone through IOT SDK(Nrf5) for enabling the 6lowpan BLE Border router using raspbeery pi. But they are connect...
    Ramya Venkatesha
    last modified by Ramya Venkatesha
  • How to use Differential A/D on KW41z?

    I see the user guide has this set of circuits, maybe it can test read differential A/D (ADC0_DM0 and ADC0_DP0). Does SDK have a corresponding example that can be used directly? I haven't found this example so far. &...
    Daniel Tseng
    last modified by Daniel Tseng
  • QN9090 BLE SDK into debug fail with MCUXpresso

    Hi all,    I get QN9090-DK006 and download "SDK_2.6.0_QN9090DK6" to import into MCUXpresso. But after I build one project to into debug mode to get below status. it don't from main() like user guid...
    Ethan Chen
    last modified by Ethan Chen
  • 88w8987 bt class 2

    Hello,   I'm trying to update bt power class of the 88w8987 and I haven't succeed yet. Their is no information in the datasheet and labtool is still failing.   What can I do ?   Best, Eric Delanghe...
    Eric Delanghe
    last modified by Eric Delanghe
  • Flash mac address 88w8987

    Hello,   I want to flash new mac address in 88w8987. Using labtool I use the sequence: 2 => Use Bluetooth Successful connect to hci1 45 => Read MAC from OTP Get 41.41.41.41.41.41 46 aa.bb.cc.dd.ee.ff ...
    Eric Delanghe
    last modified by Eric Delanghe
  • JN5169  Error?

    Why is there so many errors in a new official project?    
    DING JINKE
    last modified by DING JINKE