• [JN-SW-4170] Which API is for "Read Attributes" Response?

    Dear Sirs,   According to Chapter 2.2.1.1 of JN-UG-3103 ("Reading a Set of Attributes of a Remote Cluster"), the Destination Node will send "Read Attributes" response to the Source Node. Where can I find the .c...
    alan lin
    last modified by alan lin
  • Setting CLK_OSC32M_DIV to 0 results in runtime error

    Hello team, My customer is trying to maximize the throughput of the processor, by minimizing the clock's divisions. please find his inquires below:   1) My specific question is: how to change the CLK_OSC3...
    Shai Berman
    last modified by Shai Berman
  • [JN5169 with DR1174 carrier board] The usage of SPI interface?

    Dear Sirs,   I tried to Read the Status Register (RDSR) of the SPI flash on DR1174 carrier board. (In order to try the SPI interface, I did not use the flash memory API) However, I can not get the correct resp...
    alan lin
    last modified by alan lin
  • PPP connection with GPRS modem and FRDM-K64F

    Hi,   Is there any guide or example for establishing ppp connection with FRDM-K64F and GPRS modem (BG96). I have read some of posts GPRS demo - FRDM-K64F vs MQX 4.2 vs BGS2T modem - working now  yet I...
    Darshan Shah
    last modified by Darshan Shah
  • KW36 IOT Toolbox (APP)

    KW36 OTA update from mobile phone to peripheral that use IOT Toolbox(APP) on the mobile phone side. If we want to develop our own APP on phone, What information can NXP provide (e.g. flow chat、PDF ...) for our refer...
    Daniel Tseng
    last modified by Daniel Tseng
  • Can we have both USB and BLE functionality on QN908x Chip simultaneously

    I want to try both USB and BLE functionality on QN908x development board. Individually, I am able to run HID mouse example code for USB as well as BLE from SDK2.2.1. But, I want to have both the functionality in the s...
    Ankur Rathi
    last modified by Ankur Rathi
  • About switch image for JN518x

    I can switch to inactive image, but this image must program to address 0x48000.(288KB) My project does not need such a large reserved space (e.g. 123KB). Therefore, I want to configuration the flash layout for less ...
    Teddy Zheng
    last modified by Teddy Zheng
  • KW36 Bluetooth Address

    Hello,   sorry that I am asking that question again. I know it was discussed in other Post in this Forum, but I never seen an answer that answers my question to 100%.   So, my question is. Do I have to purch...
    Lukas Berger
    last modified by Lukas Berger
  • The FRDM-KW36 can't connect with smart phone

    Hello All ~              I have used the button to config the FRDM-KW36 as a peripheral device for to connect to the smart phone. Although the smart ph...
    sihan chen
    last modified by sihan chen
  • How to use push button of FRDM-KW36 to connect with peripheral device

    Hello ~            I am working on FRDM-KW36 development board and use (frdmkw36_wireless_examples_bluetooth_w_uart_freerots) SDK to build code by MCUXpresso IDE.    I have...
    sihan chen
    last modified by sihan chen
  • How to modify gatt_bd.h for UART read service

    HI All,           I would like to add a service for UART read and I have modified the characteristic values that show as red word. but I don't know how to setting the data size, co...
    sihan chen
    last modified by sihan chen
  • How to get frequency register of KW41Z

       Using KW41's GenFsk in MCUXpresso IDE environment.     Research program can't find the last place to write register.       Question:    1. Channel range 0 ~ 127, wh...
    Daniel Tseng
    last modified by Daniel Tseng
  • Schematic for MHT1008N reference circuit?

    Hi NXP Team!   I am trying to design an RF amplifier using your MHT1008N.   However, since I want to do the simulation on ADS,  is there any reference where I could see and analyze the schematic ...
  • Can not Read/Write long attributes on GATT Client in KW41Z BLE Stack

    Hi,   I need to program a BLE Central using GATT Client API to read and write a characteristic with 255 bytes. After connection, getting MTU is 247. In the BLE Application Developer's Guide saying The GATT Cli...
    HUNG PHAM
    last modified by HUNG PHAM
  • [ZGWUI tool] Usage of Read Attrib of General Tab?

    Dear Sirs,   About GUI tool of "ZigBee Gateway User Interface", how to set the parameters for "Read Attrib"?   Thanks!
    alan lin
    last modified by alan lin
  • Can I setting "Route Record Table Size" to more than 255?

    It is not allowed in "ZPS Configuration Editor". but in the generated source(zps_gen.c), the ZPS_tsNwkNibTblSize.u16Rct(nwkRouteRecordTable size) is type of uint16. Should I ignore the limit of "ZPS Configuration...
    Teddy Zheng
    last modified by Teddy Zheng
  • ZigBee 3.0 - connect up to 100 nodes

    We are using ZigBee 3.0 and JN-AN-1229-ZPS-Application-Template. We are having the problem of  the connection for 100 nodes. We are connecting 1 coordinator, 40 routers and 60 end devices. Some of the nodes ...
    Jia Na Lai
    last modified by Jia Na Lai
  • How to configure QN908x for the continuous SCAN mode? And to scan more than ten devices.

    How to configure QN908x for the continuous SCAN mode? And to scan more than ten devices. We tried to test this feature [always scan mode] using Wireless UART (freertos version) example code - where we commented...
    Kishan Saralaya
    last modified by Kishan Saralaya
  • [JN-AN-1218] [Light Bulb] response for On/Off?

    Dear Sirs,   Using the ZGWUI to send On/Off/Toggle command to a Light-Bulb device, we can see the response message (ex: Type:0x8000 and others) showing on ZGWUI.  My questions are: 1. In which API of the ...
    alan lin
    last modified by alan lin
  • simultaneous  connecctions of BLE

    Hi, I want to use KW36 as central to connect several BLE keys. And I have referred the DOC "Multiple Connections in Bluetooth LE Central Device ". This demo looks like, each time only one BLE temp sensor can be ...
    yanpo li
    last modified by yanpo li