• QN9080 - PWM problem

    Hello Team,   my customer has the following issue, could you please advise the below:   I am having a problem with using the SCTimer module on QN9080. The interrupts do not seem to work properly, the interru...
    Shai Berman
    last modified by Shai Berman
  • NXH3670- Couldn't find kl device

    When I use the NXH3670 flash tool, I could not connect to the dongle device, but I can connect to the headset device. The dongle device was debugged by the MCUXpresso IDE with the kl_dongle_sdk project successfully, I...
    haitaoxing@hotmail.com
    last modified by haitaoxing@hotmail.com
  • Using a different pre-configured link key with JN-AN-1216 ControlBridge

    Hi,   I am trying to set a different pre-configured link key for the JN-AN-1216 ControlBridge using JN-SW-4170 version 1840 (the latest), but the control bridge's coordinator is using the '09 key no matter what ...
    Pierre-Luc Drouin
    last modified by Pierre-Luc Drouin
  • KW36  multitask

    I try to add those sample code in frdmkw36_wireless_examples_bluetooth_w_uart_freertos wireless_uart.c: void test_task(void* argument) {    while(1) {       Serial_Print(gApp...
    mo xinyu
    last modified by mo xinyu
  • MWCT1013 Source Code/JTAG?

    Hello, I am running into some issues using Freescale CodeWarrior USB TAP (hardware) and CodeWarrior and FreeMASTER (software). My device isn''t recognized. I cannot find any drivers for this. The tap came with no docu...
    wpsigma
    last modified by wpsigma
  • Disabling Default Response when sending attribute report?

    Hi,   I am trying to disable Default Reponse when sending an attribute report with eZCL_ReportAttribute, but I am unable to get it to work. I have ZCL_DISABLE_DEFAULT_RESPONSES set to TRUE in my zcl_options.h fi...
    Pierre-Luc Drouin
    last modified by Pierre-Luc Drouin
  • How to use more than one application of IOT toolbox in one code?

    Hello,   I am new in development with NXP KW36 module. My requirement is to create one project which have below functionalities:    1. wireless uart    2. Over the air programming...
    Chintan Patel
    last modified by Chintan Patel
  • Flash mac address 88w8987

    Hello,   I want to flash new mac address in 88w8987. Using labtool I use the sequence: 2 => Use Bluetooth Successful connect to hci1 45 => Read MAC from OTP Get 41.41.41.41.41.41 46 aa.bb.cc.dd.ee.ff ...
    Eric Delanghe
    last modified by Eric Delanghe
  •    Bee Stack: Need Help with Analog-to-Digital Conversion

    have created a BeeKit solution for the MC1321x-SRB using HCS08 BeeStack codebase, and imported into CodeWarrior, the PLM folder includes the Analog-to-Digital (ADC) component, with the files "ADC_Interface.h", "ADC.h...
    Erwin Beck
    last modified by Erwin Beck
  • How to enable QN9080 Coexistence?

    In the "connectivity Framework Reference" document, it is mentioned that MWS_CoexistenceEnable () can turn on the coexistence of QN9080.   1。I need to enable gMWS_UseCoexistence_d ,but MWS_coexistenceInit() i...
    Daniel Tseng
    last modified by Daniel Tseng
  • How to use vSetPwm() function

    Hi,  I use jn1189 project. In the Driverbulb_Dr1221_Mic. C file, how does vsetpwm() function understand?                   The code is as follows:    ...
    Daniel li
    last modified by Daniel li
  • [KW21Z] For compatibility with other zigbee IC. (Not NXP device)

    Hello    I am considering developing a co-ordinator using KW21Z based Zigbee 3.0 stack. But I have concerns to implement co-ordinator for compatibility.   According to ZigBee 3.0 Devices Use...
    Young Koo Jeong
    last modified by Young Koo Jeong
  • Routing problem after moving Router far away from Coordinator

    Hi all,   Currently, I got a routing problem occurs when I tested a Zigbee network between a Coordinator and a Router. The test's steps are described below: 1. Coordinator is a USB Dongle and  is used JN-A...
    Thanh Pham
    last modified by Thanh Pham
  • How to use Serial Flash Memory (USB dongle)?

    Hi support team! Now i'm working on JN-AN-1216 ControlBridge.  I'm having a trouble with JN5169 memory. If i define a large struct =>> It make crash program. My understanding is that Zigate is un...
    Tran Minh Tan
    last modified by Tran Minh Tan
  • Problem when creating custom devices based on JN-AN-1189

    Hi. I guess the problem is me and i have missed something obvious, but i am stuck with this one for afew days.   I want to create custom devices firmware based on JN-AN-1189 I can build successfully each of the...
    Tim Gros
    last modified by Tim Gros
  • MKW41Z troubles using MWS module for BLE and 802_15_4 coexistence on same IC

    Hi everyone, I have a question about the co-existence of the BLE and 802_15_4. I am using MKW41Z microcontroller with IAR. I am able to switch radio from the BLE to 802_15_4 and vice versa through MWS module.  A...
    vanaja guduru
    last modified by vanaja guduru
  • Exporting Persistent Data on JN516x to Host

    Hi all, As I know, the ZigBee Control Bridge node by default uses the internal EEPROM to hold persisted data. This is about 4KByte in JN5169 device and can restrict network size. To overcome this, we need to export ...
    Giau Nguyen
    last modified by Giau Nguyen
  • Gas Leak sensor not sending IAS Zone notifications

    Hi ,    We are working with NXP (JN5189) as co-ordinator and pairing multiple zigbee sensors.  Test Setup Gas leak sensor is provisioned with smart cable. Sensor keeps sending gas leak events. After c...
    Hariprasad Anumala
    last modified by Hariprasad Anumala
  • ZPS_EVENT_NWK_LEAVE_INDICATION event does not occur when the End Device leave.

    Coordinator changed from Zigbee 1.2(JN-AN-1223) to Zigbee 3.0(JN-AN-1216). ZigBee 3.0 does not receive leave event of the end device.   Environment When no event occurs (ZPS_EVENT_NWK_LEAVE_INDICATION ) - zigb...
    Seung Ho Kim
    last modified by Seung Ho Kim
  • ZeD cannot find "Zigbee coordinator"

    I am trying to put together this home automation system from 2010. I installed codewarrior development studio and beekit wireless connectivity toolkit. And then I followed Beestack step-by-step demonstration up until ...
    Pratiksha Shukla
    last modified by Pratiksha Shukla