• The route did not forward the command to the destination address

    Hi, We used JN5169 to make a light control system,but now I found a problem, sometimes, the button can not control the light.Packet capture found that the button sent the command to the route, but the route did not f...
    德平 吕
    last modified by 德平 吕
  • K32W FTDI interface can't work

    I use "LPC-Link2" for debugging can work, but it doesn’t work when I use "FTDI". FTDI : JP4&JP7 short 2 and 3. PC's USB connection Carrier Main Board show following: Use MCUXpresso IDE to download, it w...
    Daniel Tseng
    last modified by Daniel Tseng
  • Thread Router Eligible Device GPIO Control

    Hello community,   I've started a Thread project, which I intend to modify so that I control the LEDs of a node 2 over the air, pressing the switches in node 1. I'm currently using the "frdmkw41z_wireless_examp...
    Santiago Roman
    last modified by Santiago Roman
  • K32W ISP for LPC-LINK2

    Refer to "ch 2.5.2 ISP button" of UM11393 DK6 Production Flash programmer can be executed on FTDI USB interface. Can the DK6 Production Flash programmer be executed on LPC-Link2?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W: JN-UG-3127

    UM11394   NXP's official website cannot find this file(JN-UG-3127). I want to understand the meaning of each parameter  
    Daniel Tseng
    last modified by Daniel Tseng
  • USB-KW41Z  BLE sniffer does not decode Ethernet II "data". Missing wireshark plug in?

    USB-KW41Z  BLE sniffer does not decode Ethernet II "data" on wireshark. It is like the "kinetis adapter information" plug in does not work.   Set up: Windows 10 + wireshark 2.6.1 + Kinetis protocol an...
    Roberto Quilez
    last modified by Roberto Quilez
  • .sNwkStatusIndicationEvent.u8Status = 0x11

    Hi Mario,   JN5169 / AN1216 / SW4170   I cannot find the enum or the #define of the field u8Status in the structure ZPS_tsAfNwkStatusIndEvent. The stack is sending me this event often with status = 0x11. ...
    Benoit Roue
    last modified by Benoit Roue
  • K32W BLE MAC

    How to write BLE MAC? Where is BLE MAC written in Flash?
    Daniel Tseng
    last modified by Daniel Tseng
  • Unable to receive 802.15.4 beacon frame when coordinator in beacon mode

    I'm unable to receive 802.15.4 beacon frame when using beacon mode.   I have imported frdmkw41z_wireless_examples_ieee_802_15_4_mwa_coordinator_freertos as a coordinator and frdmkw41z_wireless_examples_ieee...
    Paweł Górski
    last modified by Paweł Górski
  • K32W Python

    I study UM11394: "IoT_ZTBGetting Started" has the following problems: 1. Why K32W need to install Python?(Do not understand his purpose, the previous chip did not require this to install python) 2. Does FTDI and L...
    Daniel Tseng
    last modified by Daniel Tseng
  • Stack dump in sdk when create an attribute new from cluster basic 

    Dear All,   I want create an attribute contain 100 byte data of cluster basic from router. I user router is module chip jn5169, JN-AN-1217 sofware and sdk JN-SW-4170. The step are described below: 1...
    Dang Thanh Nha
    last modified by Dang Thanh Nha
  • Where can I download the source program of the FRDM-KW38 resident example?

    Hi everyone.    I'm using a FRDM-KW38.   It is introduced in the  Quick Start Guide of FRDM-KW38 that when frdm-kw38 is powered on for the first time,  the LED will blink, and the s...
    Liu chengwu
    last modified by Liu chengwu
  • QN9020 eddystone

    hi Can QN9020 be changed to eddystone? If there is any reference case procedure? Thank you!
    qq2_2ww qq2_2ww
    last modified by qq2_2ww qq2_2ww
  • Use DBG_vPrintf() with IEEE 802.15.4 Application

    Hi, I simply trying to print into a terminal  using DBG_vPrint  I have tried so many combinations but no matter what I cant get the uart to print into a terminal.   I am using a JN-5169 dongle with Be...
    Alberto Gallegos
    last modified by Alberto Gallegos
  • JN-AN-1217 ZTIMER_eStart() FAIL ?

    Greetings;   I'm using JN-AN-1217 (base device / router) for JN5169, in app_zcl_task.c / APP_ZCL_vInitialise() / ZTIMER_eStart(u8TimerZCLTick, ZCL_TICK_TIME) <-- Fails! debug output: APP: Failed to Star...
    Christopher Veeneman
    last modified by Christopher Veeneman
  • Programming  JN516X by off-board

    I am a programmer developper. I am searching for a way to program to JN516X internal flash memory by off-board. I guess that it is possible by the serial interface to communicate with the boot loader. Is my understand...
    Tomonori Tsujiyama
    last modified by Tomonori Tsujiyama
  • KMA221 programming device problem

    KMA221 is a programmable angle sensor.KMA221 has been selected. In order to improve production capacity and product quality, our company is transforming the production line, involving programming equipment.I would lik...
    克祥 黄
    last modified by 克祥 黄
  • K32W(BLE+OpenThread)

    I need to implement BLE+OpenThread, I found the following information:   1. Doc/readme.txt :  Please refer to "OpenThread Demo Applications User Guide.pdf" but I don't know where to start, can you guide m...
    Daniel Tseng
    last modified by Daniel Tseng
  • Will NTAG 5 I2C Cockpit example run on LPC54114 ?

    Greetings, I figured that one easy way to experiment with the NTAG 5 NFC chip for a prior project - which used the LPC54114 Xpresso board - was to order some NTAG 5 Boost Dev Boards.  I have two issues: 1 - I ...
    James Whitney
    last modified by James Whitney
  • QN908x BLE application fails to pair and bond  with BLE version 4.0

    Hello , Taken the FreeRTOS "wireless_example\Hid_device" example from the SDK example. Configure the pairing parameters to    .securityModeAndLevel = gSecurityMode_1_Level_2_c, .maxEncryptionKeySize = mcEn...
    Kishan Saralaya
    last modified by Kishan Saralaya