• Can I setting "Route Record Table Size" to more than 255?

    It is not allowed in "ZPS Configuration Editor". but in the generated source(zps_gen.c), the ZPS_tsNwkNibTblSize.u16Rct(nwkRouteRecordTable size) is type of uint16. Should I ignore the limit of "ZPS Configuration...
    Teddy Zheng
    last modified by Teddy Zheng
  • ZigBee 3.0 - connect up to 100 nodes

    We are using ZigBee 3.0 and JN-AN-1229-ZPS-Application-Template. We are having the problem of  the connection for 100 nodes. We are connecting 1 coordinator, 40 routers and 60 end devices. Some of the nodes ...
    Jia Na Lai
    last modified by Jia Na Lai
  • How to configure QN908x for the continuous SCAN mode? And to scan more than ten devices.

    How to configure QN908x for the continuous SCAN mode? And to scan more than ten devices. We tried to test this feature [always scan mode] using Wireless UART (freertos version) example code - where we commented...
    Kishan Saralaya
    last modified by Kishan Saralaya
  • [JN-AN-1218] [Light Bulb] response for On/Off?

    Dear Sirs,   Using the ZGWUI to send On/Off/Toggle command to a Light-Bulb device, we can see the response message (ex: Type:0x8000 and others) showing on ZGWUI.  My questions are: 1. In which API of the ...
    alan lin
    last modified by alan lin
  • simultaneous  connecctions of BLE

    Hi, I want to use KW36 as central to connect several BLE keys. And I have referred the DOC "Multiple Connections in Bluetooth LE Central Device ". This demo looks like, each time only one BLE temp sensor can be ...
    yanpo li
    last modified by yanpo li
  • support wifi iwinfo

    Hi Support,   We search Internet for a while, but cannot find iwinfo support on yocto/i.mx. Do you know anyone has ever pull iwinfo into yocto/i.mx? Thanks.   Regards, Stephen 
    Steven Yu
    last modified by Steven Yu
  • BLE Border Router with FRDMKW41Z(radio)

    Hi Team, Currently i'm working on Openthread Border router(Rasberrypi) with FRDMKW41Z as a radio. I have gone through IOT SDK(Nrf5) for enabling the 6lowpan BLE Border router using raspbeery pi. But they are connect...
    Ramya Venkatesha
    last modified by Ramya Venkatesha
  • JN516x - OTP read API and how to block JTAG

    Dear all:   Now I am using JN5161 to develop a Green power switch(using MicroMAC Stack). and I have some questions about JN516x: 1. By default, every JN516x have a 64bit pre-programmed MAC address, but i can't ...
    Zero Zero
    last modified by Zero Zero
  • MKW41z BLE  not working after enabling random address and pairing.

    I am using MKW41Z with connectivity software. I created a custom application based on the provided examples and able to run it successfully with a custom android application acting as a client. But the issue I am fac...
    Rahul Singh
    last modified by Rahul Singh
  • The multi-communication feature of the KW36

    I would like to a ask a question about the multi-communication feature of the KW36.  In our design, The KW36 will use BLE's SSP (serial port profile) and without using FreeRtos to communicate with 4 periphe...
    sihan chen
    last modified by sihan chen
  • QN9080 - Devkit stoped working

    Hello team, I have been working with QN9080 a few weeks back and everything was working properly, but when I have tried to work with the devkit once again and I got the following error: 'Wire Ack Fault'. Could you p...
    Shai Berman
    last modified by Shai Berman
  • Model of MBC13720

    Hi,   I am trying to use the MBC13720 low noise transistor to design an LNA. But I have not found its model.   To build a circuit using the transistor in ADS, what else I can do?   Thanks.
    Yuanzhi Liu
    last modified by Yuanzhi Liu
  • [JN-AN-1220] Is it possible for Light-Sensor to join Control-Bridge without NFC?

    Dear all,   I am confused if it is necessary to use NFC for Light-Sensor (node) to join Control-Bridge (Coordinator). Is it possible to let Light-Sensor (node) to directly join Control-Bridge (Coordinator)...
    alan lin
    last modified by alan lin
  • 88w8987 bt class 2

    Hello,   I'm trying to update bt power class of the 88w8987 and I haven't succeed yet. Their is no information in the datasheet and labtool is still failing.   What can I do ?   Best, Eric Delanghe...
    Eric Delanghe
    last modified by Eric Delanghe
  • How to getting started on FRDM-KW36

    Hello ~  I am working on FRDM-KW36 development board and use (frdmkw36_wireless_examples_bluetooth_w_uart_freerots) SDK to build code by MCUXpresso IDE.  Questions :  Q1 : How to enable debug UART/conso...
    sihan chen
    last modified by sihan chen
  • How to getting started on FRDM-KW36

    Hello ~  I am working on FRDM-KW36 development board and use (frdmkw36_wireless_examples_bluetooth_w_uart_freerots) SDK to build code and by MCUXpresso IDE.  Question :  Q1 : How to enable debug UART...
    sihan chen
    last modified by sihan chen
  • How to enable console/UART for FRDM-KW36 debugging

    HI All,        I am working on FRDM-KW36 development board and use (frdmkw36_wireless_examples_bluetooth_w_uart_freerots) SDK to build code through MCUXpresso IDE.  I need debug console...
    sihan chen
    last modified by sihan chen
  • QN908X Stack Timer/RTC FR not waking MCU from Deep Sleep (0)

    I'm having trouble getting the RTC Free-Run interrupt to wake up the MCU when I go into DS0.   Seems to work ok when just sleeping.    Note:  I am using a digital clock as my XTAL32K source w...
    Jose Raffucci
    last modified by Jose Raffucci
  • KW36 connect with 4 peripherals

    I would like to a ask a question about the multi-communication feature of the KW36.  In our design, The KW36 will use BLE's SSP (serial port profile) and without using FreeRtos to communicate with 4 peripher...
    sihan chen
    last modified by sihan chen
  • Need Sample code for CAN protocol of FRDM-KW36 kit

    Hello, I am working on FRDM-KW36 on mcuxpresso ide. I was looking for sample codes for CAN protocol through which i can read the data of any car(PID value).There are some flexcan sample example available on the ide b...
    chandra mani
    last modified by chandra mani