• QN9090 - Hardware Considerations

    Hello team,   My customer is planning to start drawing his schematics with QN9090 and got the inquiries below: 1a. What are the JTAG pins (for flashing and debug the device)?  1b. in case the customer wan...
    Shai Berman
    last modified by Shai Berman
  • The FRDM-KW36 can't connect with smart phone

    Hello All ~              I have used the button to config the FRDM-KW36 as a peripheral device for to connect to the smart phone. Although the smart ph...
    sihan chen
    last modified by sihan chen
  • Wifi Chipset Firmware Loading

    Hi all, I am using a module with an 8987 wifi bt Chipset. To help me debug it not working in my Linux system I would like to gain a better understanding of how it works.   Does the module come with any firmware ...
    Eoin O'Connell
    last modified by Eoin O'Connell
  • The route did not forward the command to the destination address

    Hi, We used JN5169 to make a light control system,but now I found a problem, sometimes, the button can not control the light.Packet capture found that the button sent the command to the route, but the route did not f...
    德平 吕
    last modified by 德平 吕
  • Hardfault when using eeprom in KW36 BLE demo

    I want to use eeprom in KW36 BLE demo. In frdmkw36_wireless_examples_bluetooth_hrs_freertos, I set gAppUseNvm_d and gNvUseFlexNVM_d to 1. In __NvModuleInit(), it configures eeprom and res...
    mo xinyu
    last modified by mo xinyu
  • Creating a custom profile using NXP BLE stack server, how much characteristics can be added?

    Dear, I'm using a Kinetis KW41Z with NXP BLE stack and rtos. I read several documents especially NXP DOC-332703 and DOC-328287. Did someone know how much characteristics can be added?   Regards Lothar
    Lothar Schönfeld
    last modified by Lothar Schönfeld
  • Any IRQ related limitations on using hardware triggers for ADC with BLE?

    I'm trying to configure the ADC to use a PWM output as trigger, in a BLE project.   Once the right IRQ was enabled, when I try to start the timer, the program hangs.   If I start the timer without enabling...
    sharon urban
    last modified by sharon urban
  • KW38 flexcan example not working

    Hi,   I am trying to get CAN comms working on KW38 kit. I tries two examples and on both I am facing same issue.    1. flexcan interrupt transfer 2. flexcan loopback transfer   In the loopback ...
    Ravindra Singh
    last modified by Ravindra Singh
  • QN9030

    1. BLE QN9030 passes through two or three walls and doors in the home (about 10~30 meters).     Can QN9030 meet this demand? How much dBm is needed to achieve it? 2. Can multiple QN9030 be directly ...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W HCI

    Using HCI as an example, whether the program has a reserved position to adjust the frequency offset(xtal Trim)?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W CMET

    I study JN-AN-1242 The test item of CMET only lists Zigbee mode, so it is only suitable for testing Zigbee, not suitable for testing BLE and Thread ? We need CMET for BLE and thread. When can CMET add these two opti...
    Daniel Tseng
    last modified by Daniel Tseng
  • Building issue of Demo project"N-AN-1218-Zigbee-3-0-Light-Bulb" on beyongstudion for NXP

    Hi , Could you please check what's the problem? When i import the "JN-AN-1218-ZIGBEE 3.0 -LIGHT BULD"  into the Beyondstudion for NXP and running buliding command,the building process is interuupted and waring " ...
    peter zhong
    last modified by peter zhong
  • K32W CMET operation

    I read jn-an-1242,May I ask how to use CMET in pairs?  
    Daniel Tseng
    last modified by Daniel Tseng
  • JN5169: MCPS  Synchronous Data Confirm

    According to the 2.6 User Guide, it is possible to have Synchronous Data Confirm (i.e. Return the results immediately, rather than the results being posted as a deferred confirm sometime later).   See Secti...
    Alberto Gallegos
    last modified by Alberto Gallegos
  • error ZPS_eAplZdoAddReplaceLinkKey eStatus= 174

    Hi Mario,   I found the same problem happened again, but I open a new question, since this issue problably been archived. I have used the gateway for weeks, and joined, unjoined many devices (by leave request)...
    Benoit Roue
    last modified by Benoit Roue
  • K32W DK6Programmer.exe

    When I execute  " DK6Programmer.exe -s COM29 -p heart.bin" Only the appropriate size will be cleared 1. What is the sector block? 2. How can I clear all Flash?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W multilink download

    Refer to UM11393  ch 2.9.2. I can't find J1, but looking at the file J1 should refer to J2 usb interface   Using MCUXpresso IDE to burn K32W Carrier board via Multilink and SWD, the following error messa...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Multilink

    Because K32W is a new chip, it has the following problems: 1. Does the SWD interface on the K32W main board support Multilink (debug tool) download  as usual? 2. If not support  Multilink , what debug tool...
    Daniel Tseng
    last modified by Daniel Tseng
  • Default Response on JN5169

    Hi all, I facing a problem: My coordinator not receive Default Response from any device when I send a command. I defined: /* Set this True to disable non error default responses from clusters */ #define ZCL_DISABLE_D...
    Giau Nguyen
    last modified by Giau Nguyen
  • Device leaves automatically

    Hi,   We have flashed control bridge application in our JN5189 chip which acts as a co-ordinator. As soon as we pair our end sensor with coordinator. End sensor leaves from the network. When analysed the sniff...
    Deepanraj Anbarasan
    last modified by Deepanraj Anbarasan