• K32W Turnaround Test

    I don’t understand, what is the Turnaround Test? How to measure? What is he measuring? I have studied ch17 (JN-AN-1242), but I still don't understand.
    Daniel Tseng
    last modified by Daniel Tseng
  • Default Response on JN5169

    Hi all, I facing a problem: My coordinator not receive Default Response from any device when I send a command. I defined: /* Set this True to disable non error default responses from clusters */ #define ZCL_DISABLE_D...
    Giau Nguyen
    last modified by Giau Nguyen
  • K32W Multilink

    Because K32W is a new chip, it has the following problems: 1. Does the SWD interface on the K32W main board support Multilink (debug tool) download  as usual? 2. If not support  Multilink , what debug tool...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W test tool

    I use "Test Tool 12.9.1.0" to test Multillink. The following screen will be presented without k32w selection items and the word of option may be overwritten on WIN10. How do I choose to make K32W work properly? Ca...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W: Timeout

    In the LPC-link2 USB connection: 1. When I entered the DK6 Flash Programmer, I found that the timeout jumped out,      how many seconds will it jump out of the DK6 Flash programmer? 2. When I d...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W (WIFI Co-existence)

    The documents on the NXP website do not provide WIFI Co-existence related documents(Pin settings, software timing diagram). Is NXP currently ready for this function(WIFI Co-existence)? If so, can it be released?
    Daniel Tseng
    last modified by Daniel Tseng
  • KW37_38_39 Minimum BoM Presentation.pdf

    This guide describes the hardware for the KW38 minimum BoM development board. The KW38 Minimum BoM development board is configurable, low-power, and cost-effective evaluation and development board for application prot...
    Christophe Menard
    last modified by Christophe Menard
  • Device leaves automatically

    Hi,   We have flashed control bridge application in our JN5189 chip which acts as a co-ordinator. As soon as we pair our end sensor with coordinator. End sensor leaves from the network. When analysed the sniff...
    Deepanraj Anbarasan
    last modified by Deepanraj Anbarasan
  • K32W Flash Programmer

    K32W board needs to use FTDI_USB or USB_UART to execute Flash Prrogrammer. But usually Uart of SOC is directly connected to PIO8/PIO9(TX/RX) of K32W, and there is no FTDI_USB/USB_UART How does SOC do Flash Programmer?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W baud rate

    1. Update with "DK6 Production Flash Programmer".     I know that when using LPC-Link2 USB connection can not reach 1M baud rate, what is the default speed?     What is  the  highes...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W ISP mode

    If the SOC(Wifi module) is connected to K32W, can Uart Rom Bootloader(ISP mode) run to 1M speed with no CTS/RTS ?
    Daniel Tseng
    last modified by Daniel Tseng
  • RFID TAG

    Hello,   I am working on an automotive project and I need to find RFID tags that can be scanned from radius up to 300ft, along with the scanner for it.   Thank you
    Mahmoud Abdelhadi
    last modified by Mahmoud Abdelhadi
  • The route did not forward the command to the destination address

    Hi, We used JN5169 to make a light control system,but now I found a problem, sometimes, the button can not control the light.Packet capture found that the button sent the command to the route, but the route did not f...
    德平 吕
    last modified by 德平 吕
  • K32W FTDI interface can't work

    I use "LPC-Link2" for debugging can work, but it doesn’t work when I use "FTDI". FTDI : JP4&JP7 short 2 and 3. PC's USB connection Carrier Main Board show following: Use MCUXpresso IDE to download, it w...
    Daniel Tseng
    last modified by Daniel Tseng
  • Thread Router Eligible Device GPIO Control

    Hello community,   I've started a Thread project, which I intend to modify so that I control the LEDs of a node 2 over the air, pressing the switches in node 1. I'm currently using the "frdmkw41z_wireless_examp...
    Santiago Roman
    last modified by Santiago Roman
  • K32W ISP for LPC-LINK2

    Refer to "ch 2.5.2 ISP button" of UM11393 DK6 Production Flash programmer can be executed on FTDI USB interface. Can the DK6 Production Flash programmer be executed on LPC-Link2?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W: JN-UG-3127

    UM11394   NXP's official website cannot find this file(JN-UG-3127). I want to understand the meaning of each parameter  
    Daniel Tseng
    last modified by Daniel Tseng
  • USB-KW41Z  BLE sniffer does not decode Ethernet II "data". Missing wireshark plug in?

    USB-KW41Z  BLE sniffer does not decode Ethernet II "data" on wireshark. It is like the "kinetis adapter information" plug in does not work.   Set up: Windows 10 + wireshark 2.6.1 + Kinetis protocol an...
    Roberto Quilez
    last modified by Roberto Quilez
  • .sNwkStatusIndicationEvent.u8Status = 0x11

    Hi Mario,   JN5169 / AN1216 / SW4170   I cannot find the enum or the #define of the field u8Status in the structure ZPS_tsAfNwkStatusIndEvent. The stack is sending me this event often with status = 0x11. ...
    Benoit Roue
    last modified by Benoit Roue
  • KW37_38_39_Bluetooth LE Range Performance.pdf

    This document provides information on distance measurements depending of the Bluetooth LE data rate (1Mbps, 2Mbps, LR S=2 & LR S=8). The FRDM-KW38 boards are used to perform the measurements.   Results are ...
    Christophe Menard
    last modified by Christophe Menard