• Patches for HDMI Dongle JB4.2.2_1.0.0-GA Release

    There are two patches for HDMI Dongle JB4.2, one is remove the warning message, the other is fix to that sleep will not recover.   Jack Mao
    Jack Mao
    last modified by Adrian Puga Candelario
  • ZPS_EVENT_NWK_LEAVE_INDICATION event does not occur when the End Device leave.

    Coordinator changed from Zigbee 1.2(JN-AN-1223) to Zigbee 3.0(JN-AN-1216). ZigBee 3.0 does not receive leave event of the end device.   Environment When no event occurs (ZPS_EVENT_NWK_LEAVE_INDICATION ) - zigb...
    Seung Ho Kim
    last modified by Seung Ho Kim
  • QN9020 : Internal flash write steps

    Hi,       I have some questions on the internal flash write am hoping someone could help with, please.    1) On bootup, the power to the flash is enabled by default. But as soon as "plf_init...
    Tony Makkiel
    last modified by Tony Makkiel
  • Patch for HDMI Dongle JB4.2.2_1.1.0-GA Release to Fix Wifi Issue

    This patch fix the issue in hdmi dongle JB4.2.2_1.1.0-GA release that wifi((STA+P2P)/AP) cann't be enabled properly.   In the root directory of Android Source Code, use the following command to apply the patch: ...
    Hailong Wan
    last modified by Adrian Puga Candelario
  • How does the DSPI driver of the R41Z work?

    Hello community, I am trying to communicate a R41Z-TA-A to a Serial Flash device (SST25VF040B) which uses the SPI. I've got an example library for the Serial Flash and I want to do my own driver for the flash but wit...
    Cristina Alvarez
    last modified by Cristina Alvarez
  • JN-AN-1189 - Error while compiling

    Hi.   I am using beyond studio build 1308. Stack JN-SW-4168 The target is a JN5169   And i try to compile the app note JN-AN-1189. The zipfile has been dezipped in the workspace and then imported. I us...
    Tim Gros
    last modified by Tim Gros
  • Flash mac address 88w8987

    Hello,   I want to flash new mac address in 88w8987. Using labtool I use the sequence: 2 => Use Bluetooth Successful connect to hci1 45 => Read MAC from OTP Get 41.41.41.41.41.41 46 aa.bb.cc.dd.ee.ff ...
    Eric Delanghe
    last modified by Eric Delanghe
  • disconnect after the connection

    Hello,    i use the QN908X device.    I modify the private_profile_client_project for my project and i want to connect at an other ble device.   i success to scan and connect to the server ...
    Romain Auber
    last modified by Romain Auber
  • What would be behaviour of BGA6130 for RF receiving state ?

    Hello , We are using BGA6130 in our Lora trans-receive application for getting more gain at transmit side. We are using AI thinker RA01 module and it has common RF pin for In and out , so after that i have placed BGA...
    darshan panchal
    last modified by darshan panchal
  • Is project for mc13224 compatible for mc13226?

    I want to get a few extra sets of mc13224, but was being told it has been obsoleted. Only mc13226Pro-DBG is available instead.   Possible to advise if a project that compiled for mc13224 can be loaded to mc1322...
    Isaac Lim
    last modified by Isaac Lim
  • ATD Module in MC1321x

    The MC13211/212/213 Reference Manual states that the Analog to Digital (ATD) Module is part of MC1321x. Examining C/C+ CodeWarrior Development Studio, I find "ADC_Interface.h" in PLM -> Interface folder, but only ...
    Erwin Beck
    last modified by Erwin Beck
  • QN9080 internal OSC32M at 48 MHz?

    I have a QN9080 chip revision D (QN9080DHNE) and I believe the internal OSC32M is running at 48 MHz, not 32 MHz. Is this even possible?   Here are the experiments I ran, the board has a 32 MHz external XTAL, I c...
    iosabi .
    last modified by iosabi .
  • 88W8978 datasheet

    请提供一份双频Wi-Fi芯片88W8978完整的datasheet,谢谢! 
    Wenhai Liao
    last modified by Wenhai Liao
  • Drivers for 88W8964

    Hey everyone!   I'm one of may OpenWRT contributors and I'm also a owner of a Linksys WRT3200ACM witch has a NXP 88W8964 wifi chip. Before being NXP bought all the wireless solutions from Marvell, they were dev...
    Tiago Gaspar
    last modified by Tiago Gaspar
  • Exporting Persistent Data on JN516x to Host

    Hi all, As I know, the ZigBee Control Bridge node by default uses the internal EEPROM to hold persisted data. This is about 4KByte in JN5169 device and can restrict network size. To overcome this, we need to export ...
    Giau Nguyen
    last modified by Giau Nguyen
  • Howto join live Zigbee 3.0 Light network

    Hello   I have a question similar to How and where to set default link keys? from Warren Ashcroft and ZBPro Configuration JN-AN-1218 from @youpko.   I'm using JN-AN-1218 Zigbee 3.0...
    matthias.brand@gmail.com
    last modified by matthias.brand@gmail.com
  • KW36: "Connection Failed to establish" error received when trying to connect KW36

    Hi,   I am using KW36 hid device example with security mode 1 level 2. KW36 is configured as peripheral device and i use it as a advertiser. I am using MCuXpresso KW36 SDK 2.2.2. I am using just works pairing. ...
    Sai Kalyana Raman
    last modified by Sai Kalyana Raman
  • KW36: Insufficient Authentication error response is sent to iPhone when Report Map Characteristic value is read

    Hi,   I am using KW36 as a peripheral device and working with hid_device example. I tried to pair the KW36 with the iPhone using nrf connect. i use just works pairing in my project with security mode 1 level 2....
    Sai Kalyana Raman
    last modified by Sai Kalyana Raman
  • KW36  multitask

    I try to add those sample code in frdmkw36_wireless_examples_bluetooth_w_uart_freertos wireless_uart.c: void test_task(void* argument) {    while(1) {       Serial_Print(gApp...
    mo xinyu
    last modified by mo xinyu
  • Network restore after reset on 802.15.4

    Hi,   I'm using SDK2.2.0 on MKW41Z. With the 802.15.4 examples in the SDK, a new network is created by the coordinator after every reset. Similarly, an end device always scans for all the networks in range aft...
    Alexandru Stefan
    last modified by Alexandru Stefan