• Drivers for 88W8964

    Hey everyone!   I'm one of may OpenWRT contributors and I'm also a owner of a Linksys WRT3200ACM witch has a NXP 88W8964 wifi chip. Before being NXP bought all the wireless solutions from Marvell, they were dev...
    Tiago Gaspar
    last modified by Tiago Gaspar
  • QN9090 - using all 8 ADC ch.

    Hello team,   According to the QN9090 Datasheet, there are 8 channels of ADCs. But after following the documentation, the ADC6 and ADC7 are for internal use for example measuring the internal temperat...
    Shai Berman
    last modified by Shai Berman
  • Question on the QN908x series

    1. I want to know if an external 32 Mhz and 32 kHz oscillator is required 2. the datasheet for the QN908x series says the peak power is 10mW but the tranmist at 0dB consumes 3.5 mA which corresponds to 10.5 mW power s...
    Alex Conan
    last modified by Alex Conan
  • KW36 - HeartRate_PowerDownMode_Switch??

    Hi,   I'm testing an example of heart rate. (frdmkw36_wireless_examples_bluetooth_hrs_freertos)  The Switch is different when power down mode is set and not set. 1. The SW3 operate as gKBD_Event...
    ayden hong
    last modified by ayden hong
  • QN9090 BLE SDK into debug fail with MCUXpresso

    Hi all,    I get QN9090-DK006 and download "SDK_2.6.0_QN9090DK6" to import into MCUXpresso. But after I build one project to into debug mode to get below status. it don't from main() like user guid...
    Ethan Chen
    last modified by Ethan Chen
  • KW36 FSCI bootloader

    I want to use FSCI bootloader to update KW36 and I flow this: Reprogramming a KW36 device using the FSCI bootloader . It look like success: But I press the sw, it does not start advertising. Doe...
    mo xinyu
    last modified by mo xinyu
  • FRDM-KW36 - Extended Advertising

    Hi, NXP expert.   I am testing beacon(extended Advertising) using KW36 Board. The Gap_SetExtAdvertisingParameters function returns an error while testing an extended Advertising using the beacon ...
    ayden hong
    last modified by ayden hong
  • KW35/36 to KW37/38/39 migration: flashloader UART0 pinning

    User will be concerned by this note in the following cases:  - migration from KW35/36_HVQFN48 Wettable Flank package version to KW37/38/39  - Flashloader is used via UART0 interface    So, ...
    Matthieu Baudry
    created by Matthieu Baudry
  • FRDMKW38UG.pdf

    This guide describes the hardware for the FRDM-KW38 Freedom development board. The FRDM-KW38 Freedom development board is highly configurable, low-power, and cost-effective evaluation and development board for ap...
    Christophe Menard
    last modified by Christophe Menard
  • KW38 KW39 KW37 Hardware board PCB design in check list

    In addition of the Design Guideline, PCB hardware package find here the design in check list to build sucessfully your own PCB
    Matthieu Baudry
    last modified by Matthieu Baudry
  • The FRDM-KW36 can't connect with smart phone

    Hello All ~              I have used the button to config the FRDM-KW36 as a peripheral device for to connect to the smart phone. Although the smart ph...
    sihan chen
    last modified by sihan chen
  • KW41:How to print out CFSR and HFSR?

    We use KW41's "SMAC connectivity test" as the base to develop the program. Because the current self-written program crashes during execution. I want to use HardFault to debug. Just like the following URL that  re...
    Daniel Tseng
    last modified by Daniel Tseng
  • BAP64Q - Quad PIN diode attenuator

    Dear Team,   In datasheet of BAP64Q Application circuit states that shunt diodes are biased with 0.75 Vdc.  But if i try to simulate that circuit i get very poor return loss and attenuation is around 2...
    Rohith K
    last modified by Rohith K
  • Low Power Support on OTAP Client Software

    IntroductionThis document is to guide how to modify the OTAP Client software to the Low Power module. The starting point of this document is the OTAP Client example in the FRDM-KW36 SDK v2.2.2. Deep Sleep Modes This ...
  • QN9080 - ADC Timing Test

    Hello Team,   My customer is using QN9080 for his new design, the customer has tested the ADC Timuung by trigger sample in single-mode and measured the time till finished to convert the results and he found out ...
    Shai Berman
    last modified by Shai Berman
  • kw41z zigbee home automation profile 1.2??

    Hi  I bought zha 1.2 sensor and want to connect sensor and kw41z board Is it possible? And can I use nxp zigbee home automation sdk? I wonder if kw41z supports zigbee home automation profile 1.2. thanks
    JunTae Lee
    last modified by JunTae Lee
  • Deep sleep Mode  KW41Z                                                                                                         

    Hi,   Where can I find examples of how to implement deep sleep for the KW41Z microcontrollers running Thread protocol?
    varun sahni
    last modified by varun sahni
  • Some problems about JN-AN-1247

    Hi, When I use the JN-AN-1247 in JN5189,I find a few bug. I set specific chip to JN5189 in makefile,then compile it. 1、I program the binary file into flash memory of JN5189,then start network by ZGWUI.But Sometimes i...
    德平 吕
    last modified by 德平 吕
  • QN9020 SWD DEBUG download program failed

    Hello there The QN9020DK development kit uses SWD mode to download the program. Has not been successful. Although KEIL can recognize SWD (as shown in Figure 1 below). However, a warning will be reported during the dow...
    qq2_2ww qq2_2ww
    last modified by qq2_2ww qq2_2ww
  • KW37_38_39 Minimum BoM Presentation.pdf

    This guide describes the hardware for the KW38 minimum BoM development board. The KW38 Minimum BoM development board is configurable, low-power, and cost-effective evaluation and development board for application prot...
    Christophe Menard
    last modified by Christophe Menard