• K32W multilink download

    Refer to UM11393  ch 2.9.2. I can't find J1, but looking at the file J1 should refer to J2 usb interface   Using MCUXpresso IDE to burn K32W Carrier board via Multilink and SWD, the following error messa...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Multilink

    Because K32W is a new chip, it has the following problems: 1. Does the SWD interface on the K32W main board support Multilink (debug tool) download  as usual? 2. If not support  Multilink , what debug tool...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W test tool

    I use "Test Tool 12.9.1.0" to test Multillink. The following screen will be presented without k32w selection items and the word of option may be overwritten on WIN10. How do I choose to make K32W work properly? Ca...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W: Timeout

    In the LPC-link2 USB connection: 1. When I entered the DK6 Flash Programmer, I found that the timeout jumped out,      how many seconds will it jump out of the DK6 Flash programmer? 2. When I d...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W CMET

    I read jn-an-1242,May I ask how to use CMET in pairs?  
    Daniel Tseng
    last modified by Daniel Tseng
  • In QN908x how to keep the configured NVDS data untouched while reloading firmware

    After saving the configured NVDS data tag values in the QN908x Flash when we reflash the firmware using QN908x programming tool - SWD Download option (where we un-check "Download NVDS File") previously saved NVDS data...
    Kishan Saralaya
    last modified by Kishan Saralaya
  • K32W CMET

    I study JN-AN-1242 The test item of CMET only lists Zigbee mode, so it is only suitable for testing Zigbee, not suitable for testing BLE and Thread ? We need CMET for BLE and thread. When can CMET add these two opti...
    Daniel Tseng
    last modified by Daniel Tseng
  • How to check number of nodes (router and end device) joined and leave from coordinator when run program

    Hi All,   I use module JN5169-001-M06 is coordinator, sofeware JN-AN-1217 and sdk JN-SW-4170. I config default size of the Routing table is 70 #define ZNC_MAX_TCLK_DEVICES  &...
    Dang Thanh Nha
    last modified by Dang Thanh Nha
  • QN9080 - What is the maximum bandwidth in WUART profile

    Hello Team, I have a customer who plans to use #QN9080-001-M17 in their next platform design. he needs to transmit raw data (prefer using WUART profile) at a minimum of 1.25Mbps (I know this device support ...
    Shai Berman
    last modified by Shai Berman
  • K32W (WIFI Co-existence)

    The documents on the NXP website do not provide WIFI Co-existence related documents(Pin settings, software timing diagram). Is NXP currently ready for this function(WIFI Co-existence)? If so, can it be released?
    Daniel Tseng
    last modified by Daniel Tseng
  • KW37_38_39 Minimum BoM Presentation.pdf

    This guide describes the hardware for the KW38 minimum BoM development board. The KW38 Minimum BoM development board is configurable, low-power, and cost-effective evaluation and development board for application prot...
    Christophe Menard
    last modified by Christophe Menard
  • Device leaves automatically

    Hi,   We have flashed control bridge application in our JN5189 chip which acts as a co-ordinator. As soon as we pair our end sensor with coordinator. End sensor leaves from the network. When analysed the sniff...
    Deepanraj Anbarasan
    last modified by Deepanraj Anbarasan
  • K32W CTS/RTS

     Because Uart coce of the original SDK only has TX/RX, neither will add CTS/RTS.   Does UART need to add CTS/RTS?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Flash Programmer

    K32W board needs to use FTDI_USB or USB_UART to execute Flash Prrogrammer. But usually Uart of SOC is directly connected to PIO8/PIO9(TX/RX) of K32W, and there is no FTDI_USB/USB_UART How does SOC do Flash Programmer?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W baud rate

    1. Update with "DK6 Production Flash Programmer".     I know that when using LPC-Link2 USB connection can not reach 1M baud rate, what is the default speed?     What is  the  highes...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W ISP mode

    If the SOC(Wifi module) is connected to K32W, can Uart Rom Bootloader(ISP mode) run to 1M speed with no CTS/RTS ?
    Daniel Tseng
    last modified by Daniel Tseng
  • error ZPS_eAplZdoAddReplaceLinkKey eStatus= 174

    Hi Mario,   I found the same problem happened again, but I open a new question, since this issue problably been archived. I have used the gateway for weeks, and joined, unjoined many devices (by leave request)...
    Benoit Roue
    last modified by Benoit Roue
  • Default Response on JN5169

    Hi all, I facing a problem: My coordinator not receive Default Response from any device when I send a command. I defined: /* Set this True to disable non error default responses from clusters */ #define ZCL_DISABLE_D...
    Giau Nguyen
    created by Giau Nguyen
  • RFID TAG

    Hello,   I am working on an automotive project and I need to find RFID tags that can be scanned from radius up to 300ft, along with the scanner for it.   Thank you
    Mahmoud Abdelhadi
    last modified by Mahmoud Abdelhadi
  • The route did not forward the command to the destination address

    Hi, We used JN5169 to make a light control system,but now I found a problem, sometimes, the button can not control the light.Packet capture found that the button sent the command to the route, but the route did not f...
    德平 吕
    last modified by 德平 吕