• Creating a custom profile using NXP BLE stack server, how much characteristics can be added?

    Dear, I'm using a Kinetis KW41Z with NXP BLE stack and rtos. I read several documents especially NXP DOC-332703 and DOC-328287. Did someone know how much characteristics can be added?   Regards Lothar
    Lothar Schönfeld
    last modified by Lothar Schönfeld
  • Any IRQ related limitations on using hardware triggers for ADC with BLE?

    I'm trying to configure the ADC to use a PWM output as trigger, in a BLE project.   Once the right IRQ was enabled, when I try to start the timer, the program hangs.   If I start the timer without enabling...
    sharon urban
    last modified by sharon urban
  • KW38 flexcan example not working

    Hi,   I am trying to get CAN comms working on KW38 kit. I tries two examples and on both I am facing same issue.    1. flexcan interrupt transfer 2. flexcan loopback transfer   In the loopback ...
    Ravindra Singh
    last modified by Ravindra Singh
  • QN9030

    1. BLE QN9030 passes through two or three walls and doors in the home (about 10~30 meters).     Can QN9030 meet this demand? How much dBm is needed to achieve it? 2. Can multiple QN9030 be directly ...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W HCI

    Using HCI as an example, whether the program has a reserved position to adjust the frequency offset(xtal Trim)?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W CMET

    I study JN-AN-1242 The test item of CMET only lists Zigbee mode, so it is only suitable for testing Zigbee, not suitable for testing BLE and Thread ? We need CMET for BLE and thread. When can CMET add these two opti...
    Daniel Tseng
    last modified by Daniel Tseng
  • Building issue of Demo project"N-AN-1218-Zigbee-3-0-Light-Bulb" on beyongstudion for NXP

    Hi , Could you please check what's the problem? When i import the "JN-AN-1218-ZIGBEE 3.0 -LIGHT BULD"  into the Beyondstudion for NXP and running buliding command,the building process is interuupted and waring " ...
    peter zhong
    last modified by peter zhong
  • K32W CMET operation

    I read jn-an-1242,May I ask how to use CMET in pairs?  
    Daniel Tseng
    last modified by Daniel Tseng
  • JN5169: MCPS  Synchronous Data Confirm

    According to the 2.6 User Guide, it is possible to have Synchronous Data Confirm (i.e. Return the results immediately, rather than the results being posted as a deferred confirm sometime later).   See Secti...
    Alberto Gallegos
    last modified by Alberto Gallegos
  • error ZPS_eAplZdoAddReplaceLinkKey eStatus= 174

    Hi Mario,   I found the same problem happened again, but I open a new question, since this issue problably been archived. I have used the gateway for weeks, and joined, unjoined many devices (by leave request)...
    Benoit Roue
    last modified by Benoit Roue
  • K32W DK6Programmer.exe

    When I execute  " DK6Programmer.exe -s COM29 -p heart.bin" Only the appropriate size will be cleared 1. What is the sector block? 2. How can I clear all Flash?
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W multilink download

    Refer to UM11393  ch 2.9.2. I can't find J1, but looking at the file J1 should refer to J2 usb interface   Using MCUXpresso IDE to burn K32W Carrier board via Multilink and SWD, the following error messa...
    Daniel Tseng
    last modified by Daniel Tseng
  • K32W Multilink

    Because K32W is a new chip, it has the following problems: 1. Does the SWD interface on the K32W main board support Multilink (debug tool) download  as usual? 2. If not support  Multilink , what debug tool...
    Daniel Tseng
    last modified by Daniel Tseng
  • Default Response on JN5169

    Hi all, I facing a problem: My coordinator not receive Default Response from any device when I send a command. I defined: /* Set this True to disable non error default responses from clusters */ #define ZCL_DISABLE_D...
    Giau Nguyen
    last modified by Giau Nguyen
  • Device leaves automatically

    Hi,   We have flashed control bridge application in our JN5189 chip which acts as a co-ordinator. As soon as we pair our end sensor with coordinator. End sensor leaves from the network. When analysed the sniff...
    Deepanraj Anbarasan
    last modified by Deepanraj Anbarasan
  • KW36 trimming adjust of 32kHz RTC external oscillator

    IntroductionThe FRDM-KW36 includes an RTC module with a 32 kHz crystal oscillator. This module generates a 32 kHz clock source for the MCU whilst running on very low power mode. This oscillato...
  • JN-AN-1218 build problems

    I success fully compiled the JN-AN-1218 with the following configuration make LIGHT=DimmableLight JENNIC_CHIP_FAMILY=JN516x JENNIC_CHIP=JN5168 DR=DR1175 TRACE=1 GP_SUPPORT=0 GP_DEVICE=COMBO_BASIC OTA=0 TOUCHLINK=1 &#...
    youpko
    last modified by youpko
  • In QN908x how to keep the configured NVDS data untouched while reloading firmware

    After saving the configured NVDS data tag values in the QN908x Flash when we reflash the firmware using QN908x programming tool - SWD Download option (where we un-check "Download NVDS File") previously saved NVDS data...
    Kishan Saralaya
    last modified by Kishan Saralaya
  • [JN-AN-1220:JN5169] How to read the binding table?

    Dear Sirs,   If a end device has bound with a coordinator through ZGWUI. After power cycle the end device, how to read the binding information while end device power on?   Thanks! 
    alan lin
    last modified by alan lin
  • [JN-AN-1216] How long will the Coordinator keep the data before device request?

    Dear Sirs,   In [JN-AN-1216] "IoT Control bridge", how long will the Coordinator keep the data until the device polling for it? How to extend the period?   Thanks!
    alan lin
    last modified by alan lin