• [JN-AN-1220] Is it possible for Light-Sensor to join Control-Bridge without NFC?

    Dear all,   I am confused if it is necessary to use NFC for Light-Sensor (node) to join Control-Bridge (Coordinator). Is it possible to let Light-Sensor (node) to directly join Control-Bridge (Coordinator)...
    alan lin
    last modified by alan lin
  • 88w8987 bt class 2

    Hello,   I'm trying to update bt power class of the 88w8987 and I haven't succeed yet. Their is no information in the datasheet and labtool is still failing.   What can I do ?   Best, Eric Delanghe...
    Eric Delanghe
    last modified by Eric Delanghe
  • How to getting started on FRDM-KW36

    Hello ~  I am working on FRDM-KW36 development board and use (frdmkw36_wireless_examples_bluetooth_w_uart_freerots) SDK to build code by MCUXpresso IDE.  Questions :  Q1 : How to enable debug UART/conso...
    sihan chen
    last modified by sihan chen
  • How to getting started on FRDM-KW36

    Hello ~  I am working on FRDM-KW36 development board and use (frdmkw36_wireless_examples_bluetooth_w_uart_freerots) SDK to build code and by MCUXpresso IDE.  Question :  Q1 : How to enable debug UART...
    sihan chen
    last modified by sihan chen
  • How to enable console/UART for FRDM-KW36 debugging

    HI All,        I am working on FRDM-KW36 development board and use (frdmkw36_wireless_examples_bluetooth_w_uart_freerots) SDK to build code through MCUXpresso IDE.  I need debug console...
    sihan chen
    last modified by sihan chen
  • Reprogramming a KW36 device using the OTAP Client Software

    Introduction This document guides to load a new software image in a KW36 device through OTAP (Over The Air Programming) bootloader focusing on the various memory features supported by this device. Software Requirement...
  • Smart Energy support to JN5179

    We are using JN5179 ZigBee MCU and Using ZigBee 3.0 stack. Now, we want to support the Smart Energy profile on JN5179. But ZigBee 3.0 is not supporting all clusters of Smart Energy Profile.   NXP's Smart Energy ...
    Ravi Ramani
    last modified by Ravi Ramani
  • QN908X Stack Timer/RTC FR not waking MCU from Deep Sleep (0)

    I'm having trouble getting the RTC Free-Run interrupt to wake up the MCU when I go into DS0.   Seems to work ok when just sleeping.    Note:  I am using a digital clock as my XTAL32K source w...
    Jose Raffucci
    last modified by Jose Raffucci
  • KW36 connect with 4 peripherals

    I would like to a ask a question about the multi-communication feature of the KW36.  In our design, The KW36 will use BLE's SSP (serial port profile) and without using FreeRtos to communicate with 4 peripher...
    sihan chen
    last modified by sihan chen
  • Need Sample code for CAN protocol of FRDM-KW36 kit

    Hello, I am working on FRDM-KW36 on mcuxpresso ide. I was looking for sample codes for CAN protocol through which i can read the data of any car(PID value).There are some flexcan sample example available on the ide b...
    chandra mani
    last modified by chandra mani
  • How to perform RF TEST for embedded KW36

    Hi,   We are using KW36A for our product and in it we want to test the BTLE TX and RX service for RF. based on my previous question, I came to know already that we have Test tool( https://community.nxp.com/doc...
    Kuldeep Chaturvedi
    last modified by Kuldeep Chaturvedi
  • PPP connection with GPRS modem and FRDM-K64F

    Hi,   Is there any guide or example for establishing ppp connection with FRDM-K64F and GPRS modem (BG96). I have read some of posts GPRS demo - FRDM-K64F vs MQX 4.2 vs BGS2T modem - working now  yet I...
    Darshan Shah
    last modified by Darshan Shah
  • kw36 sdk2.2.0 hci_bb have no rx dta from the ble.

    hi,dear nxp engineer   i used KW36 freedom board with 2.2.0 sdk. when running the HCI_BB demo. debugging use  the test tool as the "BLE Demo Application user's guide" infer. I do exactly as the doc instruct...
    yuan xiao
    last modified by yuan xiao
  • KW36 can switch Central / peripheral?

    Continuing the previous question, KW36A OTA   Now there is an idea:     We want to integrate the two OTA updates as following           A. BLE Demo Applications User ...
    Daniel Tseng
    last modified by Daniel Tseng
  • kw36 connection interval,slave latency supersiontimeout set

    hi, dear nxp fae     i am using a kw36 freedom board. used the SDK2.2.1 and run some examples. i want to change the three parameter connection interval, slave latency and superisontimeout. but i found there...
    yuan xiao
    last modified by yuan xiao
  • Creating HCI Custom Commands for KW36

    IntroductionHCI Application is a Host Controller Interface application which provides a serial communication to interface with the KW40/KW41/KW35/KW36/QN9080 BLE radio part. It enables the user to have a way to contro...
  • QN908x wakeup from PD0 leaves XTAL running

    I am running into a situation where my boards are waking up from PD0 and then begin to draw additional current (approx 1.5mA in my case).  I am not actively using the BLE stack in this case.  The stack is in...
    Jose Raffucci
    last modified by Jose Raffucci
  • JN-AN-1217-Zigbee-3-0-Base-Device - UART1

    Hi suppor team! Now. I'm working with JN-AN-1217-Zigbee-3-0-Base-Device Relate to end:  Enabling UART1 is Coordinator is JN-1217-AN-Zigbee-3-0-Base Device for JN5168   TB Coordinator project work well with ...
    Tran Minh Tan
    last modified by Tran Minh Tan
  • Is there an example code for ThingMagic to read NXP G2iL tag

    Is there an example code for ThingMagic to read NXP G2iL tag?
    ping mei
    last modified by ping mei
  • Interface CYW4343W WiFi/BLE with FRDM-K64F 

    Hi, I would like to interface LBEE5KL1DX-TEMP (CYW4343W) with FRDM-K64F. Is there any guide or link which is useful for interfacing CYW4343W with K64F?
    Darshan Shah
    last modified by Darshan Shah