• RSSI vs Distance measurements in an indoor environment using KW0x

    Received Signal Strength Indicator (RSSI) is measurement of the power presented in a received radio signal. An RSSI use case could be its conversion to distance. KW0x radio has a RSSI register where RSSI can be re...
    Luis Antonio Burgos Lopez
    last modified by Luis Antonio Burgos Lopez
  • I2C protocol demo code for JN5168 available?(EEPROM or RTC)

    Hello All,    I am working on JN5168-001-M00Z module. i am very well familiar with this module and beyond studio.  now i am stuck on I2C protocol.  is there any demo code is available for I2C P...
    Dheeraj Sawant
    last modified by Dheeraj Sawant
  • Main Loop Restarting every 20sec

    Hello Friends,    I am Using JN-AN-1162 Application Note.  in that i am using DEVICEREMOTE.C file to write my code.(shows in Picture)  in that "PRIVATE void vAppMainLoop(bool_t bWarmStart) "...
    Dheeraj Sawant
    last modified by Dheeraj Sawant
  • JN5179 RSSI issue with SKY66112 PA

    Hi,   We are using SKY66112 - PA with JN5179 chipset for Antenna diversity features. We are not able to exact match GPIO connection between SKY and JN5179 as per reference M16 module.   RFTX and RFRX conne...
    Hitesh Gambhava
    last modified by Hitesh Gambhava
  • Virtual COM Port Driver for Q908x USB Dongle

    HI,   I am running windows 7 and when I plug the Q908x usb dongle the O.S fails to find the driver. I tried installing SiLabs VCP, FTDI VCP, and all the drivers in the Drivers folder of the NXP tools I down...
    Xavier Vilajosana
    last modified by Xavier Vilajosana
  • Radio Range for JN5168-001-M00

    Hello ,  I am new to JN516x Zigbee Pro development ,and I want to know what is the maximum distance between 2 modules  (JN5168-001-M00) that cannot be exceeded for proper communication between the 2 modules....
    David Ashraf
    last modified by David Ashraf
  • What do wee need

    I have several questions about JN5168-001-M00; -          In case where we prefer the product, what do we need separately? -        ...
    Gungor YILDIZ
    last modified by Gungor YILDIZ
  • Implement RF Communication between Two JN5168 Module

    Hello Friends,    i just familiar with JN5168-001-M00 module.  i have learn how to compile and build a code and create binary files. credit goes to NXP community.    Now i have come to my ...
    Dheeraj Sawant
    last modified by Dheeraj Sawant
  • Commissioning Thread sensors

    Q1. If we have different Thread sensors from various vendors, What are the minimal parameters need to be configured at commissioner for joining? Thread Short Eui / Long EUI / All FFF... & Pskd   Q2. How ...
    sensenthuran
    last modified by sensenthuran
  • RAM usage on Kinetis Design Studio

    Hi everyone.   I'm using Thread protocol with a KW41Z kinetis. I'm trying to watch the RAM memory usage of one kinetis connected to the mesh but I can't. I would like to know how many memory a router is was...
    Miguel González
    last modified by Miguel González
  • CC1110 as FXTH87 434Mhz Reciever

    Hello Everyone,   I am using fxth870911d to transmit sensor data at 434 Mhz,  I am initializing the fxth87 chip as follow,   void Init_RF(void) {      /* Turn module on in...
    Sumir Jha
    last modified by Sumir Jha
  • Eclipse update site with plug-ins for ZigBee PRO is not availabe

    I'm a JN5148 user, and recently I was facing re-install the "JN5148 Software Developer’s Kit" by following the instruction from "JN-UG-3064-JN5148-SDK-2v0.pdf", everything went right except when I was trying to ...
    Li Vivian
    last modified by Li Vivian
  • Comparison between Wireless Protocols

    In the attached document, information about which is the best wireless protocol depending on your application can be found.    To find this document useful is important to know precisely what is needed on y...
  • Decrypting ZigBee packets with Wireshark

          Short video that demonstrates how to decrypt ZigBee packets using the Transport Key on Wireshark. Using ZigBee's default Trust Center link key“ZigBeeAlliance09” = 5A:69:67:42:65:65:41:...
    Juan Carlos Pacheco
    last modified by Juan Carlos Pacheco
  • NXP connectivity FCC/ETSI Certification Software

    I would like to start this discussion to talk about FCC/ETSI certification software we use to provide for connectivity customer boards. FCC/ETSI are mandatory certifications we need to pass in order to be able to...
    josem.reyes.chaidez
    last modified by josem.reyes.chaidez
  • MKW30Z OTAP demo gUseBootloaderLink_d=1 issue

    IAR 7.50;  KW40Z_Connectivity_Software_1.0.1 (KSDK_1.3.0) The issue is generated when gUseBootloaderLink_d=1 is present in Linker section. The leds don't flash; callback functions on timers are not executed (on...
    Lucian Firan
    last modified by Lucian Firan
  • KDS source filename case problems

    Hey everyone,     I'm using KDS under Linux Manjaro, and I stumbled on a filename case problems with the provided examples.   For example, it seems like the FSCI source files are all named 'FsciModule...
    romainbazile
    last modified by romainbazile
  • Any body with a solution ?

    sam khaukha
    last modified by sam khaukha
  • Bluetooth 5.0

    Is there a BLE chipset available that supports bluetooth 5.0 ? If not, can you provide us a timeline when that may be available?   Thanks,
    Kalyan V
    last modified by Kalyan V
  • How to Enable JN516x SPI master mode :JN-SW-4170/4168?

    I'm using the JN5169 with the JN-SW-4170, I want to use the SPI port on the JN516x in master mode to interface to a slave device (via CS SPISEL1 : DIO0). But my SPI read access are returning always 0xffff because the...
    Jean Bony
    last modified by Jean Bony